<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: which version of codewarrior support s9s12gn48? 5.1 and 5.2 cannot! in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/which-version-of-codewarrior-support-s9s12gn48-5-1-and-5-2/m-p/504404#M4254</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/430483"&gt;Add missing derivatives to CodeWarrior HCS12(X) 5.2 (Unofficial Method)&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Here is another way to add in support for all the missing ones.&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 23 Jul 2016 18:15:22 GMT</pubDate>
    <dc:creator>RodneyMcGee</dc:creator>
    <dc:date>2016-07-23T18:15:22Z</dc:date>
    <item>
      <title>which version of codewarrior support s9s12gn48? 5.1 and 5.2 cannot!</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/which-version-of-codewarrior-support-s9s12gn48-5-1-and-5-2/m-p/504402#M4252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 May 2016 10:48:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/which-version-of-codewarrior-support-s9s12gn48-5-1-and-5-2/m-p/504402#M4252</guid>
      <dc:creator>cailili</dc:creator>
      <dc:date>2016-05-26T10:48:27Z</dc:date>
    </item>
    <item>
      <title>Re: which version of codewarrior support s9s12gn48? 5.1 and 5.2 cannot!</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/which-version-of-codewarrior-support-s9s12gn48-5-1-and-5-2/m-p/504403#M4253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello cai,&lt;/P&gt;&lt;P&gt;Yes, the CW v5.2 miss come chips , there is a workaround for some chips ,&lt;/P&gt;&lt;P&gt;while only for the chips that have patch on the website , about the detail&lt;/P&gt;&lt;P&gt;method please refer to this thread :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-330657"&gt;How to install missing device to CodeWarrior for HCS12 v5.2&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While for some chips, we only can use the CW v5.1 .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 01:53:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/which-version-of-codewarrior-support-s9s12gn48-5-1-and-5-2/m-p/504403#M4253</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-06-15T01:53:01Z</dc:date>
    </item>
    <item>
      <title>Re: which version of codewarrior support s9s12gn48? 5.1 and 5.2 cannot!</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/which-version-of-codewarrior-support-s9s12gn48-5-1-and-5-2/m-p/504404#M4254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/430483"&gt;Add missing derivatives to CodeWarrior HCS12(X) 5.2 (Unofficial Method)&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Here is another way to add in support for all the missing ones.&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Jul 2016 18:15:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/which-version-of-codewarrior-support-s9s12gn48-5-1-and-5-2/m-p/504404#M4254</guid>
      <dc:creator>RodneyMcGee</dc:creator>
      <dc:date>2016-07-23T18:15:22Z</dc:date>
    </item>
  </channel>
</rss>