<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this  in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502606#M4213</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In MCU V6.3 the Hi-Wave external debugger was used but it was the P&amp;amp;E flash programmer.&lt;/P&gt;&lt;P&gt;When the debugger was launched, the P&amp;amp;E flash programmer was used to flash the application on-board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can install MCU V6.3 on win 7 64 bit OS too.&lt;/P&gt;&lt;P&gt;There are some posts about it on community.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Run installer under win 7 and higher:&lt;A href="https://community.nxp.com/thread/302974"&gt;Install CodeWarrior 6.3 Windows 7 &amp;amp;amp; 10 x64 directly (Classic version)&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Copy past the installation:&lt;A href="https://community.nxp.com/message/505995"&gt;Re: Re: Install CodeWarrior 6.3 (Classic) directly under Windows 7 x64&lt;/A&gt; &lt;/P&gt;&lt;P&gt;The P&amp;amp;E Drivers contained in the installation are not working with Win&amp;nbsp; 7 64 bit OS.&lt;/P&gt;&lt;P&gt;However you can download and install last version from P&amp;amp;E web site.&lt;/P&gt;&lt;P&gt;After to have installed new version, you can use the MCU v6.3 under Win 7 64 bit PC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://www.pemicro.com/faqs/faq_view.cfm?id=29" title="http://www.pemicro.com/faqs/faq_view.cfm?id=29"&gt;P&amp;amp;E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools, debug probes, and …&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;NXP Technical Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Feb 2016 09:40:30 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2016-02-12T09:40:30Z</dc:date>
    <item>
      <title>Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502603#M4210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Feb 2016 09:50:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502603#M4210</guid>
      <dc:creator>dharanidevimani</dc:creator>
      <dc:date>2016-02-11T09:50:40Z</dc:date>
    </item>
    <item>
      <title>Re: Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502604#M4211</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Flash Programmer V1.2 was released for Win XP 32 bit OS.&lt;/P&gt;&lt;P&gt;We don't have new version supporting Win 7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is the CCS feature.&lt;/P&gt;&lt;P&gt;The CCS version used is not compatible with 64 bit OS.&lt;/P&gt;&lt;P&gt;We've the same problem with CW for DSC V8.3 for instance.&lt;/P&gt;&lt;P&gt;The workaround is to update the CCS to a new version supporting the Win 7 and 64 bit OS.&lt;/P&gt;&lt;P&gt;You can install the last version included on Eclipse: CW for MCU V10.6.4.&lt;/P&gt;&lt;P&gt;Copy the CCS folder to your installation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another solution is to use the DSC Flasher.&lt;/P&gt;&lt;P&gt;You will find details at the AN:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4824.pdf" title="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4824.pdf"&gt;http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4824.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;DSC Flasher can be downloaded from the link:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;A href="http://www.nxp.com/products/microcontrollers-and-processors/more-processors/dsp-dsc/dscs/mc56f80xx/digital-signal-controller-for-motor-control-applications:56F801X?fpsp=1&amp;amp;tab=Documentation_Tab" title="http://www.nxp.com/products/microcontrollers-and-processors/more-processors/dsp-dsc/dscs/mc56f80xx/digital-signal-controller-for-motor-control-applications:56F801X?fpsp=1&amp;amp;tab=Documentation_Tab"&gt;56F801X |Digital Signal Controller|NXP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37007i75BB00BF00EC0A4D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;NXP Technical Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Feb 2016 13:04:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502604#M4211</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2016-02-11T13:04:21Z</dc:date>
    </item>
    <item>
      <title>Re: Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502605#M4212</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the answer. We will try with DSC Flasher.&lt;/P&gt;&lt;P&gt;Similarly, can you let me know the solutions available for programming the MCU in 64-bit version. Previously in 32-bit version PC, we were using "hiwave" prog of CW _MCU_V6.3_SE.&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Feb 2016 08:56:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502605#M4212</guid>
      <dc:creator>dharanidevimani</dc:creator>
      <dc:date>2016-02-12T08:56:50Z</dc:date>
    </item>
    <item>
      <title>Re: Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502606#M4213</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In MCU V6.3 the Hi-Wave external debugger was used but it was the P&amp;amp;E flash programmer.&lt;/P&gt;&lt;P&gt;When the debugger was launched, the P&amp;amp;E flash programmer was used to flash the application on-board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can install MCU V6.3 on win 7 64 bit OS too.&lt;/P&gt;&lt;P&gt;There are some posts about it on community.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Run installer under win 7 and higher:&lt;A href="https://community.nxp.com/thread/302974"&gt;Install CodeWarrior 6.3 Windows 7 &amp;amp;amp; 10 x64 directly (Classic version)&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Copy past the installation:&lt;A href="https://community.nxp.com/message/505995"&gt;Re: Re: Install CodeWarrior 6.3 (Classic) directly under Windows 7 x64&lt;/A&gt; &lt;/P&gt;&lt;P&gt;The P&amp;amp;E Drivers contained in the installation are not working with Win&amp;nbsp; 7 64 bit OS.&lt;/P&gt;&lt;P&gt;However you can download and install last version from P&amp;amp;E web site.&lt;/P&gt;&lt;P&gt;After to have installed new version, you can use the MCU v6.3 under Win 7 64 bit PC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://www.pemicro.com/faqs/faq_view.cfm?id=29" title="http://www.pemicro.com/faqs/faq_view.cfm?id=29"&gt;P&amp;amp;E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools, debug probes, and …&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;NXP Technical Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Feb 2016 09:40:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502606#M4213</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2016-02-12T09:40:30Z</dc:date>
    </item>
    <item>
      <title>Re: Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502607#M4214</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN class="replyToName"&gt;Dharani devi &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG class="font-color-meta"&gt;&lt;SPAN class="replyToName"&gt;&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;56800E Flash Programmer can work on 64bit OS with USBTAP, for the solution, please refer to:&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-102607"&gt;https://community.freescale.com/docs/DOC-102607&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Fiona Kuang&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Technical Information &amp;amp; Commercial Support&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Feb 2016 03:01:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502607#M4214</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2016-02-16T03:01:57Z</dc:date>
    </item>
    <item>
      <title>Re: Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502608#M4215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #101010; background-color: #fafafa; font-size: 18px;"&gt;Hello.&lt;/SPAN&gt;&lt;BR style="color: #101010; background-color: #fafafa; font-size: 18px;" /&gt;&lt;SPAN style="color: #101010; background-color: #fafafa; font-size: 18px;"&gt;The solution you mentioned is a workable solution in Windows 7, not in a 64-bit environment.&lt;/SPAN&gt;&lt;BR style="color: #101010; background-color: #fafafa; font-size: 18px;" /&gt;&lt;SPAN style="color: #101010; background-color: #fafafa; font-size: 18px;"&gt;I tried it several times.&lt;/SPAN&gt;&lt;BR style="color: #101010; background-color: #fafafa; font-size: 18px;" /&gt;&lt;SPAN style="color: #101010; background-color: #fafafa; font-size: 18px;"&gt;Yet I still don't work properly in 64-bit, Windows 7 environments.&lt;/SPAN&gt;&lt;BR style="color: #101010; background-color: #fafafa; font-size: 18px;" /&gt;&lt;SPAN style="color: #101010; background-color: #fafafa; font-size: 18px;"&gt;I also tried the program '&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;DSC Flasher'&lt;/SPAN&gt;, but it doesn't work either.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jan 2017 08:21:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502608#M4215</guid>
      <dc:creator>eunaehcho</dc:creator>
      <dc:date>2017-01-23T08:21:24Z</dc:date>
    </item>
    <item>
      <title>Re: Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502609#M4216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eunaeh,&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Just FYI. &lt;/SPAN&gt; I ever followed this doc of installing&amp;nbsp;&lt;SPAN style="font-size: 10pt; font-family: arial,helvetica,sans-serif;"&gt;56800E Flash Programmer v1.2&lt;/SPAN&gt; on two 64bit win7. It works normally.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;&lt;A _jive_internal="true" data-containerid="11190" data-containertype="14" data-content-finding="Community" data-objectid="102607" data-objecttype="102" href="https://community.nxp.com/docs/DOC-102607"&gt;https://community.freescale.com/docs/DOC-102607&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Please make sure you have windows admin right and test it on another 64bit win7 computer.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Jennie&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jan 2017 09:41:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502609#M4216</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2017-01-23T09:41:37Z</dc:date>
    </item>
    <item>
      <title>Re: Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502610#M4217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your kindness.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried several times, but the problem has still remained.&lt;/P&gt;&lt;P&gt;Running the 56800E Flash Programmer after the CCS, the CCS operation stops.&lt;/P&gt;&lt;P&gt;In addition, the 'Flash timeout 'error occurs in the Flash programmer as below.&lt;/P&gt;&lt;P&gt;I have been struggling for several days because this problem has not been resolved...&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12326i7E803A441CC0A972/image-size/large?v=v2&amp;amp;px=999" title="CCCSClient_Network_timeout_captureImage.JPG" alt="CCCSClient_Network_timeout_captureImage.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jan 2017 01:45:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-the-flash-programmer-of-DSC-56800E-is-available-for-Windows/m-p/502610#M4217</guid>
      <dc:creator>eunaehcho</dc:creator>
      <dc:date>2017-01-24T01:45:05Z</dc:date>
    </item>
  </channel>
</rss>