<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: T4240QDS bareboard project can't print &amp;quot;Welcome to Code Warrior&amp;quot;</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/T4240QDS-bareboard-project-can-t-print-quot-Welcome-to-Code/m-p/499873#M4175</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Joseph,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to the following answer I provided in case 00077659, if your problem remains, please provide the information which I required previously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial;"&gt;I verified CodeWarrior 10.5.1 sample project on T4240QDS(with FPGA 5), no problem to print the following message in UART1 console.&lt;BR /&gt;&amp;gt;Core0-Thread0: Welcome to CodeWarrior!&lt;BR /&gt;&lt;BR /&gt;There is an known issue regarding T4240QDS connecting CodeWarrior, I am not sure whether you got to know it previously. CodeWarrior fails to connect to T4240QDS CPU v2.0 board with the default FPGA 6. Users need to downgrade FPGA to version 5 on T4240QDS to connect to CodeWarrior.&lt;BR /&gt;&lt;SPAN&gt;Please refer to the thread(&lt;/SPAN&gt;&lt;A class="jive-link-thread-small" data-containerid="2029" data-containertype="14" data-objectid="328058" data-objecttype="1" href="https://community.nxp.com/thread/328058#comment-442081"&gt;https://community.nxp.com/message/442081#comment-442081&lt;/A&gt;&lt;SPAN&gt;) for details.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;If your problem remains, would you please enable and capture CCS log and send it to me?&lt;BR /&gt;Please refer to the following procedure.&lt;BR /&gt;Please enable CCS log from "Run-&amp;gt;Debug Configurations -&amp;gt;&amp;lt;project&amp;gt;-core0_RAM_-T4240_Download-&amp;gt;Edit...-&amp;gt;Advanced-&amp;gt;Advanced CCS setting-&amp;gt;Enable logging", and connect to the target from &lt;BR /&gt;"Run-&amp;gt;Debug Configurations-&amp;gt;&amp;lt;project&amp;gt;-core0_RAM_T4240-Download-&amp;gt;Debug”, the CCS log will be displayed in the console panel in CodeWarrior IDE. &lt;BR /&gt;(If the CCS log in the console is truncated, please enlarge the console&amp;nbsp; buffer from Window-&amp;gt;Preferences-&amp;gt;Run/Debug-&amp;gt;Console-&amp;gt;uncheck&amp;nbsp; "Limit console output". Please open the console panel from Window-&amp;gt;Show View-&amp;gt;Console, and if nothing displayed, please choose the correct session on the right top icon in the panel.)&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 May 2016 06:05:07 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2016-05-31T06:05:07Z</dc:date>
    <item>
      <title>T4240QDS bareboard project can't print "Welcome to Code Warrior"</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/T4240QDS-bareboard-project-can-t-print-quot-Welcome-to-Code/m-p/499872#M4174</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I try to run CodeWarrior PA 10.5.1&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. bareboard project&lt;/P&gt;&lt;P&gt;2. on T4240QDS (SCH-27313 REV. D5 ; S/N K1529 34823-018 ; 00:04:9F:03:CF:B8)&lt;/P&gt;&lt;P&gt;3. I keep the default UART1 as output.&lt;/P&gt;&lt;P&gt;4. But it wont show on the serial UART1 of T4240QDS.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What could be the problem?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Joseph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 May 2016 00:16:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/T4240QDS-bareboard-project-can-t-print-quot-Welcome-to-Code/m-p/499872#M4174</guid>
      <dc:creator>josephtjoharno</dc:creator>
      <dc:date>2016-05-25T00:16:08Z</dc:date>
    </item>
    <item>
      <title>Re: T4240QDS bareboard project can't print "Welcome to Code Warrior"</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/T4240QDS-bareboard-project-can-t-print-quot-Welcome-to-Code/m-p/499873#M4175</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Joseph,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to the following answer I provided in case 00077659, if your problem remains, please provide the information which I required previously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial;"&gt;I verified CodeWarrior 10.5.1 sample project on T4240QDS(with FPGA 5), no problem to print the following message in UART1 console.&lt;BR /&gt;&amp;gt;Core0-Thread0: Welcome to CodeWarrior!&lt;BR /&gt;&lt;BR /&gt;There is an known issue regarding T4240QDS connecting CodeWarrior, I am not sure whether you got to know it previously. CodeWarrior fails to connect to T4240QDS CPU v2.0 board with the default FPGA 6. Users need to downgrade FPGA to version 5 on T4240QDS to connect to CodeWarrior.&lt;BR /&gt;&lt;SPAN&gt;Please refer to the thread(&lt;/SPAN&gt;&lt;A class="jive-link-thread-small" data-containerid="2029" data-containertype="14" data-objectid="328058" data-objecttype="1" href="https://community.nxp.com/thread/328058#comment-442081"&gt;https://community.nxp.com/message/442081#comment-442081&lt;/A&gt;&lt;SPAN&gt;) for details.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;If your problem remains, would you please enable and capture CCS log and send it to me?&lt;BR /&gt;Please refer to the following procedure.&lt;BR /&gt;Please enable CCS log from "Run-&amp;gt;Debug Configurations -&amp;gt;&amp;lt;project&amp;gt;-core0_RAM_-T4240_Download-&amp;gt;Edit...-&amp;gt;Advanced-&amp;gt;Advanced CCS setting-&amp;gt;Enable logging", and connect to the target from &lt;BR /&gt;"Run-&amp;gt;Debug Configurations-&amp;gt;&amp;lt;project&amp;gt;-core0_RAM_T4240-Download-&amp;gt;Debug”, the CCS log will be displayed in the console panel in CodeWarrior IDE. &lt;BR /&gt;(If the CCS log in the console is truncated, please enlarge the console&amp;nbsp; buffer from Window-&amp;gt;Preferences-&amp;gt;Run/Debug-&amp;gt;Console-&amp;gt;uncheck&amp;nbsp; "Limit console output". Please open the console panel from Window-&amp;gt;Show View-&amp;gt;Console, and if nothing displayed, please choose the correct session on the right top icon in the panel.)&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 May 2016 06:05:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/T4240QDS-bareboard-project-can-t-print-quot-Welcome-to-Code/m-p/499873#M4175</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2016-05-31T06:05:07Z</dc:date>
    </item>
  </channel>
</rss>