<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic having functions of type Union in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/having-functions-of-type-Union/m-p/274186#M396</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With IAR I was able to typedef a variable as a union then create a function of that type variable so the return on the function would be used with the features I had in the union. CW10 is not liking this. I'm getting a "declaration syntax error". I can not find any documentation that states a function can NOT be of type Union in C and why has IAR allowed this as valid syntax and executes correctly?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 Dec 2013 01:30:48 GMT</pubDate>
    <dc:creator>markgreggory</dc:creator>
    <dc:date>2013-12-21T01:30:48Z</dc:date>
    <item>
      <title>having functions of type Union</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/having-functions-of-type-Union/m-p/274186#M396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With IAR I was able to typedef a variable as a union then create a function of that type variable so the return on the function would be used with the features I had in the union. CW10 is not liking this. I'm getting a "declaration syntax error". I can not find any documentation that states a function can NOT be of type Union in C and why has IAR allowed this as valid syntax and executes correctly?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Dec 2013 01:30:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/having-functions-of-type-Union/m-p/274186#M396</guid>
      <dc:creator>markgreggory</dc:creator>
      <dc:date>2013-12-21T01:30:48Z</dc:date>
    </item>
    <item>
      <title>Re: having functions of type Union</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/having-functions-of-type-Union/m-p/274187#M397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Found the problem. I had to remove: #include &amp;lt;stdio.h&amp;gt;&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Dec 2013 01:42:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/having-functions-of-type-Union/m-p/274187#M397</guid>
      <dc:creator>markgreggory</dc:creator>
      <dc:date>2013-12-21T01:42:26Z</dc:date>
    </item>
  </channel>
</rss>