<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to write to eSDHC memory using Codewarrior 10.5 for PA Flash Programmer? in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-write-to-eSDHC-memory-using-Codewarrior-10-5-for-PA-Flash/m-p/474668#M3730</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CodeWarrior for PA doesn't provide support SD card programming in Flash Programmer. SDFlash.elf and SDFlash_Utility.elf are placed by mistake in CodeWarrior for PA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Jan 2016 08:14:17 GMT</pubDate>
    <dc:creator>addiyi</dc:creator>
    <dc:date>2016-01-08T08:14:17Z</dc:date>
    <item>
      <title>How to write to eSDHC memory using Codewarrior 10.5 for PA Flash Programmer?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-write-to-eSDHC-memory-using-Codewarrior-10-5-for-PA-Flash/m-p/474667#M3729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to write to the eSDHC memory via a P2041 processor using the Flash Programmer I get an error message saying the command failed. I have added a device to the devices list setting the algorithm used to SDFlash.elf and the utility field to SDFlash_Utility.elf (both elf files are located in the Flash Programmer directory of Codewarrior). I may have an incorrect format for the device xml file as I can't find a device that is capable of eSDHC programming in the provided list to use as an example.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There doesn't seem to be a place to set the base address for the eSDHC registers and the memory is not mapped via a LAW.&lt;/P&gt;&lt;P&gt;How do I point the programmer or algorithm to the eSDHC base register?&lt;/P&gt;&lt;P&gt;Or am I suppose to map the memory using a LAW (which doesn't seem to be possible as there is not transaction target ID for the eSDHC)?&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've attached my device xml file.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337858"&gt;MTFC4GMWDQ-3M.xml.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jan 2016 08:59:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-write-to-eSDHC-memory-using-Codewarrior-10-5-for-PA-Flash/m-p/474667#M3729</guid>
      <dc:creator>jsvholmes</dc:creator>
      <dc:date>2016-01-07T08:59:13Z</dc:date>
    </item>
    <item>
      <title>Re: How to write to eSDHC memory using Codewarrior 10.5 for PA Flash Programmer?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-write-to-eSDHC-memory-using-Codewarrior-10-5-for-PA-Flash/m-p/474668#M3730</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CodeWarrior for PA doesn't provide support SD card programming in Flash Programmer. SDFlash.elf and SDFlash_Utility.elf are placed by mistake in CodeWarrior for PA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jan 2016 08:14:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-write-to-eSDHC-memory-using-Codewarrior-10-5-for-PA-Flash/m-p/474668#M3730</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2016-01-08T08:14:17Z</dc:date>
    </item>
  </channel>
</rss>