<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: Can't connect CCS</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459959#M3409</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;From the CCS console, I can sorta add a command converter, but trying to debug from CW removes the command converter:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22074iC1C06AC181C8B4A9/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Mar 2016 00:10:36 GMT</pubDate>
    <dc:creator>jasonhendrix</dc:creator>
    <dc:date>2016-03-09T00:10:36Z</dc:date>
    <item>
      <title>Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459955#M3405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to connect to the LS1021ATWR dev board with Code Warrior for QorIQ 10.0.8 and the TAP.&amp;nbsp; I keep getting the following error:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CCSProtocolPlugin::Can't connect to CCS&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The CCS.exe is running according to task manager, and has opened port 41475 according to netstat.&amp;nbsp; I'm running on Windows 8.1, 64-bit.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can access the probe's serial configuration interface through USB/serial.&amp;nbsp; If I configure an ethernet HW connection instead of USB, I get the same error.&amp;nbsp; Any suggestions on bringing the CW debugger and CCS together in harmony?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 01:29:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459955#M3405</guid>
      <dc:creator>jasonhendrix</dc:creator>
      <dc:date>2016-03-08T01:29:09Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459956#M3406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to bolow section from LS1021A_TWR_README.txt:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Information about processor revision 1&lt;/P&gt;&lt;P&gt;#--------------------------------------------#&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To debug a target with this processor revision you must use the CFG file "LS102xA_Rev1_ConfigChain.cfg" that can be found at the location&lt;/P&gt;&lt;P&gt;[CW install path]/ARMv7/ARM_Support/Configuration_Files/jtag_chains/. This file will be imported following the next steps:&lt;/P&gt;&lt;P&gt;1. Open "Debug Configurations..." and select your project;&lt;/P&gt;&lt;P&gt;2. Click on the "Edit..." button which can be found next to the drop list called "Connection" from the "Target Settings" view;&lt;/P&gt;&lt;P&gt;3. Click on the "Edit..." button which can be found next to the drop list called "Target";&lt;/P&gt;&lt;P&gt;4. Click on the "Edit..." button which can be found next to the drop list called "Target type";&lt;/P&gt;&lt;P&gt;5. Click "Import..." and then "File System..." and select the file specified above and then click OK until you return&lt;/P&gt;&lt;P&gt;to "Hardware or Simulator Target" window;&lt;/P&gt;&lt;P&gt;6. Select in the "Hardware or Simulator Target" window the initialization and memory files from the project;&lt;/P&gt;&lt;P&gt;7. Click OK until you return to "Debug Configurations..." window and click "Debug".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 07:26:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459956#M3406</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2016-03-08T07:26:44Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459957#M3407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the response.&amp;nbsp; Unfortunately, I can't perform step&amp;nbsp; 7, because:&lt;/P&gt;&lt;P&gt;"/LS102xA_Rev1_ConfigChain.cfg/LS1021A/C...Initialize target script is undefined."&lt;/P&gt;&lt;P&gt;That's the message that appears at the top of the "Hardware or Simulator Target" window as soon as I select the "Initialize Target" checkbox in the Initialization tab or the "Memory Configuration" checkbox in the Memory tab.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 18:30:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459957#M3407</guid>
      <dc:creator>jasonhendrix</dc:creator>
      <dc:date>2016-03-08T18:30:49Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459958#M3408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Still getting the error "Can't connect to CCS Server".&amp;nbsp; But I did find the CCS console and it claims the connection was opened momentarily and then closed.&amp;nbsp; I'll try attaching a picture:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1125i28C0F73FD995574A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 23:06:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459958#M3408</guid>
      <dc:creator>jasonhendrix</dc:creator>
      <dc:date>2016-03-08T23:06:01Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459959#M3409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;From the CCS console, I can sorta add a command converter, but trying to debug from CW removes the command converter:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22074iC1C06AC181C8B4A9/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 00:10:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459959#M3409</guid>
      <dc:creator>jasonhendrix</dc:creator>
      <dc:date>2016-03-09T00:10:36Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459960#M3410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figured out how to add an initialization script for the Initialization and Memory tabs (click in the table cell in the right-most column in the "core" row. see attached picture).&amp;nbsp; No change in the ccs connection problem, however.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22093iAD14BC4F50FCC879/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 00:34:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459960#M3410</guid>
      <dc:creator>jasonhendrix</dc:creator>
      <dc:date>2016-03-09T00:34:37Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459961#M3411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;See post below for solution to the "script is undefined" problem.&amp;nbsp; You have to click in the table cell for the core and the script and then you will get a browse button.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 00:37:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459961#M3411</guid>
      <dc:creator>jasonhendrix</dc:creator>
      <dc:date>2016-03-09T00:37:02Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459962#M3412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Am I using processor rev 1?&amp;nbsp; How do I tell?&amp;nbsp; Here is the U-boot banner from my dev-kit:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22073iAE2051E3909F7292/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 01:31:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459962#M3412</guid>
      <dc:creator>jasonhendrix</dc:creator>
      <dc:date>2016-03-09T01:31:09Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459963#M3413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Still can't connect to CCS.&lt;/P&gt;&lt;P&gt;One last bit of info - the CCS Log:&lt;/P&gt;&lt;P&gt;ccs_open&lt;/P&gt;&lt;P&gt;&amp;nbsp; ipaddr = 127.0.0.1&lt;/P&gt;&lt;P&gt;&amp;nbsp; port = 41475&lt;/P&gt;&lt;P&gt;&amp;nbsp; timeout = 60&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_open; ccs_error = 0&lt;/P&gt;&lt;P&gt;ccs_get_connection_count&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; count = 1&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_get_connection_count; ccs_error = 0&lt;/P&gt;&lt;P&gt;ccs_available_connections&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; count = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_available_connections; ccs_error = 0&lt;/P&gt;&lt;P&gt;ccs_available_connections&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; count = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_available_connections; ccs_error = 0&lt;/P&gt;&lt;P&gt;ccs_config_cc&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; config_string = cwtap:0&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_config_cc; ccs_error = 0&lt;/P&gt;&lt;P&gt;ccs_available_connections&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; count = 1&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_available_connections; ccs_error = 0&lt;/P&gt;&lt;P&gt;ccs_cc_version&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; cc = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; version.major = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; version.minor = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_cc_version; ccs_error = 0&lt;/P&gt;&lt;P&gt;ccs_set_timeout&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; timeout = 60&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_set_timeout; ccs_error = 0&lt;/P&gt;&lt;P&gt;ccs_get_config_chain&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; device_list: (size = 0)&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_get_config_chain; ccs_error = 0&lt;/P&gt;&lt;P&gt;ccs_config_server&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; cc = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; server_config = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; value = 10000&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_config_server; ccs_error = 0&lt;/P&gt;&lt;P&gt;ccs_config_chain&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; cc = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; device_list: (size = 4)&lt;/P&gt;&lt;P&gt;&amp;nbsp; device[0]:: core_type=Generic Device(0); device_descr=[ir_length:8;dr_bypass_length:1;bypass_instruction:0xFF,0x00,0x00,0x00]&lt;/P&gt;&lt;P&gt;&amp;nbsp; device[1]:: core_type=LS1020A(273)&lt;/P&gt;&lt;P&gt;&amp;nbsp; device[2]:: core_type=DAP(232)&lt;/P&gt;&lt;P&gt;&amp;nbsp; device[3]:: core_type=SAP2(272)&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_config_chain; ccs_error = 0&lt;/P&gt;&lt;P&gt;ccs_get_config_chain&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; device_list: (size = 4)&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_get_config_chain; ccs_error = 0&lt;/P&gt;&lt;P&gt;ccs_get_config_chain&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; device_list: (size = 4)&lt;/P&gt;&lt;P&gt;&amp;nbsp; device[0]:: core_type=Generic Device(0)&lt;/P&gt;&lt;P&gt;&amp;nbsp; device[1]:: core_type=LS1020A(273)&lt;/P&gt;&lt;P&gt;&amp;nbsp; device[2]:: core_type=DAP(232)&lt;/P&gt;&lt;P&gt;&amp;nbsp; device[3]:: core_type=SAP2(272)&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_get_config_chain; ccs_error = 0&lt;/P&gt;&lt;P&gt;ccs_available_connections&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; count = 1&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_available_connections; ccs_error = 0&lt;/P&gt;&lt;P&gt;ccs_delete_cc&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; count = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_delete_cc; ccs_error = 0&lt;/P&gt;&lt;P&gt;ccs_close&lt;/P&gt;&lt;P&gt;&amp;nbsp; serverh = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; ccs_close; ccs_error = 0&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 03:07:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459963#M3413</guid>
      <dc:creator>jasonhendrix</dc:creator>
      <dc:date>2016-03-09T03:07:14Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459964#M3414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here's some evidence that the TAP probe is attached and alive:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22225i33A1BCE25F5C3E80/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 03:35:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459964#M3414</guid>
      <dc:creator>jasonhendrix</dc:creator>
      <dc:date>2016-03-09T03:35:07Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459965#M3415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Still can't connect to CCS.&lt;/P&gt;&lt;P&gt; I updated the probe OS. findcc now recognizes the probe tip, though it does call it a Cortex-10 tip.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22654i97D7CD0BFF341A4E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22690i25CF31123A9C9AEC/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 04:02:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459965#M3415</guid>
      <dc:creator>jasonhendrix</dc:creator>
      <dc:date>2016-03-09T04:02:16Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459966#M3416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are using Rev2, so it's not necessary to use steps from "&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Information about processor revision 1&lt;/SPAN&gt;".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Check the switches on your to use jtag and not CMSIS-DAP (SW2.8 = 1), then perform following steps in ccs and provide the output:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(bin) 51 % config cc cwtap&lt;/P&gt;&lt;P&gt;(bin) 52 % show cc&lt;/P&gt;&lt;P&gt;0: CodeWarrior TAP (cwtap) CC software ver. {0.0}&lt;/P&gt;&lt;P&gt;(bin) 53 % ccs::config_chain {ls1020a dap sap2}&lt;/P&gt;&lt;P&gt;(bin) 54 % display ::ccs::get_config_chain&lt;/P&gt;&lt;P&gt;Chain Position 0: LS1020A&lt;/P&gt;&lt;P&gt;Chain Position 1: CoreSight ATB Funnel&lt;/P&gt;&lt;P&gt;Chain Position 2: CoreSight TMC&lt;/P&gt;&lt;P&gt;Chain Position 3: CoreSight TMC&lt;/P&gt;&lt;P&gt;Chain Position 4: CoreSight TMC&lt;/P&gt;&lt;P&gt;Chain Position 5: CoreSight CTI&lt;/P&gt;&lt;P&gt;Chain Position 6: CoreSight CTI&lt;/P&gt;&lt;P&gt;Chain Position 7: CoreSight CTI&lt;/P&gt;&lt;P&gt;Chain Position 8: CoreSight ATB Funnel&lt;/P&gt;&lt;P&gt;Chain Position 9: Cortex-A7&lt;/P&gt;&lt;P&gt;Chain Position 10: Cortex-A7 PMU&lt;/P&gt;&lt;P&gt;Chain Position 11: Cortex-A7&lt;/P&gt;&lt;P&gt;Chain Position 12: Cortex-A7 PMU&lt;/P&gt;&lt;P&gt;Chain Position 13: CoreSight CTI&lt;/P&gt;&lt;P&gt;Chain Position 14: CoreSight CTI&lt;/P&gt;&lt;P&gt;Chain Position 15: Cortex-A7 ETM&lt;/P&gt;&lt;P&gt;Chain Position 16: Cortex-A7 ETM&lt;/P&gt;&lt;P&gt;Chain Position 17: DAP&lt;/P&gt;&lt;P&gt;Chain Position 18: SAP2&lt;/P&gt;&lt;P&gt;(bin) 55 % ::ccs::all_run_mode&lt;/P&gt;&lt;P&gt;CortexA7: Execute Mode &lt;/P&gt;&lt;P&gt;CortexA7: Reset Mode&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 06:23:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459966#M3416</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2016-03-09T06:23:10Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459967#M3417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SW2.8 = 1, here is my CCS output:&lt;/P&gt;&lt;P&gt;(bin) 44 % config cc cwtap&lt;/P&gt;&lt;P&gt;(bin) 45 % show cc&lt;/P&gt;&lt;P&gt;0: CodeWarrior TAP (cwtap) CC software ver. {0.0}&lt;/P&gt;&lt;P&gt;(bin) 46 % ccs::config_chain {ls1020a dap sap2}&lt;/P&gt;&lt;P&gt;(bin) 47 % display ::ccs::get_config_chain&lt;/P&gt;&lt;P&gt;Chain Position 0: LS1020A&lt;/P&gt;&lt;P&gt;Chain Position 1: CoreSight ATB Funnel&lt;/P&gt;&lt;P&gt;Chain Position 2: CoreSight TMC&lt;/P&gt;&lt;P&gt;Chain Position 3: CoreSight TMC&lt;/P&gt;&lt;P&gt;Chain Position 4: CoreSight TMC&lt;/P&gt;&lt;P&gt;Chain Position 5: CoreSight CTI&lt;/P&gt;&lt;P&gt;Chain Position 6: CoreSight CTI&lt;/P&gt;&lt;P&gt;Chain Position 7: CoreSight CTI&lt;/P&gt;&lt;P&gt;Chain Position 8: CoreSight ATB Funnel&lt;/P&gt;&lt;P&gt;Chain Position 9: Cortex-A7&lt;/P&gt;&lt;P&gt;Chain Position 10: Cortex-A7 PMU&lt;/P&gt;&lt;P&gt;Chain Position 11: Cortex-A7&lt;/P&gt;&lt;P&gt;Chain Position 12: Cortex-A7 PMU&lt;/P&gt;&lt;P&gt;Chain Position 13: CoreSight CTI&lt;/P&gt;&lt;P&gt;Chain Position 14: CoreSight CTI&lt;/P&gt;&lt;P&gt;Chain Position 15: Cortex-A7 ETM&lt;/P&gt;&lt;P&gt;Chain Position 16: Cortex-A7 ETM&lt;/P&gt;&lt;P&gt;Chain Position 17: DAP&lt;/P&gt;&lt;P&gt;Chain Position 18: SAP2&lt;/P&gt;&lt;P&gt;(bin) 48 % ::ccs::all_run_mode&lt;/P&gt;&lt;P&gt;CortexA7: Execute Mode &lt;/P&gt;&lt;P&gt;CortexA7: Execute Mode &lt;/P&gt;&lt;P&gt;(bin) 49 % &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 06:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459967#M3417</guid>
      <dc:creator>jasonhendrix</dc:creator>
      <dc:date>2016-03-09T06:31:27Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459968#M3418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It looks fine. Now, please create a new Bareboard project, make sure Board type is LS1021ATWR, build the project. Open the ccs console and enter log v command, then try to debug the project and provide the ccs log. Also, if you get Can't connect to ccs error at first attempt, try again (I saw "Can't connect to ccs" happens at first attempt).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 09:28:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459968#M3418</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2016-03-09T09:28:21Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459969#M3419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I won't post the log output because it's copious, but more importantly, I hit the breakpoint in main in the new bareboard project.&amp;nbsp; I'll pull at that thread a little bit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 20:44:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459969#M3419</guid>
      <dc:creator>jasonhendrix</dc:creator>
      <dc:date>2016-03-09T20:44:47Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect CCS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459970#M3420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the help, Adrian.&amp;nbsp; I can download and step through my program now.&amp;nbsp; The final steps for me were to restore the debug configuration back to the default config.&amp;nbsp; I still had it set with the JTAG config file for rev 1.&amp;nbsp; I don't know why I couldn't connect when I first created my project and tried to debug.&amp;nbsp; If it had, I wouldn't have learned all this great stuff.&amp;nbsp; I would summarize my lessons learned like so:&lt;/P&gt;&lt;P&gt;* If you're using rev 2 of the LS1021A process on the LS1021A-TWR dev board, the default debug configuration should work&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; * I tested this with projects for both DDR and OCRAM.&lt;/P&gt;&lt;P&gt;* You can use Window's Resource Monitor to verify that CCS is up and has a TCP connection to the TAP&lt;/P&gt;&lt;P&gt;* The TAP OS is also useful - connect to it via telnet or serial over USB&lt;/P&gt;&lt;P&gt;* The CCS console is useful and can be accessed by right-clicking on the icon in the system tray.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 21:05:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459970#M3420</guid>
      <dc:creator>jasonhendrix</dc:creator>
      <dc:date>2016-03-09T21:05:27Z</dc:date>
    </item>
  </channel>
</rss>