<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic debugger problems in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/debugger-problems/m-p/458869#M3379</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am having problems trying to debug in CW 10.6.&amp;nbsp; The program runs when I click "step", it "steps into" when I click "step over", and has other similar issues.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I was first using CW, there were "release" and "debug" configurations, and the file that contained main() was called "processorexpert.c".&amp;nbsp; Now there is only one confuguration, named after the MCU, and the file that contains main() is called main.c.&amp;nbsp; I am worried that optimizer settings are not correct for debugging.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, is there a way to restore factory settings or verify that settings are correct?&amp;nbsp; Should I reinstall CW?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any thoughts would be appreciated.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Dec 2015 22:56:22 GMT</pubDate>
    <dc:creator>unclemike</dc:creator>
    <dc:date>2015-12-03T22:56:22Z</dc:date>
    <item>
      <title>debugger problems</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/debugger-problems/m-p/458869#M3379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am having problems trying to debug in CW 10.6.&amp;nbsp; The program runs when I click "step", it "steps into" when I click "step over", and has other similar issues.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I was first using CW, there were "release" and "debug" configurations, and the file that contained main() was called "processorexpert.c".&amp;nbsp; Now there is only one confuguration, named after the MCU, and the file that contains main() is called main.c.&amp;nbsp; I am worried that optimizer settings are not correct for debugging.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, is there a way to restore factory settings or verify that settings are correct?&amp;nbsp; Should I reinstall CW?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any thoughts would be appreciated.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Dec 2015 22:56:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/debugger-problems/m-p/458869#M3379</guid>
      <dc:creator>unclemike</dc:creator>
      <dc:date>2015-12-03T22:56:22Z</dc:date>
    </item>
    <item>
      <title>Re: debugger problems</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/debugger-problems/m-p/458870#M3380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;we can go to IDE menu "windows", "preference" , then restore default settings for each options.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="2015-12-04_14-47-17.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53118i391373DF928035C9/image-size/large?v=v2&amp;amp;px=999" role="button" title="2015-12-04_14-47-17.jpg" alt="2015-12-04_14-47-17.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can also go to your workspace folder, then remove .metadata folder then restart CW. your CW workspace setting go to default one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can this help you?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Dec 2015 06:50:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/debugger-problems/m-p/458870#M3380</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2015-12-04T06:50:54Z</dc:date>
    </item>
  </channel>
</rss>