<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MK70FN1M0VMJ12 device and code warrior as IDE  in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MK70FN1M0VMJ12-device-and-code-warrior-as-IDE/m-p/447120#M3227</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i'm using MK70FN1M0VMJ12 device and code warrior as IDE when i'm tring to run the code in ram its telling to update the bootload software. Is there any setting which i have to do. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Jul 2015 10:44:41 GMT</pubDate>
    <dc:creator>ankurchauhan</dc:creator>
    <dc:date>2015-07-01T10:44:41Z</dc:date>
    <item>
      <title>MK70FN1M0VMJ12 device and code warrior as IDE </title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MK70FN1M0VMJ12-device-and-code-warrior-as-IDE/m-p/447120#M3227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i'm using MK70FN1M0VMJ12 device and code warrior as IDE when i'm tring to run the code in ram its telling to update the bootload software. Is there any setting which i have to do. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2015 10:44:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MK70FN1M0VMJ12-device-and-code-warrior-as-IDE/m-p/447120#M3227</guid>
      <dc:creator>ankurchauhan</dc:creator>
      <dc:date>2015-07-01T10:44:41Z</dc:date>
    </item>
    <item>
      <title>Re:  MK70FN1M0VMJ12 device and code warrior as IDE</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MK70FN1M0VMJ12-device-and-code-warrior-as-IDE/m-p/447121#M3228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ankur Chauhan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this the message you get?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61157iBE81FE3855925167/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If yes, then you need to unplug the USB cable and place a jumper on the J10 connector in your tower K70 board and connect the USB cable again, this way the OSJTAG will enter to bootloader mode and the latest firmware will be programmed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After the firmware has been updated you should see a window like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61158i9EB493F74F4481EF/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now you should unplug the USB cable, remove the jumper from the J10 connector and connect the USB cable again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Carlos Mendoza&lt;/P&gt;&lt;P&gt;Technical Support Engineer&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2015 21:06:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MK70FN1M0VMJ12-device-and-code-warrior-as-IDE/m-p/447121#M3228</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2015-07-01T21:06:52Z</dc:date>
    </item>
  </channel>
</rss>