<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: Codewarrior tap status wrong</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-tap-status-wrong/m-p/437025#M3073</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes,I have two cwtaps,but i have only one probe,the probe is JTAG/COP has a 16-pin connector.I used the other cwtap,the error still happened.I will try to buy another probe to test.Thank you for your answer!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Aug 2015 08:02:54 GMT</pubDate>
    <dc:creator>hxmh</dc:creator>
    <dc:date>2015-08-14T08:02:54Z</dc:date>
    <item>
      <title>Codewarrior tap status wrong</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-tap-status-wrong/m-p/437022#M3070</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, i have bought a codewarrior tap newly,but it could not be connected to the p1010 board. I used CCS to get the codewarrior tap status ,the error shows in the pic.The Probe Tip i used is CWH-CTP-COP-YE,it is also newly bought. Can you tell me what is wrong?Thank you!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120540i6D6A231DA652FA65/image-size/large?v=v2&amp;amp;px=999" title="63045_63045.jpg" alt="63045_63045.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52424iCF477424C3F28473/image-size/large?v=v2&amp;amp;px=999" title="image.jpg" alt="image.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2015 01:45:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-tap-status-wrong/m-p/437022#M3070</guid>
      <dc:creator>hxmh</dc:creator>
      <dc:date>2015-08-13T01:45:05Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior tap status wrong</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-tap-status-wrong/m-p/437023#M3071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the info it seems you're using CW for PA V10.5.&lt;/P&gt;&lt;P&gt;Am I right ?&lt;/P&gt;&lt;P&gt;You're using CodeWarrior TAP + CWH-CTP-COP-YE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know what the error ERROR:1567016 means but:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; JTAG/COP probe has a 16-pin connector&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; OnCE probe has a 14-pin connector&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; BDM probe has a 26-pin connector&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you tried with a demo example created with the Project wizard (File + New) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Aug 2015 07:28:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-tap-status-wrong/m-p/437023#M3071</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-08-14T07:28:43Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior tap status wrong</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-tap-status-wrong/m-p/437024#M3072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try to update the cwtap OS, it could help. To do that, in ccs console enter the command:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;updatecwtap --force fsl037000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If updating cwtap doesn't help, I'm pretty sure it is a problem with the Probe, because when you have no probe connected to cwtap you don't get this error. Do you have additional probe to test?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Aug 2015 07:48:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-tap-status-wrong/m-p/437024#M3072</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2015-08-14T07:48:45Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior tap status wrong</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-tap-status-wrong/m-p/437025#M3073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes,I have two cwtaps,but i have only one probe,the probe is JTAG/COP has a 16-pin connector.I used the other cwtap,the error still happened.I will try to buy another probe to test.Thank you for your answer!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Aug 2015 08:02:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-tap-status-wrong/m-p/437025#M3073</guid>
      <dc:creator>hxmh</dc:creator>
      <dc:date>2015-08-14T08:02:54Z</dc:date>
    </item>
  </channel>
</rss>