<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: How can I download the SPI Sample Code for the K60 MCU ?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-can-I-download-the-SPI-Sample-Code-for-the-K60-MCU/m-p/261131#M278</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You must install CW for MCU v10.5 and MQX V4.0.2 (these are the last versions).&lt;/P&gt;&lt;P&gt;Under MQX installation, please have a look to:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - the folder \Freescale_MQX_4_0_2\doc\tools\cw -&amp;gt; the manual FSL_MQX_in_CW_10_x.pdf,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - the folder \Freescale_MQX_4_0_2\doc -&amp;gt; FSL_MQX_release_notes.pdf&lt;/P&gt;&lt;P&gt;the user_config.h will allow you to enable or not the BSP functions.&lt;/P&gt;&lt;P&gt;++++++++++++++++&lt;/P&gt;&lt;P&gt;extract of Manual&lt;/P&gt;&lt;P&gt;SPI I/O Driver&lt;/P&gt;&lt;P&gt;This driver supports the operation master mode. If enabled in user configuration, the SPI device drivers are installed during the BSP startup code as “spi0:” (or “spiX:” where X is index of the SPI module used). The SPI driver is significantly rewritten in the MQX 4.0, so that there is no distinct interrupt or polled driver type. See I/O User Guide for details. On Kinetis and Vybrid platforms, the driver uses DMA to function.&lt;/P&gt;&lt;P&gt;++++++++++++++++&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an example for SPI ... under Basic example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Jan 2014 13:57:54 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2014-01-30T13:57:54Z</dc:date>
    <item>
      <title>How can I download the SPI Sample Code for the K60 MCU ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-can-I-download-the-SPI-Sample-Code-for-the-K60-MCU/m-p/261130#M277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the CW to generate the BSP for the TWR-K60D100M module.&amp;nbsp; I need to add the SPI driver component in the BSP.&amp;nbsp; How can I do it ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jan 2014 23:47:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-can-I-download-the-SPI-Sample-Code-for-the-K60-MCU/m-p/261130#M277</guid>
      <dc:creator>johnng</dc:creator>
      <dc:date>2014-01-27T23:47:41Z</dc:date>
    </item>
    <item>
      <title>Re: How can I download the SPI Sample Code for the K60 MCU ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-can-I-download-the-SPI-Sample-Code-for-the-K60-MCU/m-p/261131#M278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You must install CW for MCU v10.5 and MQX V4.0.2 (these are the last versions).&lt;/P&gt;&lt;P&gt;Under MQX installation, please have a look to:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - the folder \Freescale_MQX_4_0_2\doc\tools\cw -&amp;gt; the manual FSL_MQX_in_CW_10_x.pdf,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - the folder \Freescale_MQX_4_0_2\doc -&amp;gt; FSL_MQX_release_notes.pdf&lt;/P&gt;&lt;P&gt;the user_config.h will allow you to enable or not the BSP functions.&lt;/P&gt;&lt;P&gt;++++++++++++++++&lt;/P&gt;&lt;P&gt;extract of Manual&lt;/P&gt;&lt;P&gt;SPI I/O Driver&lt;/P&gt;&lt;P&gt;This driver supports the operation master mode. If enabled in user configuration, the SPI device drivers are installed during the BSP startup code as “spi0:” (or “spiX:” where X is index of the SPI module used). The SPI driver is significantly rewritten in the MQX 4.0, so that there is no distinct interrupt or polled driver type. See I/O User Guide for details. On Kinetis and Vybrid platforms, the driver uses DMA to function.&lt;/P&gt;&lt;P&gt;++++++++++++++++&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an example for SPI ... under Basic example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jan 2014 13:57:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-can-I-download-the-SPI-Sample-Code-for-the-K60-MCU/m-p/261131#M278</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-01-30T13:57:54Z</dc:date>
    </item>
  </channel>
</rss>