<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC9S12XEP100/Data Flash in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MC9S12XEP100-Data-Flash/m-p/417112#M2773</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rasika,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Processor Expert proposes the following option:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A name="SetByte"&gt;&lt;/A&gt;&lt;STRONG&gt;SetByte&lt;/STRONG&gt; - This method writes a given byte to a specified address in EEPROM. The method also sets address pointer for &lt;A href="#SetActByte"&gt;SetActByte&lt;/A&gt; and &lt;A href="#GetActByte"&gt;GetActByte&lt;/A&gt; methods (applicable only if these methods are enabled). The pointer is set to address passed as the parameter.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A name="GetByte"&gt;&lt;/A&gt;&lt;STRONG&gt;GetByte&lt;/STRONG&gt; - This method reads a byte from a specified EEPROM address. The method also sets address pointer for &lt;A href="#SetActByte"&gt;SetActByte&lt;/A&gt; and &lt;A href="#GetActByte"&gt;GetActByte&lt;/A&gt; methods (applicable only if these methods are enabled). The pointer is set to address passed as the parameter.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A name="SetWord"&gt;&lt;/A&gt;&lt;STRONG&gt;SetWord&lt;/STRONG&gt; - This method writes a given word (2 bytes) to the specified address in EEPROM. The method also sets address pointer for &lt;A href="#SetActByte"&gt;SetActByte&lt;/A&gt; and &lt;A href="#GetActByte"&gt;GetActByte&lt;/A&gt; methods (applicable only if these methods are enabled). The pointer is set to address passed as the parameter + 1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A name="GetWord"&gt;&lt;/A&gt;&lt;STRONG&gt;GetWord&lt;/STRONG&gt; - This method reads a word (2 bytes) from the specified EEPROM address. The method also sets address pointer for &lt;A href="#SetActByte"&gt;SetActByte&lt;/A&gt; and &lt;A href="#GetActByte"&gt;GetActByte&lt;/A&gt; methods (applicable only if these methods are enabled). The pointer is set to address passed as the parameter + 1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A name="SetLong"&gt;&lt;/A&gt;&lt;STRONG&gt;SetLong&lt;/STRONG&gt; - This method writes a given long word (4 bytes) to the specified address in EEPROM. The method also sets address pointer for &lt;A href="#SetActByte"&gt;SetActByte&lt;/A&gt; and &lt;A href="#GetActByte"&gt;GetActByte&lt;/A&gt; methods (applicable only if these methods are enabled). The pointer is set to address passed as the parameter + 3.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A name="GetLong"&gt;&lt;/A&gt;&lt;STRONG&gt;GetLong&lt;/STRONG&gt; - This method reads a long word (4 bytes) from the specified EEPROM address. The method also sets address pointer for &lt;A href="#SetActByte"&gt;SetActByte&lt;/A&gt; and &lt;A href="#GetActByte"&gt;GetActByte&lt;/A&gt; methods (applicable only if these methods are enabled). The pointer is set to address passed as the parameter + 3.&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SetLong writes 4 bytes in 1 time.&lt;/P&gt;&lt;P&gt;We don't have other option using the Processor Expert IntEEPROM.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Sep 2015 13:02:29 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2015-09-10T13:02:29Z</dc:date>
    <item>
      <title>MC9S12XEP100/Data Flash</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MC9S12XEP100-Data-Flash/m-p/417108#M2769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all!!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using MC9S12XEP100 board. I want to use Data Flash feature to write say 100 bytes and read it back from data flash in PE enabled environment. How to do that?? Please help!! &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2015 05:09:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MC9S12XEP100-Data-Flash/m-p/417108#M2769</guid>
      <dc:creator>rasika</dc:creator>
      <dc:date>2015-06-02T05:09:47Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12XEP100/Data Flash</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MC9S12XEP100-Data-Flash/m-p/417109#M2770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just see this question.&lt;/P&gt;&lt;P&gt;It seems to be old one.&lt;/P&gt;&lt;P&gt;Is it still open ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Sep 2015 09:45:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MC9S12XEP100-Data-Flash/m-p/417109#M2770</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-09-09T09:45:17Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12XEP100/Data Flash</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MC9S12XEP100-Data-Flash/m-p/417110#M2771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pascal,&lt;/P&gt;&lt;P&gt;Yes!! It is still open. It will be a great help if you can answer with steps to follow..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Sep 2015 10:59:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MC9S12XEP100-Data-Flash/m-p/417110#M2771</guid>
      <dc:creator>rasika</dc:creator>
      <dc:date>2015-09-09T10:59:48Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12XEP100/Data Flash</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MC9S12XEP100-Data-Flash/m-p/417111#M2772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rasika,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ok.&lt;/P&gt;&lt;P&gt;If you're using Processor Expert (PEx) I think you want to use the IntEEPROM (Internal EEPROM) bean.&lt;/P&gt;&lt;P&gt;If it's not the case let me know.&lt;/P&gt;&lt;P&gt;Some Information associated to the bean:&lt;/P&gt;&lt;P&gt;+++++++++++++++&lt;/P&gt;&lt;P&gt;&lt;STRONG class="VSP"&gt;Version specific information for HCS12X derivatives that supports Emulated EEPROM feature &lt;/STRONG&gt;&lt;/P&gt;&lt;P class="text_title"&gt;D-Flash and buffer RAM Memory&lt;/P&gt;&lt;P&gt;Before Emulated EEPROM can be used, D-Flash and Buffer RAM area must be partitioned. Partitions are defined by &lt;A&gt;Emulated EEPROM&lt;/A&gt; properties (see help of the properties). Partitioning will not take effect unless &lt;A&gt;Partition&lt;/A&gt; method is called or &lt;A&gt;Partition D-flash in init&lt;/A&gt; property is set (Partitions can be created only in special mode).&lt;/P&gt;&lt;P&gt;The range of addressess selected in &lt;A&gt;Address range&lt;/A&gt; properties is checked when writting to corresponding area. The other memory range is set to maximum available memory, i.e. when &lt;A&gt;Address range&lt;/A&gt; targets to D-Flash (D-Flash begins at global address 0x100000) then selected range is checked on all writes to D-Flash, but maximum available buffer RAM range is checked on all writes to buffer RAM (end of Buffer RAM is at global address 0x13FFFF). And vice versa, when &lt;A&gt;Address range&lt;/A&gt; targets to Buffer RAM then selected range is checked on all writes to Buffer RAM, but maximum available D-Flash range is checked on all writes to D-Flash. Size of buffer ram for Emulated EEPROM area is defined only by the property "Buffer RAM sector count for Emulated EEPROM (ERPART)".&lt;/P&gt;&lt;P&gt;&lt;A&gt;EraseEeprom&lt;/A&gt; method doesn't implement mass erase. Sector erase is used instead. The method erases all available sectors for D-Flash user partition.&lt;/P&gt;&lt;P&gt;The memory type the component is writing to (D-Flash or Emulated EEPROM - buffer RAM) is determined by an Address passed as the parameter of SetXX/GetXX methods. If the address targets to the buffer RAM, simple write to a RAM memory is performed and completed on exit of the write method, i.e. waiting settings selected by &lt;A&gt;SetWait&lt;/A&gt; method or &lt;A&gt;Wait enabled in init.&lt;/A&gt; property is not used (ignored) and Busy method returns always FALSE. When a write to Buffer RAM (Emulated EEPROM) occurs, interrupts are not used and &lt;A&gt;OnWriteEnd&lt;/A&gt; and &lt;A&gt;OnWritePageEnd&lt;/A&gt; events are not invoked.&lt;/P&gt;&lt;P&gt;+++++++++++++++&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't have specific example on my hand.&lt;/P&gt;&lt;P&gt;I need to work on it.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Sep 2015 15:47:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MC9S12XEP100-Data-Flash/m-p/417111#M2772</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-09-09T15:47:51Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12XEP100/Data Flash</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MC9S12XEP100-Data-Flash/m-p/417112#M2773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rasika,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Processor Expert proposes the following option:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A name="SetByte"&gt;&lt;/A&gt;&lt;STRONG&gt;SetByte&lt;/STRONG&gt; - This method writes a given byte to a specified address in EEPROM. The method also sets address pointer for &lt;A href="#SetActByte"&gt;SetActByte&lt;/A&gt; and &lt;A href="#GetActByte"&gt;GetActByte&lt;/A&gt; methods (applicable only if these methods are enabled). The pointer is set to address passed as the parameter.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A name="GetByte"&gt;&lt;/A&gt;&lt;STRONG&gt;GetByte&lt;/STRONG&gt; - This method reads a byte from a specified EEPROM address. The method also sets address pointer for &lt;A href="#SetActByte"&gt;SetActByte&lt;/A&gt; and &lt;A href="#GetActByte"&gt;GetActByte&lt;/A&gt; methods (applicable only if these methods are enabled). The pointer is set to address passed as the parameter.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A name="SetWord"&gt;&lt;/A&gt;&lt;STRONG&gt;SetWord&lt;/STRONG&gt; - This method writes a given word (2 bytes) to the specified address in EEPROM. The method also sets address pointer for &lt;A href="#SetActByte"&gt;SetActByte&lt;/A&gt; and &lt;A href="#GetActByte"&gt;GetActByte&lt;/A&gt; methods (applicable only if these methods are enabled). The pointer is set to address passed as the parameter + 1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A name="GetWord"&gt;&lt;/A&gt;&lt;STRONG&gt;GetWord&lt;/STRONG&gt; - This method reads a word (2 bytes) from the specified EEPROM address. The method also sets address pointer for &lt;A href="#SetActByte"&gt;SetActByte&lt;/A&gt; and &lt;A href="#GetActByte"&gt;GetActByte&lt;/A&gt; methods (applicable only if these methods are enabled). The pointer is set to address passed as the parameter + 1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A name="SetLong"&gt;&lt;/A&gt;&lt;STRONG&gt;SetLong&lt;/STRONG&gt; - This method writes a given long word (4 bytes) to the specified address in EEPROM. The method also sets address pointer for &lt;A href="#SetActByte"&gt;SetActByte&lt;/A&gt; and &lt;A href="#GetActByte"&gt;GetActByte&lt;/A&gt; methods (applicable only if these methods are enabled). The pointer is set to address passed as the parameter + 3.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A name="GetLong"&gt;&lt;/A&gt;&lt;STRONG&gt;GetLong&lt;/STRONG&gt; - This method reads a long word (4 bytes) from the specified EEPROM address. The method also sets address pointer for &lt;A href="#SetActByte"&gt;SetActByte&lt;/A&gt; and &lt;A href="#GetActByte"&gt;GetActByte&lt;/A&gt; methods (applicable only if these methods are enabled). The pointer is set to address passed as the parameter + 3.&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SetLong writes 4 bytes in 1 time.&lt;/P&gt;&lt;P&gt;We don't have other option using the Processor Expert IntEEPROM.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Sep 2015 13:02:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MC9S12XEP100-Data-Flash/m-p/417112#M2773</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-09-10T13:02:29Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12XEP100/Data Flash</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MC9S12XEP100-Data-Flash/m-p/417113#M2774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pascal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the information associated with IntEEPROM bean and the mentioned methods.&lt;/P&gt;&lt;P&gt;I will study and give a try with above information. Will let you know once I succeed in it. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you so much for your help&lt;SPAN style="line-height: 1.5;"&gt;. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5;"&gt;Rasika.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Sep 2015 08:40:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MC9S12XEP100-Data-Flash/m-p/417113#M2774</guid>
      <dc:creator>rasika</dc:creator>
      <dc:date>2015-09-11T08:40:23Z</dc:date>
    </item>
  </channel>
</rss>