<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: cwide.exe has  stopped working in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/cwide-exe-has-stopped-working/m-p/415614#M2754</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ever had one customer met similar problem with CW.&lt;/P&gt;&lt;P&gt;It seems that this issue is caused by a installation problem. Or, conflicting with anti-virus would also cause such a problem.&lt;/P&gt;&lt;P&gt;so, may I propose a re-installing of the application from scratch? A repair install may not do the job.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Aug 2015 02:56:51 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2015-08-11T02:56:51Z</dc:date>
    <item>
      <title>cwide.exe has  stopped working</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/cwide-exe-has-stopped-working/m-p/415613#M2753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use CodeWarrior version 10.8.3 on windows 8. I used it as simulator and has problemthat&amp;nbsp; when run the code with&amp;nbsp; trace And profile.&lt;/P&gt;&lt;P&gt;At the end of run appear a message "cwide.exe has&amp;nbsp; stopped working"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2015 05:40:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/cwide-exe-has-stopped-working/m-p/415613#M2753</guid>
      <dc:creator>yaakovbar-on</dc:creator>
      <dc:date>2015-08-06T05:40:42Z</dc:date>
    </item>
    <item>
      <title>Re: cwide.exe has  stopped working</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/cwide-exe-has-stopped-working/m-p/415614#M2754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ever had one customer met similar problem with CW.&lt;/P&gt;&lt;P&gt;It seems that this issue is caused by a installation problem. Or, conflicting with anti-virus would also cause such a problem.&lt;/P&gt;&lt;P&gt;so, may I propose a re-installing of the application from scratch? A repair install may not do the job.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 02:56:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/cwide-exe-has-stopped-working/m-p/415614#M2754</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2015-08-11T02:56:51Z</dc:date>
    </item>
  </channel>
</rss>