<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックImporting a CW2.5 project ?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Importing-a-CW2-5-project/m-p/408405#M2595</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to import a CW 2.5 project into CW10.6.4 ? This is for a MCF5272.&amp;nbsp; When I try to open the .mcp &lt;/P&gt;&lt;P&gt;file it says the tool chain is not supported. But I can create new MCF5272 projects (and build them) so I have the tools.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;--jschimpf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Oct 2015 18:45:33 GMT</pubDate>
    <dc:creator>jschimpf</dc:creator>
    <dc:date>2015-10-19T18:45:33Z</dc:date>
    <item>
      <title>Importing a CW2.5 project ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Importing-a-CW2-5-project/m-p/408405#M2595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to import a CW 2.5 project into CW10.6.4 ? This is for a MCF5272.&amp;nbsp; When I try to open the .mcp &lt;/P&gt;&lt;P&gt;file it says the tool chain is not supported. But I can create new MCF5272 projects (and build them) so I have the tools.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;--jschimpf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Oct 2015 18:45:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Importing-a-CW2-5-project/m-p/408405#M2595</guid>
      <dc:creator>jschimpf</dc:creator>
      <dc:date>2015-10-19T18:45:33Z</dc:date>
    </item>
    <item>
      <title>Re: Importing a CW2.5 project ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Importing-a-CW2-5-project/m-p/408406#M2596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;The Project Importer in v10.6 only supports DSC products.&lt;BR /&gt; &lt;BR /&gt; For other products, the solution is to create a new bareboard project in CW10.6.4, and then add/copy all your source files to the new project. This is the cleanest way to import a project. Below is an application note for how to do this:&lt;BR /&gt; &lt;BR /&gt; &lt;/SPAN&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;&lt;A href="http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf"&gt;http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;&lt;BR /&gt; &lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fiona Kuang&lt;/P&gt;&lt;P&gt;Technical Information &amp;amp; Commercial Support&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Oct 2015 06:00:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Importing-a-CW2-5-project/m-p/408406#M2596</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2015-10-20T06:00:40Z</dc:date>
    </item>
    <item>
      <title>Re: Importing a CW2.5 project ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Importing-a-CW2-5-project/m-p/408407#M2597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jim,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As explained Fiona the imported is working for DSC projects only.&lt;/P&gt;&lt;P&gt;You're using a CodeWarrior development tool for Coldfire devices.&lt;/P&gt;&lt;P&gt;If the version used is really V2.5, it's a very very old version probably named CW for E68K V2.5.&lt;/P&gt;&lt;P&gt;This version was released in 2001.&lt;/P&gt;&lt;P&gt;Jump to MCU V10.6.4 could be not very easy. May be the jump is too important.&lt;/P&gt;&lt;P&gt;The Doc "&lt;A href="http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf" title="http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf"&gt;http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf&lt;/A&gt; " was based on the last Classic version.&lt;/P&gt;&lt;P&gt;For Coldfire it was CW for ColdFire V7.2 released end of 2009.&lt;/P&gt;&lt;P&gt;Jumping from V2.5 to V7.2 could be not easy as there are lot of changes: EWL, etc ...&lt;/P&gt;&lt;P&gt;You can refer to the 2 TNs attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know if there is a best way to convert an old project to last Eclipse version.&lt;/P&gt;&lt;P&gt;May be the you can follow the process provided in the AN.&lt;/P&gt;&lt;P&gt;Else if it's not working, another solution could be to split the operation:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - move from V2.5 to V7.2,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - move V7.2 to MCU V10.6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Oct 2015 08:03:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Importing-a-CW2-5-project/m-p/408407#M2597</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-10-20T08:03:49Z</dc:date>
    </item>
  </channel>
</rss>