<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: error while initialization of PE  in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/error-while-initialization-of-PE/m-p/403062#M2531</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi KDN.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;processor expert use its own generated header file IO_Map.c for MCU IO registers defination.&lt;/P&gt;&lt;P&gt;while NON- processor expert project use mcu header file such as mc9s12xhz.c for the same purpose.&lt;/P&gt;&lt;P&gt;because both of these two files are for MCU registers definition, they can't coexist in the same project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I often see similar problem as yours when customer porting non-pe project to pe project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you use processor expert, please remove mc9s12xhz.c and mc9s12xhz.h from your project. this can avoid the conflict.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can this help?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Jul 2015 02:09:50 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2015-07-14T02:09:50Z</dc:date>
    <item>
      <title>error while initialization of PE</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/error-while-initialization-of-PE/m-p/403061#M2530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;why this error coming when I am trying to use processor expert&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="49758_49758.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120475i0F86EE1913C797BF/image-size/large?v=v2&amp;amp;px=999" role="button" title="49758_49758.JPG" alt="49758_49758.JPG" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="error.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54574i0A80D15BF4022E38/image-size/large?v=v2&amp;amp;px=999" role="button" title="error.JPG" alt="error.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Jul 2015 15:59:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/error-while-initialization-of-PE/m-p/403061#M2530</guid>
      <dc:creator>kdn</dc:creator>
      <dc:date>2015-07-11T15:59:29Z</dc:date>
    </item>
    <item>
      <title>Re: error while initialization of PE</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/error-while-initialization-of-PE/m-p/403062#M2531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi KDN.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;processor expert use its own generated header file IO_Map.c for MCU IO registers defination.&lt;/P&gt;&lt;P&gt;while NON- processor expert project use mcu header file such as mc9s12xhz.c for the same purpose.&lt;/P&gt;&lt;P&gt;because both of these two files are for MCU registers definition, they can't coexist in the same project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I often see similar problem as yours when customer porting non-pe project to pe project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you use processor expert, please remove mc9s12xhz.c and mc9s12xhz.h from your project. this can avoid the conflict.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can this help?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2015 02:09:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/error-while-initialization-of-PE/m-p/403062#M2531</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2015-07-14T02:09:50Z</dc:date>
    </item>
  </channel>
</rss>