<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックPORTA question - frdm-kl26z</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/PORTA-question-frdm-kl26z/m-p/400157#M2490</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to use PTA1 gpio as an input pin and want the pin output to be 0. But by default it is high. It was used for LPSCI configuration and I have disabled it and used it as an input pin.&lt;/P&gt;&lt;P&gt;I have made sure, it used as a gpiopin and then used it as an input pin in the code. Could someone please advice why is pin high by default.&lt;/P&gt;&lt;P&gt;The schematic says ,the pin is used for UART1_TX which I have disabled it.&lt;/P&gt;&lt;P&gt;Here goes my piece of code.&lt;/P&gt;&lt;P&gt;PORT_HAL_SetMuxMode(PORTA,1u,kPortMuxAsGpio); and have used gpio river to set it as input pin.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Jayanth BR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Oct 2015 02:51:29 GMT</pubDate>
    <dc:creator>jayanthvasisht</dc:creator>
    <dc:date>2015-10-15T02:51:29Z</dc:date>
    <item>
      <title>PORTA question - frdm-kl26z</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/PORTA-question-frdm-kl26z/m-p/400157#M2490</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to use PTA1 gpio as an input pin and want the pin output to be 0. But by default it is high. It was used for LPSCI configuration and I have disabled it and used it as an input pin.&lt;/P&gt;&lt;P&gt;I have made sure, it used as a gpiopin and then used it as an input pin in the code. Could someone please advice why is pin high by default.&lt;/P&gt;&lt;P&gt;The schematic says ,the pin is used for UART1_TX which I have disabled it.&lt;/P&gt;&lt;P&gt;Here goes my piece of code.&lt;/P&gt;&lt;P&gt;PORT_HAL_SetMuxMode(PORTA,1u,kPortMuxAsGpio); and have used gpio river to set it as input pin.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Jayanth BR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Oct 2015 02:51:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/PORTA-question-frdm-kl26z/m-p/400157#M2490</guid>
      <dc:creator>jayanthvasisht</dc:creator>
      <dc:date>2015-10-15T02:51:29Z</dc:date>
    </item>
    <item>
      <title>Re: PORTA question - frdm-kl26z</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/PORTA-question-frdm-kl26z/m-p/400158#M2491</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I could figure out the reason. It is connected to the opensda mcu via usb chip and is pulled high. Will be closing the question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jayanth BR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2015 02:29:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/PORTA-question-frdm-kl26z/m-p/400158#M2491</guid>
      <dc:creator>jayanthvasisht</dc:creator>
      <dc:date>2015-10-16T02:29:34Z</dc:date>
    </item>
  </channel>
</rss>