<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: get error with Code Warrior 7.2 saying won't run on Windows 64 bit</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/get-error-with-Code-Warrior-7-2-saying-won-t-run-on-Windows-64/m-p/394278#M2409</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Keith,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We've 2 versions supporting the Coldfire V2 to V4 cores:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - CW for Coldfire V7.2 which is based on classic version and was released in 2010,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - CW for MCU V10.6.4 which is&amp;nbsp; based on Eclipse and released middle of 2015.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We recommend to use the last version CW for MCU V10.6.4.&lt;/P&gt;&lt;P&gt;Now if you want to us the classic version, it's possible but this product was designed for XP 32bit OS and the installer is checking the OS type.&lt;/P&gt;&lt;P&gt;The installer detects if 64 bit OS is used and generates an error.&lt;/P&gt;&lt;P&gt;To install it you need to:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - install the tool on 32 bit OS,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - copy the installation folder under your Win 7 64 bit PC,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - execute the \bin\regserver.bat file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some drivers installed are not compatible with 64 bit OS.&lt;/P&gt;&lt;P&gt;This is the case of P&amp;amp;E drivers.&lt;/P&gt;&lt;P&gt;On their web site you can download a new driver version.&lt;/P&gt;&lt;P&gt;Click on &lt;A href="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=163" title="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=163"&gt;P&amp;amp;E Microcomputer Systems - USB-ML-CFE (Discontinued) - USB BDM Interface cable for the ColdFire V2/V3/V4 (Discontinue…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Select FAQs, Manuals &amp;amp; Downloads Tab.&lt;/P&gt;&lt;P&gt;you can download the last driver version 12.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can access it via the FAQ:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/faqs/faq_view.cfm?id=211" title="http://www.pemicro.com/faqs/faq_view.cfm?id=211"&gt;P&amp;amp;E Microcomputer Systems&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you've problem you can refer to the &lt;A href="http://www.pemicro.com/faqs/faq_view.cfm?id=29" title="http://www.pemicro.com/faqs/faq_view.cfm?id=29"&gt;http://www.pemicro.com/faqs/faq_view.cfm?id=29&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/faqs/faq_view.cfm?id=29" title="http://www.pemicro.com/faqs/faq_view.cfm?id=29"&gt;P&amp;amp;E Microcomputer Systems&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hope this will help you.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Nov 2015 15:39:25 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2015-11-09T15:39:25Z</dc:date>
    <item>
      <title>get error with Code Warrior 7.2 saying won't run on Windows 64 bit</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/get-error-with-Code-Warrior-7-2-saying-won-t-run-on-Windows-64/m-p/394277#M2408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just downloaded Code Warrior for Freescale V7.2 and tried running. During installation, says won't run on 64-bit OS. I am using Windows 7.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can this be worked around? Are they telling me we have to run a mediocre CPU or in a VM?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the help. I'm new to Freescale but have used many other ARM chipsets.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Keith Rhodes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 08 Nov 2015 22:43:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/get-error-with-Code-Warrior-7-2-saying-won-t-run-on-Windows-64/m-p/394277#M2408</guid>
      <dc:creator>keithrhodes</dc:creator>
      <dc:date>2015-11-08T22:43:00Z</dc:date>
    </item>
    <item>
      <title>Re: get error with Code Warrior 7.2 saying won't run on Windows 64 bit</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/get-error-with-Code-Warrior-7-2-saying-won-t-run-on-Windows-64/m-p/394278#M2409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Keith,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We've 2 versions supporting the Coldfire V2 to V4 cores:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - CW for Coldfire V7.2 which is based on classic version and was released in 2010,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - CW for MCU V10.6.4 which is&amp;nbsp; based on Eclipse and released middle of 2015.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We recommend to use the last version CW for MCU V10.6.4.&lt;/P&gt;&lt;P&gt;Now if you want to us the classic version, it's possible but this product was designed for XP 32bit OS and the installer is checking the OS type.&lt;/P&gt;&lt;P&gt;The installer detects if 64 bit OS is used and generates an error.&lt;/P&gt;&lt;P&gt;To install it you need to:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - install the tool on 32 bit OS,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - copy the installation folder under your Win 7 64 bit PC,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - execute the \bin\regserver.bat file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some drivers installed are not compatible with 64 bit OS.&lt;/P&gt;&lt;P&gt;This is the case of P&amp;amp;E drivers.&lt;/P&gt;&lt;P&gt;On their web site you can download a new driver version.&lt;/P&gt;&lt;P&gt;Click on &lt;A href="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=163" title="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=163"&gt;P&amp;amp;E Microcomputer Systems - USB-ML-CFE (Discontinued) - USB BDM Interface cable for the ColdFire V2/V3/V4 (Discontinue…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Select FAQs, Manuals &amp;amp; Downloads Tab.&lt;/P&gt;&lt;P&gt;you can download the last driver version 12.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can access it via the FAQ:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/faqs/faq_view.cfm?id=211" title="http://www.pemicro.com/faqs/faq_view.cfm?id=211"&gt;P&amp;amp;E Microcomputer Systems&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you've problem you can refer to the &lt;A href="http://www.pemicro.com/faqs/faq_view.cfm?id=29" title="http://www.pemicro.com/faqs/faq_view.cfm?id=29"&gt;http://www.pemicro.com/faqs/faq_view.cfm?id=29&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/faqs/faq_view.cfm?id=29" title="http://www.pemicro.com/faqs/faq_view.cfm?id=29"&gt;P&amp;amp;E Microcomputer Systems&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hope this will help you.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Nov 2015 15:39:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/get-error-with-Code-Warrior-7-2-saying-won-t-run-on-Windows-64/m-p/394278#M2409</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-11-09T15:39:25Z</dc:date>
    </item>
  </channel>
</rss>