<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development Tools中的主题 Command line compilation for MPC5606B</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-line-compilation-for-MPC5606B/m-p/384923#M2261</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to download CodeWarrior without the IDE? I only want the command line tools e.g. mwcceppc and the include folders that come with it. If this is not possible, what are some alternative tool chains to compile, build for MPC5606B powerpc? Is there a popular GCC variant?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Nov 2014 20:54:03 GMT</pubDate>
    <dc:creator>swarooph</dc:creator>
    <dc:date>2014-11-06T20:54:03Z</dc:date>
    <item>
      <title>Command line compilation for MPC5606B</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-line-compilation-for-MPC5606B/m-p/384923#M2261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to download CodeWarrior without the IDE? I only want the command line tools e.g. mwcceppc and the include folders that come with it. If this is not possible, what are some alternative tool chains to compile, build for MPC5606B powerpc? Is there a popular GCC variant?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Nov 2014 20:54:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-line-compilation-for-MPC5606B/m-p/384923#M2261</guid>
      <dc:creator>swarooph</dc:creator>
      <dc:date>2014-11-06T20:54:03Z</dc:date>
    </item>
    <item>
      <title>Re: Command line compilation for MPC5606B</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-line-compilation-for-MPC5606B/m-p/384924#M2262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The download includes the IDE, but you do not have to use it.&lt;/P&gt;&lt;P&gt;If you download CodeWarrior, it comes with command line tools and include folders/libraries/etc.&lt;/P&gt;&lt;P&gt;Simply use these tools and not the IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Nov 2014 04:32:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-line-compilation-for-MPC5606B/m-p/384924#M2262</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-11-07T04:32:50Z</dc:date>
    </item>
    <item>
      <title>Re: Command line compilation for MPC5606B</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-line-compilation-for-MPC5606B/m-p/384925#M2263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;in addition to Erich info.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are 2 dev tools supporting MPC5606B:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - CW for MPC55xx/56xx V2.10 based on classic IDE,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MPC55XX_56XX&amp;amp;tid=CWH" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MPC55XX_56XX&amp;amp;tid=CWH"&gt;CodeWarrior Dev Tools for MPC55xx/MPC56xx|Freescale&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - CW for MCU V10.6 based on Eclipse.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&amp;amp;tid=CWH" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&amp;amp;tid=CWH"&gt;CodeWarrior for Microcontrollers-Eclipse IDE|Freescale&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We don't have standalone version.&lt;/P&gt;&lt;P&gt;However you can use a make file (a .bat file) to build your application without using the IDE/Ecipse.&lt;/P&gt;&lt;P&gt;The V2.10 includes an interesting doc listing all options available on IDE and corresponding for CMD.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Refer to the AN4094 attached ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached you will find an example using a bat file.&lt;/P&gt;&lt;P&gt;I've tested this example on MPC V2.10.&lt;/P&gt;&lt;P&gt;But it should work (the bat file) on MCU v10.6 too.&lt;/P&gt;&lt;P&gt;To be running you must edit the test.bat and change the folder according to your installation path.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hope this will help you&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal Irrle&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Nov 2014 08:48:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-line-compilation-for-MPC5606B/m-p/384925#M2263</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-11-07T08:48:27Z</dc:date>
    </item>
    <item>
      <title>Re: Command line compilation for MPC5606B</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-line-compilation-for-MPC5606B/m-p/384926#M2264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pascal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the detailed answer. As Erich says, I know that IDE installation comes with command line utilities. I guess there is no way then to download only the command line utilities. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please confirm if any of the options you mentioned are free to download without purchase? CW (Special Suite) is free and should have most of the basic functionality with command line as well right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the quick response.&lt;/P&gt;&lt;P&gt;Swarooph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Nov 2014 18:20:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-line-compilation-for-MPC5606B/m-p/384926#M2264</guid>
      <dc:creator>swarooph</dc:creator>
      <dc:date>2014-11-07T18:20:58Z</dc:date>
    </item>
    <item>
      <title>Re: Command line compilation for MPC5606B</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-line-compilation-for-MPC5606B/m-p/384927#M2265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Swarooph,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no way to download command line tools only.&lt;/P&gt;&lt;P&gt;To have details about tool version, please go to the link:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SUITES&amp;amp;tid=CWH" title="http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SUITES&amp;amp;tid=CWH"&gt;CodeWarrior Development Suites|Freescale&lt;/A&gt;&lt;/P&gt;&lt;P&gt;At left side:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -&amp;gt; select Qorivva/5xxx(Classic IDE) for license information regarding CW for MPC55xx/56xx V2.10.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -&amp;gt; select Qorivva 56xx(Eclipse) for license information regarding CW for MCU V10.6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To resume:&lt;/P&gt;&lt;P&gt;&amp;nbsp; - CW for MPC55xx/56xx V2.10 are 2 suites:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Special Edition: C compiler and C source-level debuggerףode and data size restricted to 128 KB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Standard suite: Full version&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; - Cw for MCU V10.6 are 4 suites:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Special Edition: C source-level debugger/programmer C code and data size restricted to Qorivva: 512 KB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Basic suite: C source-level debugger/programmer C code and data size restricted to Qorivva: 1 MB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Standard suite: Unlimited C compiler and C source-level debugger.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Professional suite: Unlimited C/C++ Compiler and Debugger and RTOS(MQX, etc ...).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Special Editions are free of charge.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal Irrle&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Nov 2014 08:09:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-line-compilation-for-MPC5606B/m-p/384927#M2265</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-11-10T08:09:05Z</dc:date>
    </item>
  </channel>
</rss>