<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 64 bit install in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/64-bit-install/m-p/375862#M2114</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Classic CodeWarrior does not support Windows 7 or Windows 8, the latest version 7.2 only supports Windows XP and Vista(32-bit).&lt;/P&gt;&lt;P&gt;The first version for Coldfire which officially supports Windows 7 is Eclipse version v10.0, and now the latest Eclipse CodeWarrior version is 10.6: &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&lt;/A&gt;&lt;/P&gt;&lt;P&gt;There is a workaround to install CW for Coldfire v7.2 on Windows 7 64 bit in XP mode. This mode is available only on Win 7 Professional. It’s a XP emulation. &lt;/P&gt;&lt;P&gt;However there is a P&amp;amp;E driver issue. Customer must download the V10 from P&amp;amp;E web site too. &lt;/P&gt;&lt;P&gt;For details, please refer to:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN3936.pdf"&gt;http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN3936.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, this is un-official recommended installation. By default we recommend use to switch to Eclipse CodeWarrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fiona Kuang&lt;/P&gt;&lt;P&gt;Technical Information &amp;amp; Commercial Support&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Dec 2014 02:41:39 GMT</pubDate>
    <dc:creator>TICS_Fiona</dc:creator>
    <dc:date>2014-12-29T02:41:39Z</dc:date>
    <item>
      <title>64 bit install</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/64-bit-install/m-p/375861#M2113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How do I install CW on my PC running Windows 8.1? I get a popup window that says, &lt;/P&gt;&lt;P&gt;"CodeWarrior Development Studio For ColdFirev7.2 does not support 64 bit OS."&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried changing compatibility mode to Windows 7 and got the same window. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Dec 2014 17:39:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/64-bit-install/m-p/375861#M2113</guid>
      <dc:creator>dangela</dc:creator>
      <dc:date>2014-12-25T17:39:03Z</dc:date>
    </item>
    <item>
      <title>Re: 64 bit install</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/64-bit-install/m-p/375862#M2114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Classic CodeWarrior does not support Windows 7 or Windows 8, the latest version 7.2 only supports Windows XP and Vista(32-bit).&lt;/P&gt;&lt;P&gt;The first version for Coldfire which officially supports Windows 7 is Eclipse version v10.0, and now the latest Eclipse CodeWarrior version is 10.6: &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&lt;/A&gt;&lt;/P&gt;&lt;P&gt;There is a workaround to install CW for Coldfire v7.2 on Windows 7 64 bit in XP mode. This mode is available only on Win 7 Professional. It’s a XP emulation. &lt;/P&gt;&lt;P&gt;However there is a P&amp;amp;E driver issue. Customer must download the V10 from P&amp;amp;E web site too. &lt;/P&gt;&lt;P&gt;For details, please refer to:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN3936.pdf"&gt;http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN3936.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, this is un-official recommended installation. By default we recommend use to switch to Eclipse CodeWarrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fiona Kuang&lt;/P&gt;&lt;P&gt;Technical Information &amp;amp; Commercial Support&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Dec 2014 02:41:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/64-bit-install/m-p/375862#M2114</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2014-12-29T02:41:39Z</dc:date>
    </item>
  </channel>
</rss>