<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development Tools中的主题 Re: CMake for Codewarrior</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CMake-for-Codewarrior/m-p/252165#M207</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have not used CMake to generate makefile for Qorivva,but you can try to configure its build tool chains as the command line tools in CodeWarrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Classic CodeWarrior, these tools are under:&lt;/P&gt;&lt;P&gt;&amp;lt;CW path&amp;gt;\CW for MPC55xx and MPC56xx 2.x\PowerPC_EABI_Tools\Command_Line_Tools &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Eclipse CodeWarrior, they are under:&lt;BR /&gt;&amp;lt;CW path&amp;gt;\CW MCU v10.x\MCU\PA_Tools\Command_Line_Tools&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jan 2014 02:58:41 GMT</pubDate>
    <dc:creator>TICS_Fiona</dc:creator>
    <dc:date>2014-01-28T02:58:41Z</dc:date>
    <item>
      <title>CMake for Codewarrior</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CMake-for-Codewarrior/m-p/252164#M206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Hi,&lt;/P&gt;&lt;P&gt;I am using CMake for developing the Makefile, I have also&lt;BR /&gt;created tool chain file for the same, but it is not working as per expectation.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any one has developed toolchain file or used CMake 2.8 for Codewarrior? It&lt;BR /&gt;would be helpful if some experts can share experiences on CMake and code&lt;BR /&gt;warrior&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jan 2014 11:31:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CMake-for-Codewarrior/m-p/252164#M206</guid>
      <dc:creator>vinitp</dc:creator>
      <dc:date>2014-01-23T11:31:21Z</dc:date>
    </item>
    <item>
      <title>Re: CMake for Codewarrior</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CMake-for-Codewarrior/m-p/252165#M207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have not used CMake to generate makefile for Qorivva,but you can try to configure its build tool chains as the command line tools in CodeWarrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Classic CodeWarrior, these tools are under:&lt;/P&gt;&lt;P&gt;&amp;lt;CW path&amp;gt;\CW for MPC55xx and MPC56xx 2.x\PowerPC_EABI_Tools\Command_Line_Tools &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Eclipse CodeWarrior, they are under:&lt;BR /&gt;&amp;lt;CW path&amp;gt;\CW MCU v10.x\MCU\PA_Tools\Command_Line_Tools&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2014 02:58:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CMake-for-Codewarrior/m-p/252165#M207</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2014-01-28T02:58:41Z</dc:date>
    </item>
  </channel>
</rss>