<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development Tools中的主题 TWR-MFC52259 printf , realloc , and profiler</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/TWR-MFC52259-printf-realloc-and-profiler/m-p/373200#M2060</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class="p1"&gt;The board that the project is being run on is a TWR MCF52259 using CodeWarrior v 10.6.&lt;/P&gt;&lt;P class="p2" style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="p1"&gt;When using %f with printf their is some strange behavior. The letter f is printed and than nothing after the %f is printed out (including \n). Currently I’ve been just using %d and working around the issue for benchmarking but would like to be able to use %f.&lt;/P&gt;&lt;P class="p2" style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="p1"&gt;Is there a function that is used to replace realloc like there is for malloc? If not is there a common work around?&lt;/P&gt;&lt;P class="p2" style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="p1"&gt;For the profiler I see some timer C files have been made but didn’t see one for the 5225X boards. Is there an example of using the ColdFire_Support profiler for a 5225X board that I could look at?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Nov 2014 15:30:38 GMT</pubDate>
    <dc:creator>jacobbarthelmeh</dc:creator>
    <dc:date>2014-11-26T15:30:38Z</dc:date>
    <item>
      <title>TWR-MFC52259 printf , realloc , and profiler</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/TWR-MFC52259-printf-realloc-and-profiler/m-p/373200#M2060</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class="p1"&gt;The board that the project is being run on is a TWR MCF52259 using CodeWarrior v 10.6.&lt;/P&gt;&lt;P class="p2" style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="p1"&gt;When using %f with printf their is some strange behavior. The letter f is printed and than nothing after the %f is printed out (including \n). Currently I’ve been just using %d and working around the issue for benchmarking but would like to be able to use %f.&lt;/P&gt;&lt;P class="p2" style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="p1"&gt;Is there a function that is used to replace realloc like there is for malloc? If not is there a common work around?&lt;/P&gt;&lt;P class="p2" style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="p1"&gt;For the profiler I see some timer C files have been made but didn’t see one for the 5225X boards. Is there an example of using the ColdFire_Support profiler for a 5225X board that I could look at?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Nov 2014 15:30:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/TWR-MFC52259-printf-realloc-and-profiler/m-p/373200#M2060</guid>
      <dc:creator>jacobbarthelmeh</dc:creator>
      <dc:date>2014-11-26T15:30:38Z</dc:date>
    </item>
  </channel>
</rss>