<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックInclude a .lib file in a CW 10.2 libmaker project</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Include-a-lib-file-in-a-CW-10-2-libmaker-project/m-p/373005#M2057</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello guys,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need an help on CodeWarrior 10.2.&lt;/P&gt;&lt;P&gt;I have an old project with a HCS08 microcontroller (MC9S08DZ60) made with CodeWarrior 6.3. In this project I create a library that includes some .c and .h files, obviously, and the ansiis.lib.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I have to migrate the project in the CodeWarrior 10.2 and I must have full compatibility: hence, I have to create a .lib that can be also used in old existing project compiled using CW 6.3.&lt;/P&gt;&lt;P&gt;In CW 10.2, first of all I tried to used the "CodeWarrior classic project importer", but I cannot compile it without error: it say to me that the main is not defined in the startup file.&lt;/P&gt;&lt;P&gt;So I created a new project using the same .c and .h files and I able to compile it. Only that I can not include the ansiis.lib. I imported the project "hc08_lib", that contains ansi library, and I referenced the "hcs08_c_no_float" project that generates the ansiis.lib.&lt;/P&gt;&lt;P&gt;However, when I build my project.lib file, it does not contains the ansiis.lib.&lt;/P&gt;&lt;P&gt;How I make it possible? I found the method to make this in S08 linker options, but not in a libmaker project.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance at all that will help me.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bye!&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Mar 2015 10:56:15 GMT</pubDate>
    <dc:creator>marcoporzio</dc:creator>
    <dc:date>2015-03-10T10:56:15Z</dc:date>
    <item>
      <title>Include a .lib file in a CW 10.2 libmaker project</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Include-a-lib-file-in-a-CW-10-2-libmaker-project/m-p/373005#M2057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello guys,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need an help on CodeWarrior 10.2.&lt;/P&gt;&lt;P&gt;I have an old project with a HCS08 microcontroller (MC9S08DZ60) made with CodeWarrior 6.3. In this project I create a library that includes some .c and .h files, obviously, and the ansiis.lib.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I have to migrate the project in the CodeWarrior 10.2 and I must have full compatibility: hence, I have to create a .lib that can be also used in old existing project compiled using CW 6.3.&lt;/P&gt;&lt;P&gt;In CW 10.2, first of all I tried to used the "CodeWarrior classic project importer", but I cannot compile it without error: it say to me that the main is not defined in the startup file.&lt;/P&gt;&lt;P&gt;So I created a new project using the same .c and .h files and I able to compile it. Only that I can not include the ansiis.lib. I imported the project "hc08_lib", that contains ansi library, and I referenced the "hcs08_c_no_float" project that generates the ansiis.lib.&lt;/P&gt;&lt;P&gt;However, when I build my project.lib file, it does not contains the ansiis.lib.&lt;/P&gt;&lt;P&gt;How I make it possible? I found the method to make this in S08 linker options, but not in a libmaker project.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance at all that will help me.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bye!&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Mar 2015 10:56:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Include-a-lib-file-in-a-CW-10-2-libmaker-project/m-p/373005#M2057</guid>
      <dc:creator>marcoporzio</dc:creator>
      <dc:date>2015-03-10T10:56:15Z</dc:date>
    </item>
    <item>
      <title>Re: Include a .lib file in a CW 10.2 libmaker project</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Include-a-lib-file-in-a-CW-10-2-libmaker-project/m-p/373006#M2058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marco.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suggest you check MCU_Build_Tools_Utilities.pdf under CW10 install, "Libmaker Utility","Libmaker Interface" for how to add a library in libmaker.&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Mar 2015 09:05:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Include-a-lib-file-in-a-CW-10-2-libmaker-project/m-p/373006#M2058</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2015-03-16T09:05:21Z</dc:date>
    </item>
    <item>
      <title>Re: Include a .lib file in a CW 10.2 libmaker project</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Include-a-lib-file-in-a-CW-10-2-libmaker-project/m-p/373007#M2059</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Zhang,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First of all thank you for your answer.&lt;/P&gt;&lt;P&gt;I followed your suggestion. I found some interesting things that I previously missed.&lt;/P&gt;&lt;P&gt;However my issue was not solved: I tried to follow the manual but or I compiled the project without error, but without that ansi.lib was included ignoring my command, or I had an error ("mingw32-make: ***").&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that .lib files can not be included in another library. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Mar 2015 14:22:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Include-a-lib-file-in-a-CW-10-2-libmaker-project/m-p/373007#M2059</guid>
      <dc:creator>marcoporzio</dc:creator>
      <dc:date>2015-03-17T14:22:16Z</dc:date>
    </item>
  </channel>
</rss>