<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FXTH8700 driver for PE Multilink in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FXTH8700-driver-for-PE-Multilink/m-p/372464#M2036</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using the FXTH8700 TPMS sensor.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I downloaded the starter project from the web site but I can't download the firmware on the sensor.&lt;/P&gt;&lt;P&gt;I installed the "MCU v10.6 S08 Service Pack for HCS08 FXTH870000".&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The error occurs when I try to download the firmware using a PE Multilink.&lt;/P&gt;&lt;P&gt;It is:&lt;/P&gt;&lt;P&gt;-An application file was not specified in the launch configuration.-&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Differently from other project for mpxy8600 sensors, I saw that in the folder: Project_Setting/Debugger &lt;/P&gt;&lt;P&gt;I have only the file .launch and it is missing the .pemicro file.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could be this the problem?&lt;/P&gt;&lt;P&gt;Where can I find that file?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;RIccardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Oct 2014 09:44:57 GMT</pubDate>
    <dc:creator>riccardocescato</dc:creator>
    <dc:date>2014-10-07T09:44:57Z</dc:date>
    <item>
      <title>FXTH8700 driver for PE Multilink</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FXTH8700-driver-for-PE-Multilink/m-p/372464#M2036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using the FXTH8700 TPMS sensor.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I downloaded the starter project from the web site but I can't download the firmware on the sensor.&lt;/P&gt;&lt;P&gt;I installed the "MCU v10.6 S08 Service Pack for HCS08 FXTH870000".&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The error occurs when I try to download the firmware using a PE Multilink.&lt;/P&gt;&lt;P&gt;It is:&lt;/P&gt;&lt;P&gt;-An application file was not specified in the launch configuration.-&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Differently from other project for mpxy8600 sensors, I saw that in the folder: Project_Setting/Debugger &lt;/P&gt;&lt;P&gt;I have only the file .launch and it is missing the .pemicro file.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could be this the problem?&lt;/P&gt;&lt;P&gt;Where can I find that file?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;RIccardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Oct 2014 09:44:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FXTH8700-driver-for-PE-Multilink/m-p/372464#M2036</guid>
      <dc:creator>riccardocescato</dc:creator>
      <dc:date>2014-10-07T09:44:57Z</dc:date>
    </item>
    <item>
      <title>Re: FXTH8700 driver for PE Multilink</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FXTH8700-driver-for-PE-Multilink/m-p/372465#M2037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Riccardo:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the error message it seems that the Debug Configuration is missing the application file to load (.abs/ .afx/ .elf).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To check this go to Run -&amp;gt; Debug Configurations, select your PE Multilink connection from the left side and check that the application file is present.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;:smileyinfo: &lt;STRONG&gt;NOTE&lt;/STRONG&gt;: The application file will not exist if the project has not been compiled successfully.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Debug_App_File.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46514iDA0F915970F5D497/image-size/large?v=v2&amp;amp;px=999" role="button" title="Debug_App_File.png" alt="Debug_App_File.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Oct 2014 02:01:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FXTH8700-driver-for-PE-Multilink/m-p/372465#M2037</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-10-08T02:01:41Z</dc:date>
    </item>
  </channel>
</rss>