<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: code runs in debug but not run</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-runs-in-debug-but-not-run/m-p/371120#M2004</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you please provide information about the CodeWarrior version you are using and also the board/cpu?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Jan 2015 08:35:53 GMT</pubDate>
    <dc:creator>addiyi</dc:creator>
    <dc:date>2015-01-23T08:35:53Z</dc:date>
    <item>
      <title>code runs in debug but not run</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-runs-in-debug-but-not-run/m-p/371119#M2003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have some code that compiles and when i run it in debug mode, it works fine.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, when I choose the run option, it doesn't work&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2015 07:45:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-runs-in-debug-but-not-run/m-p/371119#M2003</guid>
      <dc:creator>gerryk</dc:creator>
      <dc:date>2015-01-23T07:45:00Z</dc:date>
    </item>
    <item>
      <title>Re: code runs in debug but not run</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-runs-in-debug-but-not-run/m-p/371120#M2004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you please provide information about the CodeWarrior version you are using and also the board/cpu?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2015 08:35:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-runs-in-debug-but-not-run/m-p/371120#M2004</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2015-01-23T08:35:53Z</dc:date>
    </item>
    <item>
      <title>Re: code runs in debug but not run</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-runs-in-debug-but-not-run/m-p/371121#M2005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CodeWarrior for MCU&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Version: 10.5&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Build Id:130916&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Custom Board with K20DX32, 64 TQFP, 50 MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the output of the JLINK console when entering debug mode:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Executing Initialization File: D:\CSSD Documents\Apparata\500RackFirmware\Arm\V0-2 Code Warrier\V0-2/Project_Settings/Debugger/init_kinetis.tcl&lt;/P&gt;&lt;P&gt;radix x &lt;/P&gt;&lt;P&gt;thread break: Stopped, 0x0, 0x0, cpuARMLittle, V0-2.elf (state, tid, pid, cpu, target) &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config hexprefix 0x &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemIdentifier p &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemWidth 32 &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemAccess 32 &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemSwap off &lt;/P&gt;&lt;P&gt;cmdwin::reg User\/System Mode Registers/LR = 0xFFFFFFFF &lt;/P&gt;&lt;P&gt;cmdwin::reg Core Debug Registers/DEMCR = 0x1000001 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION0 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION1 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION2 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION3 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Flash Patch and Breakpoint Unit Registers/FP_COMP0 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Flash Patch and Breakpoint Unit Registers/FP_COMP1 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Flash Patch and Breakpoint Unit Registers/FP_COMP2 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Flash Patch and Breakpoint Unit Registers/FP_COMP3 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Flash Patch and Breakpoint Unit Registers/FP_COMP4 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Flash Patch and Breakpoint Unit Registers/FP_COMP5 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_CTRL = 0x40000000 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_CYCCNT = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_CPICNT = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_EXCCNT = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_SLEEPCNT = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_LSUCNT = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FOLDCNT = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_COMP0 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_COMP1 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_COMP2 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_COMP3 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_MASK0 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_MASK1 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_MASK2 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_MASK3 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Instrumentation Trace Macrocell Registers/ITM_LAR = 0xc5acce55 &lt;/P&gt;&lt;P&gt;cmdwin::reg Instrumentation Trace Macrocell Registers/ITM_TER = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Instrumentation Trace Macrocell Registers/ITM_TPR = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Instrumentation Trace Macrocell Registers/ITM_TCR = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Instrumentation Trace Macrocell Registers/ITM_LAR = 0x1 &lt;/P&gt;&lt;P&gt;cmdwin::reg Embedded Trace Funnel Registers/ETF_FCR = 0x300 &lt;/P&gt;&lt;P&gt;cmdwin::reg System Control Registers/SCB_VTOR = 0x20000000 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting 3rd party flash programming...&lt;/P&gt;&lt;P&gt;INF: &lt;/P&gt;&lt;P&gt;Jlink: J-Link: Flash download: Flash programming performed for 1 range (9216 bytes)INF: &lt;/P&gt;&lt;P&gt;Jlink: J-Link: Flash download: Total time needed: 0.514s (Prepare: 0.269s, Compare: 0.004s, Erase: 0.072s, Program: 0.160s, Verify: 0.001s, Restore: 0.006s)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code now running in debug mode, so I am assuming that at this point the flash is programmed with the code as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can terminate the debug session and the code keeps running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However as soon as I power cycle, the code does not run.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I do a run command, I get the follow console output&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Executing Initialization File: D:\CSSD Documents\Apparata\500RackFirmware\Arm\V0-2 Code Warrier\V0-2/Project_Settings/Debugger/init_kinetis.tcl&lt;/P&gt;&lt;P&gt;radix x &lt;/P&gt;&lt;P&gt;thread break: Stopped, 0x0, 0x0, cpuARMLittle, V0-2.elf (state, tid, pid, cpu, target) &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config hexprefix 0x &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemIdentifier p &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemWidth 32 &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemAccess 32 &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemSwap off &lt;/P&gt;&lt;P&gt;cmdwin::reg User\/System Mode Registers/LR = 0xFFFFFFFF &lt;/P&gt;&lt;P&gt;cmdwin::reg Core Debug Registers/DEMCR = 0x1000001 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION0 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION1 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION2 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION3 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Flash Patch and Breakpoint Unit Registers/FP_COMP0 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Flash Patch and Breakpoint Unit Registers/FP_COMP1 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Flash Patch and Breakpoint Unit Registers/FP_COMP2 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Flash Patch and Breakpoint Unit Registers/FP_COMP3 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Flash Patch and Breakpoint Unit Registers/FP_COMP4 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Flash Patch and Breakpoint Unit Registers/FP_COMP5 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_CTRL = 0x40000000 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_CYCCNT = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_CPICNT = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_EXCCNT = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_SLEEPCNT = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_LSUCNT = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FOLDCNT = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_COMP0 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_COMP1 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_COMP2 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_COMP3 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_MASK0 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_MASK1 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_MASK2 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_MASK3 = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Instrumentation Trace Macrocell Registers/ITM_LAR = 0xc5acce55 &lt;/P&gt;&lt;P&gt;cmdwin::reg Instrumentation Trace Macrocell Registers/ITM_TER = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Instrumentation Trace Macrocell Registers/ITM_TPR = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Instrumentation Trace Macrocell Registers/ITM_TCR = 0x0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Instrumentation Trace Macrocell Registers/ITM_LAR = 0x1 &lt;/P&gt;&lt;P&gt;cmdwin::reg Embedded Trace Funnel Registers/ETF_FCR = 0x300 &lt;/P&gt;&lt;P&gt;cmdwin::reg System Control Registers/SCB_VTOR = 0x20000000 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting 3rd party flash programming...&lt;/P&gt;&lt;P&gt;INF: &lt;/P&gt;&lt;P&gt;Jlink: J-Link: Flash download: Flash programming was not necessaryINF: &lt;/P&gt;&lt;P&gt;Jlink: J-Link: Flash download: Total time needed: 0.286s (Prepare: 0.270s, Compare: 0.009s, Erase: 0.000s, Program: 0.000s, Verify: 0.000s, Restore: 0.006s)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So this seems to be telling me that the flash is programmed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So why does it not run?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2015 21:53:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-runs-in-debug-but-not-run/m-p/371121#M2005</guid>
      <dc:creator>gerryk</dc:creator>
      <dc:date>2015-01-23T21:53:31Z</dc:date>
    </item>
    <item>
      <title>Re: code runs in debug but not run</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-runs-in-debug-but-not-run/m-p/371122#M2006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK I have built the same code in Processor Expert Driver Suite and IAR Embedded Workbench and everything works fine, runs in both normal and debug mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So it seems like a Code Warrior issue......&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2015 23:43:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-runs-in-debug-but-not-run/m-p/371122#M2006</guid>
      <dc:creator>gerryk</dc:creator>
      <dc:date>2015-01-23T23:43:07Z</dc:date>
    </item>
    <item>
      <title>Re: code runs in debug but not run</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-runs-in-debug-but-not-run/m-p/371123#M2007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is a similar problem with what you have encountered:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/319623" title="https://community.freescale.com/thread/319623"&gt;https://community.freescale.com/thread/319623&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fiona Kuang&lt;/P&gt;&lt;P&gt;Technical Information &amp;amp; Commercial Support&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jan 2015 08:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-runs-in-debug-but-not-run/m-p/371123#M2007</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2015-01-26T08:02:59Z</dc:date>
    </item>
  </channel>
</rss>