<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックCan I use GCC with CodeWarrior 10.2 (CW10.2) ?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-I-use-GCC-with-CodeWarrior-10-2-CW10-2/m-p/364137#M1888</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have a permanent floating license to CW 10.2. I would like to upgrade the MQX version I am using for a project from 4.0.2 to 4.1.1 . The problem is that 4.1.1 uses the new GCC compiler. Is there any way I can still compile the new MQX versions with CodeWarrior 10.2? Is there some way to install support for the GCC toolchain in CW 10.2?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Oct 2014 18:38:20 GMT</pubDate>
    <dc:creator>dmitriyc</dc:creator>
    <dc:date>2014-10-02T18:38:20Z</dc:date>
    <item>
      <title>Can I use GCC with CodeWarrior 10.2 (CW10.2) ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-I-use-GCC-with-CodeWarrior-10-2-CW10-2/m-p/364137#M1888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have a permanent floating license to CW 10.2. I would like to upgrade the MQX version I am using for a project from 4.0.2 to 4.1.1 . The problem is that 4.1.1 uses the new GCC compiler. Is there any way I can still compile the new MQX versions with CodeWarrior 10.2? Is there some way to install support for the GCC toolchain in CW 10.2?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Oct 2014 18:38:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-I-use-GCC-with-CodeWarrior-10-2-CW10-2/m-p/364137#M1888</guid>
      <dc:creator>dmitriyc</dc:creator>
      <dc:date>2014-10-02T18:38:20Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use GCC with CodeWarrior 10.2 (CW10.2) ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-I-use-GCC-with-CodeWarrior-10-2-CW10-2/m-p/364138#M1889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't remember if the GCC was or not included in the MCU v10.2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - I will re-install it -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Under MCU V10.6, the GCC is delivered under the installation folder \CW MCU v10.6\Cross_Tools\arm-none-eabi-gcc-4_7_3.&lt;/P&gt;&lt;P&gt;Can you use the GCC under MCU V10.2 ?&lt;/P&gt;&lt;P&gt;I think yes ... you can call the tool in command line (we're using this way to build project).&lt;/P&gt;&lt;P&gt;Now building the MQX lib, it's another story.&lt;/P&gt;&lt;P&gt;I think it will not be easy ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't recommend you this configuration.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal Irrle&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Oct 2014 14:43:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-I-use-GCC-with-CodeWarrior-10-2-CW10-2/m-p/364138#M1889</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-10-03T14:43:07Z</dc:date>
    </item>
  </channel>
</rss>