<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development Tools中的主题 Re: Re: quitIDE command</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quitIDE-command/m-p/363931#M1883</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Windows 7 64 bit OS.&lt;/P&gt;&lt;P&gt;I've installed CW for DSC V8.2 and V8.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've performed several tests and found that I reproduced the problem on my side too.&lt;/P&gt;&lt;P&gt;However if I'm using a script (.tcl) file where I use the cmdwin::quitIDE instruction, no error is generated.&lt;/P&gt;&lt;P&gt;I've created a short example for DSC V8.2 and DSC V8.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The .tcl contains:&lt;/P&gt;&lt;P&gt;cmdwin::project -o test_dsc.mcp&lt;/P&gt;&lt;P&gt;cmdwin::debug&lt;/P&gt;&lt;P&gt;cmdwin::go&lt;/P&gt;&lt;P&gt;cmdwin::wait 5000&lt;/P&gt;&lt;P&gt;cmdwin::kill&lt;/P&gt;&lt;P&gt;cmdwin::project -close&lt;/P&gt;&lt;P&gt;cmdwin::quitIDE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See below the command prompt displays:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;++++++++++&lt;/P&gt;&lt;P&gt;E:\Temp_bis\Community\341628\test_dsc&amp;gt;"E:\Freescale\CodeWarrior for DSC56800E v8&lt;/P&gt;&lt;P&gt;.2\bin\cmdide.exe" /d test.tcl&lt;/P&gt;&lt;P&gt;Metrowerks CodeWarrior IDE. Hit /? for help&lt;/P&gt;&lt;P&gt;No Error. (Code 0)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;E:\Temp_bis\Community\341628\test_dsc&amp;gt;"E:\Freescale\CodeWarrior for DSC56800E v8&lt;/P&gt;&lt;P&gt;.3\bin\cmdide.exe" /d test_8_3.tcl&lt;/P&gt;&lt;P&gt;Freescale CodeWarrior IDE. Hit /? for help&lt;/P&gt;&lt;P&gt;No Error. (Code 0)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;E:\Temp_bis\Community\341628\test_dsc&amp;gt;&lt;/P&gt;&lt;P&gt;++++++++++&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However if I launch the IDE and use the cmdwin::quitIDE instruction outside a script file I get the error.&lt;/P&gt;&lt;P&gt;E:\Temp_bis\Community\341628\test_dsc&amp;gt;"E:\Freescale\CodeWarrior for DSC56800E v8&lt;/P&gt;&lt;P&gt;.3\bin\cmdide.exe"&lt;/P&gt;&lt;P&gt;Freescale CodeWarrior IDE. Hit /? for help&lt;/P&gt;&lt;P&gt;ERROR: Error Opening Project File. (Code 1)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This error is not linked to an issue in IDE but it's a problem between cmdIDE.exe and Command Window.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached you will find a video showing you more info and the project I've used.&lt;/P&gt;&lt;P&gt;I don't think this issue will be solved as the new development tool is based on Eclipse.&lt;/P&gt;&lt;P&gt;Last version supporting DSC architectures is CW for MCU V10.6&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Feb 2015 16:03:23 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2015-02-17T16:03:23Z</dc:date>
    <item>
      <title>quitIDE command</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quitIDE-command/m-p/363928#M1880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got an&amp;nbsp; "Opening File" error (ERRORLEVEL 1 in the DOS shell) when I use "cmdwin::quitIDE" command in "command Window".&amp;nbsp;&amp;nbsp; System accepts this command and quit IDE without any incidence.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anybody give me some hints on how to get rid of this error?&amp;nbsp;&amp;nbsp; Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Feb 2015 19:19:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quitIDE-command/m-p/363928#M1880</guid>
      <dc:creator>danielmak</dc:creator>
      <dc:date>2015-02-10T19:19:50Z</dc:date>
    </item>
    <item>
      <title>Re: quitIDE command</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quitIDE-command/m-p/363929#M1881</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel Mak,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you tell us the CodeWarrior version and the device you are using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Carlos Mendoza&lt;/P&gt;&lt;P&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2015 02:59:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quitIDE-command/m-p/363929#M1881</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2015-02-11T02:59:40Z</dc:date>
    </item>
    <item>
      <title>Re: quitIDE command</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quitIDE-command/m-p/363930#M1882</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for responding to my question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're using DSC56800/E Version 8.3, Build091203 with a USB TAP in a XP machine.&amp;nbsp; CmdIDE.exe is 5.9.0 Build 4713.&amp;nbsp; We're in the process of expanding our capacity and a second setup is needed.&amp;nbsp; The original XP machine has CmdIDE 5.6.1 Build 1658.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Daniel Mak&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2015 16:08:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quitIDE-command/m-p/363930#M1882</guid>
      <dc:creator>danielmak</dc:creator>
      <dc:date>2015-02-11T16:08:34Z</dc:date>
    </item>
    <item>
      <title>Re: Re: quitIDE command</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quitIDE-command/m-p/363931#M1883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Windows 7 64 bit OS.&lt;/P&gt;&lt;P&gt;I've installed CW for DSC V8.2 and V8.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've performed several tests and found that I reproduced the problem on my side too.&lt;/P&gt;&lt;P&gt;However if I'm using a script (.tcl) file where I use the cmdwin::quitIDE instruction, no error is generated.&lt;/P&gt;&lt;P&gt;I've created a short example for DSC V8.2 and DSC V8.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The .tcl contains:&lt;/P&gt;&lt;P&gt;cmdwin::project -o test_dsc.mcp&lt;/P&gt;&lt;P&gt;cmdwin::debug&lt;/P&gt;&lt;P&gt;cmdwin::go&lt;/P&gt;&lt;P&gt;cmdwin::wait 5000&lt;/P&gt;&lt;P&gt;cmdwin::kill&lt;/P&gt;&lt;P&gt;cmdwin::project -close&lt;/P&gt;&lt;P&gt;cmdwin::quitIDE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See below the command prompt displays:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;++++++++++&lt;/P&gt;&lt;P&gt;E:\Temp_bis\Community\341628\test_dsc&amp;gt;"E:\Freescale\CodeWarrior for DSC56800E v8&lt;/P&gt;&lt;P&gt;.2\bin\cmdide.exe" /d test.tcl&lt;/P&gt;&lt;P&gt;Metrowerks CodeWarrior IDE. Hit /? for help&lt;/P&gt;&lt;P&gt;No Error. (Code 0)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;E:\Temp_bis\Community\341628\test_dsc&amp;gt;"E:\Freescale\CodeWarrior for DSC56800E v8&lt;/P&gt;&lt;P&gt;.3\bin\cmdide.exe" /d test_8_3.tcl&lt;/P&gt;&lt;P&gt;Freescale CodeWarrior IDE. Hit /? for help&lt;/P&gt;&lt;P&gt;No Error. (Code 0)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;E:\Temp_bis\Community\341628\test_dsc&amp;gt;&lt;/P&gt;&lt;P&gt;++++++++++&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However if I launch the IDE and use the cmdwin::quitIDE instruction outside a script file I get the error.&lt;/P&gt;&lt;P&gt;E:\Temp_bis\Community\341628\test_dsc&amp;gt;"E:\Freescale\CodeWarrior for DSC56800E v8&lt;/P&gt;&lt;P&gt;.3\bin\cmdide.exe"&lt;/P&gt;&lt;P&gt;Freescale CodeWarrior IDE. Hit /? for help&lt;/P&gt;&lt;P&gt;ERROR: Error Opening Project File. (Code 1)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This error is not linked to an issue in IDE but it's a problem between cmdIDE.exe and Command Window.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached you will find a video showing you more info and the project I've used.&lt;/P&gt;&lt;P&gt;I don't think this issue will be solved as the new development tool is based on Eclipse.&lt;/P&gt;&lt;P&gt;Last version supporting DSC architectures is CW for MCU V10.6&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Feb 2015 16:03:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quitIDE-command/m-p/363931#M1883</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-02-17T16:03:23Z</dc:date>
    </item>
    <item>
      <title>Re: quitIDE command</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quitIDE-command/m-p/363932#M1884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pascal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for getting back to me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I’ll try the cwdwin commands you showed me.  I use similar commands except for the “project-close” in the .tcl file.  Let me add this command to find out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Feb 2015 17:27:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quitIDE-command/m-p/363932#M1884</guid>
      <dc:creator>danielmak</dc:creator>
      <dc:date>2015-02-17T17:27:50Z</dc:date>
    </item>
    <item>
      <title>Re: quitIDE command</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quitIDE-command/m-p/363933#M1885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pascal,&lt;/P&gt;&lt;P&gt;I tried the same cmdwin commands you suggested in a tlc script file but Error 1 still wouldn't go away.&lt;/P&gt;&lt;P&gt;Seems to me that this error is related to&amp;nbsp; "A Command Window Interpreter is still running.&amp;nbsp; CodeWarrior may crash while exiting".&amp;nbsp; It occurred when it executed the "cmdwin::quitIDE" command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Feb 2015 21:25:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quitIDE-command/m-p/363933#M1885</guid>
      <dc:creator>danielmak</dc:creator>
      <dc:date>2015-02-26T21:25:48Z</dc:date>
    </item>
  </channel>
</rss>