<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: Changeing from C to C++</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Changeing-from-C-to-C/m-p/361085#M1846</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Philip,&lt;/P&gt;&lt;P&gt;If you select C++ as language in the new project wizard, then the Processor Expert option under the Rapid Application Development is disabled, this is because Processor Expert creates C code but not C++. If you need to create a C++ project and also use Processor Expert here is this post that can help you:&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2012/10/04/processor-expert-gcc-c-and-kinetis-l-and-mqxlite/" title="http://mcuoneclipse.com/2012/10/04/processor-expert-gcc-c-and-kinetis-l-and-mqxlite/"&gt;http://mcuoneclipse.com/2012/10/04/processor-expert-gcc-c-and-kinetis-l-and-mqxlite/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Oct 2014 01:25:05 GMT</pubDate>
    <dc:creator>Carlos_Mendoza</dc:creator>
    <dc:date>2014-10-02T01:25:05Z</dc:date>
    <item>
      <title>Changeing from C to C++</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Changeing-from-C-to-C/m-p/361084#M1845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a C project working with the evaluation version of CodeWarrior, but when i try adding C++ classes, it acts like it doesn't know about C++. I get errors like "unknown type name class". I see references in the settings for a C compiler, but know a C++ compiler. I tried creating a brand new project and selecting C++, but then when I went to configure the processor in Processor Expert, it said that a processor was not selected even though I had selected my Kintetis K51DN512 in the wizard. Questions - (1) how do I get C++ to build, and (2) how do I get a new project to use my processor?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Oct 2014 14:26:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Changeing-from-C-to-C/m-p/361084#M1845</guid>
      <dc:creator>philipsearcy</dc:creator>
      <dc:date>2014-10-01T14:26:29Z</dc:date>
    </item>
    <item>
      <title>Re: Changeing from C to C++</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Changeing-from-C-to-C/m-p/361085#M1846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Philip,&lt;/P&gt;&lt;P&gt;If you select C++ as language in the new project wizard, then the Processor Expert option under the Rapid Application Development is disabled, this is because Processor Expert creates C code but not C++. If you need to create a C++ project and also use Processor Expert here is this post that can help you:&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2012/10/04/processor-expert-gcc-c-and-kinetis-l-and-mqxlite/" title="http://mcuoneclipse.com/2012/10/04/processor-expert-gcc-c-and-kinetis-l-and-mqxlite/"&gt;http://mcuoneclipse.com/2012/10/04/processor-expert-gcc-c-and-kinetis-l-and-mqxlite/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Oct 2014 01:25:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Changeing-from-C-to-C/m-p/361085#M1846</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2014-10-02T01:25:05Z</dc:date>
    </item>
  </channel>
</rss>