<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックAnyone else having Debugging Programming issues with CW 10.6 and PE Universal Multilink?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Anyone-else-having-Debugging-Programming-issues-with-CW-10-6-and/m-p/358287#M1771</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good day All,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was curious if anyone else is having debugging/programming issues with CW 10.6 and PE Micro's Universal Multilink with Kinetis K60 projects?&amp;nbsp; I ask, as I have been having a nasty time with this.&amp;nbsp; I was initially using KDS and had issues with the Multilink... these were eventually sorted, but had to abandon KDS for a some other issues (i.e. incremental compile programs, unable to debug some projects in RAM, etc).&amp;nbsp; I then switched back to CW 10.6 and for some basic Processor Exprt projects all worked mostly OK... I still had issues, but would start working after several attempts.&amp;nbsp; As I now work on a larger project I am having repeated connectivity issues between 10.6 and the PE Multilink... at least that is what the error dialog is saying.&amp;nbsp; To rule out the Multilink I purchased PE's Kinetis programming software and when 10.6 cannot connect to the Multilink for debugging or programming, I launch the PE Software and I can always connect, initialize, and even program the connected K60 part...&amp;nbsp; I then close this program and try debugging, programming, etc and I get the error that "The Debugger can not connect to the PE Device...".&amp;nbsp; Just to ensure that it was not my hardware, I use Freescale's K60 Tower board and I get the same issue.&amp;nbsp;&amp;nbsp; If I use an older version of CW (i.e. 10.2) I do not seem to have this issue...&amp;nbsp; I suppose could simply use 10.2, but would prefer to use the latest tools if possible.&amp;nbsp; For me there seems to something amiss with CW 10.6 and the Multilink... Has anyone else had this issue and if so did you ever resolve it?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Sam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Jan 2015 04:00:48 GMT</pubDate>
    <dc:creator>samsaprunoff</dc:creator>
    <dc:date>2015-01-20T04:00:48Z</dc:date>
    <item>
      <title>Anyone else having Debugging Programming issues with CW 10.6 and PE Universal Multilink?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Anyone-else-having-Debugging-Programming-issues-with-CW-10-6-and/m-p/358287#M1771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good day All,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was curious if anyone else is having debugging/programming issues with CW 10.6 and PE Micro's Universal Multilink with Kinetis K60 projects?&amp;nbsp; I ask, as I have been having a nasty time with this.&amp;nbsp; I was initially using KDS and had issues with the Multilink... these were eventually sorted, but had to abandon KDS for a some other issues (i.e. incremental compile programs, unable to debug some projects in RAM, etc).&amp;nbsp; I then switched back to CW 10.6 and for some basic Processor Exprt projects all worked mostly OK... I still had issues, but would start working after several attempts.&amp;nbsp; As I now work on a larger project I am having repeated connectivity issues between 10.6 and the PE Multilink... at least that is what the error dialog is saying.&amp;nbsp; To rule out the Multilink I purchased PE's Kinetis programming software and when 10.6 cannot connect to the Multilink for debugging or programming, I launch the PE Software and I can always connect, initialize, and even program the connected K60 part...&amp;nbsp; I then close this program and try debugging, programming, etc and I get the error that "The Debugger can not connect to the PE Device...".&amp;nbsp; Just to ensure that it was not my hardware, I use Freescale's K60 Tower board and I get the same issue.&amp;nbsp;&amp;nbsp; If I use an older version of CW (i.e. 10.2) I do not seem to have this issue...&amp;nbsp; I suppose could simply use 10.2, but would prefer to use the latest tools if possible.&amp;nbsp; For me there seems to something amiss with CW 10.6 and the Multilink... Has anyone else had this issue and if so did you ever resolve it?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Sam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2015 04:00:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Anyone-else-having-Debugging-Programming-issues-with-CW-10-6-and/m-p/358287#M1771</guid>
      <dc:creator>samsaprunoff</dc:creator>
      <dc:date>2015-01-20T04:00:48Z</dc:date>
    </item>
    <item>
      <title>Re: Anyone else having Debugging Programming issues with CW 10.6 and PE Universal Multilink?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Anyone-else-having-Debugging-Programming-issues-with-CW-10-6-and/m-p/358288#M1772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you check in your task manager if you have multiple DE.exe running (see &lt;A href="http://mcuoneclipse.com/2012/06/01/killing-me-softly-zombies-and-debugger-engines/" title="http://mcuoneclipse.com/2012/06/01/killing-me-softly-zombies-and-debugger-engines/"&gt;Killing Me Softly: Zombies and Debugger Engines | MCU on Eclipse&lt;/A&gt;) and if so, kill them?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2015 05:09:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Anyone-else-having-Debugging-Programming-issues-with-CW-10-6-and/m-p/358288#M1772</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-01-20T05:09:22Z</dc:date>
    </item>
    <item>
      <title>Re: Anyone else having Debugging Programming issues with CW 10.6 and PE Universal Multilink?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Anyone-else-having-Debugging-Programming-issues-with-CW-10-6-and/m-p/358289#M1773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good day Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response!&amp;nbsp; The was one the first things I checked, as I remembered your post about this last Fall.&amp;nbsp; That being said that is not the case here...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2015 14:40:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Anyone-else-having-Debugging-Programming-issues-with-CW-10-6-and/m-p/358289#M1773</guid>
      <dc:creator>samsaprunoff</dc:creator>
      <dc:date>2015-01-20T14:40:20Z</dc:date>
    </item>
    <item>
      <title>Re: Anyone else having Debugging Programming issues with CW 10.6 and PE Universal Multilink?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Anyone-else-having-Debugging-Programming-issues-with-CW-10-6-and/m-p/358290#M1774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Honestly, without much information it is hard to tell what the problem could be. It could be hardware, software or a combination of both.&lt;/P&gt;&lt;P&gt;Maybe you can have a look at my article here&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2014/11/03/debugging-failure-check-list-and-hints/" title="http://mcuoneclipse.com/2014/11/03/debugging-failure-check-list-and-hints/"&gt;Debugging Failure: Check List and Hints | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;which summarizes what I have encountered on my own desk?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2015 14:47:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Anyone-else-having-Debugging-Programming-issues-with-CW-10-6-and/m-p/358290#M1774</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-01-20T14:47:18Z</dc:date>
    </item>
    <item>
      <title>Re: Anyone else having Debugging Programming issues with CW 10.6 and PE Universal Multilink?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Anyone-else-having-Debugging-Programming-issues-with-CW-10-6-and/m-p/358291#M1775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good day Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will take a look at your article.&amp;nbsp; However, I have ruled out a number of things by doing the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. I have tried different hardware (K60) and have the same result... and the test hardware is Freescale's own K60 Tower dev system&lt;/P&gt;&lt;P&gt;2. To ensure that it is not the multilink and the thin BDM cable, I launch PE's Flash Programming software and I am able to immediately connect, initialize, and program the attached K60... 0 Problems and I have never had a connection issue... never.... And remember this test is without touching or altering the K60 target, multilink, etc... &lt;/P&gt;&lt;P&gt;3. If I make a simple rudimentary Processor Expert project (i.e. blink a LED) I have this issue&lt;/P&gt;&lt;P&gt;4. If I use CW 10.2 I do not have as much problem... once in a while&amp;nbsp; CW will fail to connect to the Multilink, but after a few attempts it starts to work OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Based upon the above it really looks as if there are issues between CW 10.6 and the multilink.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I said I could go back to CW 10.2... which is looking like what I must do in order to try and maintain some level of productivity...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again for the link!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2015 15:19:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Anyone-else-having-Debugging-Programming-issues-with-CW-10-6-and/m-p/358291#M1775</guid>
      <dc:creator>samsaprunoff</dc:creator>
      <dc:date>2015-01-20T15:19:41Z</dc:date>
    </item>
  </channel>
</rss>