<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to enable brake chopper pwm signal ? in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-enable-brake-chopper-pwm-signal/m-p/358069#M1770</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The BC function generates the DC-bus break control signal based on the actual DC-bus voltage. &lt;/P&gt;&lt;P&gt;So the u_dc_bus_ON and u_dc_bus_OFF thresholds have to be properly set and also actual DC-bus voltage have to be measured and passed to BC function following BC update. Check if all above is done properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The usage of the BC eTPU function is demonstrated&amp;nbsp; in the application “BLDC Motor with Speed Closed Loop and DC-Bus Break Controller”. For a detailed description of the demo refer to AN2954 (&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN2954.pdf"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'TimesLTStd-Roman','serif';"&gt;&lt;/SPAN&gt;&lt;/A&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN2954.pdf" target="test_blank"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN2954.pdf&lt;/A&gt;). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Mar 2015 09:34:09 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2015-03-18T09:34:09Z</dc:date>
    <item>
      <title>How to enable brake chopper pwm signal ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-enable-brake-chopper-pwm-signal/m-p/358068#M1769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to enable brake chopper pwm signal in GCT and it Works as long as I don't connect motor to the drive. BC pwm signal doesn't switch when three output pwm for motor are switching.&lt;/P&gt;&lt;P&gt;Anyone can help me please?&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2015 16:21:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-enable-brake-chopper-pwm-signal/m-p/358068#M1769</guid>
      <dc:creator>simon123</dc:creator>
      <dc:date>2015-03-04T16:21:22Z</dc:date>
    </item>
    <item>
      <title>Re: How to enable brake chopper pwm signal ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-enable-brake-chopper-pwm-signal/m-p/358069#M1770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The BC function generates the DC-bus break control signal based on the actual DC-bus voltage. &lt;/P&gt;&lt;P&gt;So the u_dc_bus_ON and u_dc_bus_OFF thresholds have to be properly set and also actual DC-bus voltage have to be measured and passed to BC function following BC update. Check if all above is done properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The usage of the BC eTPU function is demonstrated&amp;nbsp; in the application “BLDC Motor with Speed Closed Loop and DC-Bus Break Controller”. For a detailed description of the demo refer to AN2954 (&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN2954.pdf"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'TimesLTStd-Roman','serif';"&gt;&lt;/SPAN&gt;&lt;/A&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN2954.pdf" target="test_blank"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN2954.pdf&lt;/A&gt;). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2015 09:34:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-enable-brake-chopper-pwm-signal/m-p/358069#M1770</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2015-03-18T09:34:09Z</dc:date>
    </item>
  </channel>
</rss>