<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: &amp;quot;Flash File To Target&amp;quot; fails with; &amp;quot;0 Bytes Programmed, Check Restricted Address Range&amp;quot; in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-Flash-File-To-Target-quot-fails-with-quot-0-Bytes/m-p/358054#M1764</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jorge:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your response.  I ended up deleting the build configurations and re-creating them from scratch. That seemed to get the flash utility to download the image to flash.  Unfortunately the program will not run from reset so I have that piece to work out at the moment.  Running in debug mode works fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Oct 2014 19:00:53 GMT</pubDate>
    <dc:creator>thomasm</dc:creator>
    <dc:date>2014-10-03T19:00:53Z</dc:date>
    <item>
      <title>"Flash File To Target" fails with; "0 Bytes Programmed, Check Restricted Address Range"</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-Flash-File-To-Target-quot-fails-with-quot-0-Bytes/m-p/358052#M1762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the "Flash File To Target" utility of CW 10.5 for K60 and get failure "0 Bytes Programmed, Check Restricted Address Range". Code works fine in debug/RAM and debug/FLASH but I cannot write my application to flash.&amp;nbsp; Where should I look to fix this?&amp;nbsp; I tried to modify the target task by un-checking the "Restrict to Addresses in this Range" box but this didn't help. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Sep 2014 15:51:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-Flash-File-To-Target-quot-fails-with-quot-0-Bytes/m-p/358052#M1762</guid>
      <dc:creator>thomasm</dc:creator>
      <dc:date>2014-09-30T15:51:01Z</dc:date>
    </item>
    <item>
      <title>Re: "Flash File To Target" fails with; "0 Bytes Programmed, Check Restricted Address Range"</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-Flash-File-To-Target-quot-fails-with-quot-0-Bytes/m-p/358053#M1763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Thomas:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you get a "&lt;EM&gt;Program Command Succeeded&lt;/EM&gt;" kind of message in the console? It sounds like the next cases:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/357064"&gt;Re: K60 flash programming problem&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/409295"&gt;Please help: flash to target results in 0 bytes programmed&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First thing to check is that the file you want to flash actually has some information to be loaded to "Flash" space (e.g. that you are not selecting a file from the [RAM] build folder)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Oct 2014 02:38:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-Flash-File-To-Target-quot-fails-with-quot-0-Bytes/m-p/358053#M1763</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-10-01T02:38:14Z</dc:date>
    </item>
    <item>
      <title>Re: "Flash File To Target" fails with; "0 Bytes Programmed, Check Restricted Address Range"</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-Flash-File-To-Target-quot-fails-with-quot-0-Bytes/m-p/358054#M1764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jorge:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your response.  I ended up deleting the build configurations and re-creating them from scratch. That seemed to get the flash utility to download the image to flash.  Unfortunately the program will not run from reset so I have that piece to work out at the moment.  Running in debug mode works fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Oct 2014 19:00:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-Flash-File-To-Target-quot-fails-with-quot-0-Bytes/m-p/358054#M1764</guid>
      <dc:creator>thomasm</dc:creator>
      <dc:date>2014-10-03T19:00:53Z</dc:date>
    </item>
    <item>
      <title>Re: "Flash File To Target" fails with; "0 Bytes Programmed, Check Restricted Address Range"</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-Flash-File-To-Target-quot-fails-with-quot-0-Bytes/m-p/358055#M1765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thomas:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If program only works in debug mode, it could be caused by library selection:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/391776"&gt;Re: MK10DX256VLK7 doesn't run standalone, just when debugging. Verified it's running from FLASH, not RAM.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Oct 2014 20:43:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-Flash-File-To-Target-quot-fails-with-quot-0-Bytes/m-p/358055#M1765</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-10-03T20:43:25Z</dc:date>
    </item>
    <item>
      <title>Re: "Flash File To Target" fails with; "0 Bytes Programmed, Check Restricted Address Range"</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-Flash-File-To-Target-quot-fails-with-quot-0-Bytes/m-p/358056#M1766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much, Jorge!&amp;nbsp; That resolved the final issue. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Oct 2014 23:11:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-Flash-File-To-Target-quot-fails-with-quot-0-Bytes/m-p/358056#M1766</guid>
      <dc:creator>thomasm</dc:creator>
      <dc:date>2014-10-03T23:11:16Z</dc:date>
    </item>
    <item>
      <title>Re: "Flash File To Target" fails with; "0 Bytes Programmed, Check Restricted Address Range"</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-Flash-File-To-Target-quot-fails-with-quot-0-Bytes/m-p/358057#M1767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Jorge Gonzalez&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;I got the same problem. But when I tried to do the changes as request, it didnt work. Fyi, I am using the MK30DX256VLL7. Is there any other possibility that may cause this?&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Aug 2015 08:30:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-Flash-File-To-Target-quot-fails-with-quot-0-Bytes/m-p/358057#M1767</guid>
      <dc:creator>blurblur</dc:creator>
      <dc:date>2015-08-03T08:30:36Z</dc:date>
    </item>
    <item>
      <title>Re: "Flash File To Target" fails with; "0 Bytes Programmed, Check Restricted Address Range"</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-Flash-File-To-Target-quot-fails-with-quot-0-Bytes/m-p/358058#M1768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello norzilah abu bakar:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What do you mean with "the same problem"?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please create a new post in the space &lt;A href="https://community.nxp.com/space/2020"&gt;CodeWarrior Development Tools&lt;/A&gt;​&amp;nbsp; and provide details about your issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Aug 2015 22:00:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-Flash-File-To-Target-quot-fails-with-quot-0-Bytes/m-p/358058#M1768</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-08-04T22:00:12Z</dc:date>
    </item>
  </channel>
</rss>