<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic support for BDM parallel port in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/support-for-BDM-parallel-port/m-p/350380#M1606</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i am using codewarrior 5.1 for s12x. Operating system is Windows 7 and 64bit. i am running the hiwave.exe file to flash and debug the code and the flash tool is BDM multilink parallel port debugger from PandE micro. But when i am running the debugger from the ide i get the following error. &lt;/P&gt;&lt;P&gt;Error 126 while loading library : C:\Program Files (x86)\Freescale\CWS12v5.1\Prog\PEOSBDMV1.DLL&lt;/P&gt;&lt;P&gt;Error 126 while loading library : PEOSBDMV1.DLL&lt;/P&gt;&lt;P&gt;Unable to load OSBDMDRIVER : PEOSBDMV1.DLL&lt;/P&gt;&lt;P&gt;Can someone please help me to resolve this issue. i posted the same query in P and E micro they are saying there is no supported drivers for parallel port BDM for windows 7 and 64 bit as it is obsolete and need to switch to USB, It will take some time for me to switch to USB. Meanwhile can someone please help me on this. Can i run my virtual xp in windows 7 64. please please help me. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;vihaan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Jan 2015 05:00:16 GMT</pubDate>
    <dc:creator>vihaanred</dc:creator>
    <dc:date>2015-01-16T05:00:16Z</dc:date>
    <item>
      <title>support for BDM parallel port</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/support-for-BDM-parallel-port/m-p/350380#M1606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i am using codewarrior 5.1 for s12x. Operating system is Windows 7 and 64bit. i am running the hiwave.exe file to flash and debug the code and the flash tool is BDM multilink parallel port debugger from PandE micro. But when i am running the debugger from the ide i get the following error. &lt;/P&gt;&lt;P&gt;Error 126 while loading library : C:\Program Files (x86)\Freescale\CWS12v5.1\Prog\PEOSBDMV1.DLL&lt;/P&gt;&lt;P&gt;Error 126 while loading library : PEOSBDMV1.DLL&lt;/P&gt;&lt;P&gt;Unable to load OSBDMDRIVER : PEOSBDMV1.DLL&lt;/P&gt;&lt;P&gt;Can someone please help me to resolve this issue. i posted the same query in P and E micro they are saying there is no supported drivers for parallel port BDM for windows 7 and 64 bit as it is obsolete and need to switch to USB, It will take some time for me to switch to USB. Meanwhile can someone please help me on this. Can i run my virtual xp in windows 7 64. please please help me. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;vihaan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jan 2015 05:00:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/support-for-BDM-parallel-port/m-p/350380#M1606</guid>
      <dc:creator>vihaanred</dc:creator>
      <dc:date>2015-01-16T05:00:16Z</dc:date>
    </item>
    <item>
      <title>Re: support for BDM parallel port</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/support-for-BDM-parallel-port/m-p/350381#M1607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi vihaan.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P&amp;amp;E BDM parallel port is P&amp;amp;E product but not Freescale's. I ever got feedback from P&amp;amp;E for this tool :&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;I'm afraid our software and hardware does not support parallel port debugging &lt;/P&gt;&lt;P&gt;on any platform after Windows XP. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We don't officially support using a VM, but you can try it. It has been known &lt;/P&gt;&lt;P&gt;to work for other issues, so it may work in this case as well.&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;Hope this information can make sense to you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2015 03:30:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/support-for-BDM-parallel-port/m-p/350381#M1607</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2015-01-20T03:30:50Z</dc:date>
    </item>
    <item>
      <title>Re: support for BDM parallel port</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/support-for-BDM-parallel-port/m-p/350382#M1608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much for your response. i will try out VM, but i dont know if it will be successful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2015 05:59:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/support-for-BDM-parallel-port/m-p/350382#M1608</guid>
      <dc:creator>vihaanred</dc:creator>
      <dc:date>2015-01-20T05:59:58Z</dc:date>
    </item>
    <item>
      <title>Re: support for BDM parallel port</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/support-for-BDM-parallel-port/m-p/350383#M1609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you are welcome!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2015 06:07:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/support-for-BDM-parallel-port/m-p/350383#M1609</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2015-01-20T06:07:04Z</dc:date>
    </item>
  </channel>
</rss>