<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックThe CodeWarrior TAP can't connects USB to the target boards debugger port</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/The-CodeWarrior-TAP-can-t-connects-USB-to-the-target-boards/m-p/345670#M1511</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi，everybody, I use MCS8157 at the moment, But some problems appear at the use of&amp;nbsp; CodeWarrior TAP, The CodeWarrior TAP can't connects USB to the target boards debugger port, When the connection runs at 82%, a error is happend, that is ccs: core&amp;nbsp; not supported or failed to reset the target. We have test the signals of poreset, hreset and hreset_in, when the poreset is deasserted, the device keep hreset low until&amp;nbsp; after 1.975 seconds, that is it meets the requirement of 1.98 seconds in the MSC8157RM. We use the version 10.0. Please see the file attached.&amp;nbsp; Thank you !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 07 Sep 2014 10:39:45 GMT</pubDate>
    <dc:creator>dianlu09</dc:creator>
    <dc:date>2014-09-07T10:39:45Z</dc:date>
    <item>
      <title>The CodeWarrior TAP can't connects USB to the target boards debugger port</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/The-CodeWarrior-TAP-can-t-connects-USB-to-the-target-boards/m-p/345670#M1511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi，everybody, I use MCS8157 at the moment, But some problems appear at the use of&amp;nbsp; CodeWarrior TAP, The CodeWarrior TAP can't connects USB to the target boards debugger port, When the connection runs at 82%, a error is happend, that is ccs: core&amp;nbsp; not supported or failed to reset the target. We have test the signals of poreset, hreset and hreset_in, when the poreset is deasserted, the device keep hreset low until&amp;nbsp; after 1.975 seconds, that is it meets the requirement of 1.98 seconds in the MSC8157RM. We use the version 10.0. Please see the file attached.&amp;nbsp; Thank you !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 Sep 2014 10:39:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/The-CodeWarrior-TAP-can-t-connects-USB-to-the-target-boards/m-p/345670#M1511</guid>
      <dc:creator>dianlu09</dc:creator>
      <dc:date>2014-09-07T10:39:45Z</dc:date>
    </item>
    <item>
      <title>Re: The CodeWarrior TAP can't connects USB to the target boards debugger port</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/The-CodeWarrior-TAP-can-t-connects-USB-to-the-target-boards/m-p/345671#M1512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MSC8157 is not support in CW10.0, and CWTAP(different from USBTAP) is not supported in CW10.0, please use CW10.5 for your case. &lt;/P&gt;&lt;P&gt;Please contact Freescale support if you do not have CW10.5, and let me know your SR number.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Sep 2014 02:52:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/The-CodeWarrior-TAP-can-t-connects-USB-to-the-target-boards/m-p/345671#M1512</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2014-09-09T02:52:29Z</dc:date>
    </item>
  </channel>
</rss>