<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Version S19 file during build in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Version-S19-file-during-build/m-p/342803#M1446</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Not sure whether this is possible, but is there a way when generating the output ".s19" file to include a version number. Currently it just takes the name of the project, then I have to rename the file and give a version number manually, this can lead to human error.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Using Codewarrior IDE version 5.9&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Oct 2014 07:39:49 GMT</pubDate>
    <dc:creator>vengeful</dc:creator>
    <dc:date>2014-10-22T07:39:49Z</dc:date>
    <item>
      <title>Version S19 file during build</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Version-S19-file-during-build/m-p/342803#M1446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Not sure whether this is possible, but is there a way when generating the output ".s19" file to include a version number. Currently it just takes the name of the project, then I have to rename the file and give a version number manually, this can lead to human error.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Using Codewarrior IDE version 5.9&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Oct 2014 07:39:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Version-S19-file-during-build/m-p/342803#M1446</guid>
      <dc:creator>vengeful</dc:creator>
      <dc:date>2014-10-22T07:39:49Z</dc:date>
    </item>
    <item>
      <title>Re: Version S19 file during build</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Version-S19-file-during-build/m-p/342804#M1447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You could run a post-build step where you perform that rename with a version number.&lt;/P&gt;&lt;P&gt;You can execute multiple commands (see &lt;A href="http://mcuoneclipse.com/2014/09/23/executing-multiple-commands-as-post-build-steps-in-eclipse/" title="http://mcuoneclipse.com/2014/09/23/executing-multiple-commands-as-post-build-steps-in-eclipse/"&gt;Executing Multiple Commands as Post-Build Steps in Eclipse | MCU on Eclipse&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Oct 2014 07:44:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Version-S19-file-during-build/m-p/342804#M1447</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-10-22T07:44:41Z</dc:date>
    </item>
  </channel>
</rss>