<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to add the MK22FX512VLH12 for use in Codewarrior V10.3 in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-add-the-MK22FX512VLH12-for-use-in-Codewarrior-V10-3/m-p/341812#M1423</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As the title states, Im using Codewarrior v10.3.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was told by Jorge at Freescale that the above micro can be used in Codewarrior, but it doesn't show up in the devices list when I create a new bareboard project. I informed him but he hasn't responded yet, and I need to get this project moving. Is there an update or something I need to download? The MK22 BSP, PSP, also isn't present when I try to import a project. Is there somewhere I can download that? I have been using MQX 3.8, but have MQX 4.0, and 4.1 installed if that matters. The MK22 BSP BSP, is in 4.1 BUT not for codewarrior.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;P.S. I do NOT want to use KDS! It doesn't work (at least for the above micro).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Nov 2014 14:17:31 GMT</pubDate>
    <dc:creator>larrydemuth</dc:creator>
    <dc:date>2014-11-14T14:17:31Z</dc:date>
    <item>
      <title>How to add the MK22FX512VLH12 for use in Codewarrior V10.3</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-add-the-MK22FX512VLH12-for-use-in-Codewarrior-V10-3/m-p/341812#M1423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As the title states, Im using Codewarrior v10.3.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was told by Jorge at Freescale that the above micro can be used in Codewarrior, but it doesn't show up in the devices list when I create a new bareboard project. I informed him but he hasn't responded yet, and I need to get this project moving. Is there an update or something I need to download? The MK22 BSP, PSP, also isn't present when I try to import a project. Is there somewhere I can download that? I have been using MQX 3.8, but have MQX 4.0, and 4.1 installed if that matters. The MK22 BSP BSP, is in 4.1 BUT not for codewarrior.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;P.S. I do NOT want to use KDS! It doesn't work (at least for the above micro).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Nov 2014 14:17:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-add-the-MK22FX512VLH12-for-use-in-Codewarrior-V10-3/m-p/341812#M1423</guid>
      <dc:creator>larrydemuth</dc:creator>
      <dc:date>2014-11-14T14:17:31Z</dc:date>
    </item>
    <item>
      <title>Re: How to add the MK22FX512VLH12 for use in Codewarrior V10.3</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-add-the-MK22FX512VLH12-for-use-in-Codewarrior-V10-3/m-p/341813#M1424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Larry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CW for MCU v10.3 is little old one.&lt;/P&gt;&lt;P&gt;MCU V10.6 is the last version released some months ago.&lt;/P&gt;&lt;P&gt;The MK22FX512 is supported by this version.&lt;/P&gt;&lt;P&gt;With the Project wizard you can create an example with MQX-Lite too.&lt;/P&gt;&lt;P&gt;Regarding MQX V4.1 there is a patch for MK22FN but not for the MK22FX.&lt;/P&gt;&lt;P&gt;Attached you will find the MQXLite doc included in the MCU V10.6 installation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't have anymore the MCU V10.3 installation.&lt;/P&gt;&lt;P&gt;However I've the MCU V10.5.&lt;/P&gt;&lt;P&gt;In the release note I see the following:&lt;/P&gt;&lt;P&gt;New device support:&lt;/P&gt;&lt;P&gt; Kinetis E Series: MKE02Z16, MKE02Z32, MKE02Z64&lt;/P&gt;&lt;P&gt; Kinetis K Series: MK21FX512, MK21FN1M0, MK22FX512, MK22FN1M0.&lt;/P&gt;&lt;P&gt;The MK22FX was included since MCU V10.5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need more info regarding MQX, can I suggest you to post a question on &lt;A href="https://community.nxp.com/space/2023"&gt;MQX Software Solutions&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal Irrle&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Nov 2014 12:05:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-add-the-MK22FX512VLH12-for-use-in-Codewarrior-V10-3/m-p/341813#M1424</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-11-18T12:05:40Z</dc:date>
    </item>
  </channel>
</rss>