<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic No ADC16 VRef setting on MC56F84789 in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/No-ADC16-VRef-setting-on-MC56F84789/m-p/340935#M1407</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We choose the ADC16 A/D converter in the properties of the ADC bean.&lt;/P&gt;&lt;P&gt;After that the setting "Volt. ref. source" disappears.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We use MC56F84789 and CodeWarrior v10.6 Update 2.0.0&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 12px;"&gt;Does anyone have the same problem?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Nov 2014 12:09:24 GMT</pubDate>
    <dc:creator>marco76</dc:creator>
    <dc:date>2014-11-14T12:09:24Z</dc:date>
    <item>
      <title>No ADC16 VRef setting on MC56F84789</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/No-ADC16-VRef-setting-on-MC56F84789/m-p/340935#M1407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We choose the ADC16 A/D converter in the properties of the ADC bean.&lt;/P&gt;&lt;P&gt;After that the setting "Volt. ref. source" disappears.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We use MC56F84789 and CodeWarrior v10.6 Update 2.0.0&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 12px;"&gt;Does anyone have the same problem?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Nov 2014 12:09:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/No-ADC16-VRef-setting-on-MC56F84789/m-p/340935#M1407</guid>
      <dc:creator>marco76</dc:creator>
      <dc:date>2014-11-14T12:09:24Z</dc:date>
    </item>
    <item>
      <title>Re: No ADC16 VRef setting on MC56F84789</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/No-ADC16-VRef-setting-on-MC56F84789/m-p/340936#M1408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marco,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've reproduced the behavior on my side too.&lt;/P&gt;&lt;P&gt;I don't find relevant information in the doc excepted:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A name="DSP56xGrp8"&gt;&lt;/A&gt;&lt;SPAN class="versionspeclabel"&gt;Settings supported for Freescale 56800/E 56F801x, 56F802x, 56F803x, 56F81x, 56F82x, 56F82xx and 56F83x and MCF MCF5213_12_11, MCF521xx, MCF5221x, MCF5222x, MCF5223x and MCF5225x derivatives only or only if driver supports software waiting in order to volt. reference establish.&lt;/SPAN&gt;&lt;UL&gt;&lt;LI&gt;&lt;A name="RecoveryTimeRef"&gt;&lt;/A&gt;&lt;STRONG&gt;Volt. ref. recovery time&lt;/STRONG&gt; - This property specifies recovery time of a voltage reference after switching it on.&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A name="DSP56xGrp12"&gt;&lt;/A&gt;&lt;SPAN class="versionspeclabel"&gt;Settings supported for Freescale 56800/E 56F801x, 56F802x, 56F803x and 56F82xx and MCF MCF5213_12_11, MCF521xx, MCF5221x, MCF5222x, MCF5223x and MCF5225x derivatives only or only if ADC supports volt. ref. selection&lt;/SPAN&gt;&lt;UL&gt;&lt;LI&gt;&lt;A name="VoltRef"&gt;&lt;/A&gt;&lt;STRONG&gt;Volt. ref. source&lt;/STRONG&gt; - Voltage reference sources can be configured as internal or external.&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will check with Processor Expert team to have their feedback.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal Irrle&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Nov 2014 10:41:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/No-ADC16-VRef-setting-on-MC56F84789/m-p/340936#M1408</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-11-18T10:41:48Z</dc:date>
    </item>
    <item>
      <title>Re: No ADC16 VRef setting on MC56F84789</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/No-ADC16-VRef-setting-on-MC56F84789/m-p/340937#M1409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marco,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got feedback from Processor Expert team regarding this behavior.&lt;/P&gt;&lt;P&gt;See below:&lt;/P&gt;&lt;P&gt;+++++++++++++++++++&lt;/P&gt;&lt;P&gt;The MC56F84789 contains two different ADC device.&lt;/P&gt;&lt;P&gt;The ADC12 contains independent selection of voltage reference pins as is implemented in the ADC component.&lt;/P&gt;&lt;P&gt;The ADC16 support just selection of alternate pair of voltage reference pins and it is not encapsulated by the ADC component now.&lt;/P&gt;&lt;P&gt;As a workaround, users can use the PESL macro ADC_SAR_VOLTAGE_REF to select alternate pair of pins (see the help for details).&lt;/P&gt;&lt;P&gt;The macro must be called after ADC component initialization code (e.g. after PE_low_level_init() in the main() function).&lt;/P&gt;&lt;P&gt;+++++++++++++++++++&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal Irrle&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Nov 2014 13:35:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/No-ADC16-VRef-setting-on-MC56F84789/m-p/340937#M1409</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-11-21T13:35:08Z</dc:date>
    </item>
    <item>
      <title>Re: No ADC16 VRef setting on MC56F84789</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/No-ADC16-VRef-setting-on-MC56F84789/m-p/340938#M1410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pascal,&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Nov 2014 15:36:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/No-ADC16-VRef-setting-on-MC56F84789/m-p/340938#M1410</guid>
      <dc:creator>marco76</dc:creator>
      <dc:date>2014-11-21T15:36:29Z</dc:date>
    </item>
  </channel>
</rss>