<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development Tools中的主题 Re: Evaluation: CodeWarrior for MPC5xxv8.7 fails during installation, (windrvr6.inf file missing)</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Evaluation-CodeWarrior-for-MPC5xxv8-7-fails-during-installation/m-p/339084#M1394</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately CodeWarrior for MPC5xx V8.7 is not working on Win 7. It is a 32-bit application. Please view the note on its webpage:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MPC5XX"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MPC5XX&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We recommend to use Windows 2000, Windows XP/Vista (32-bit).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are the official OS supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At this time there is no plan for a new version supporting Win 7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are two workarounds:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1)- install it on win XP,&lt;/P&gt;&lt;P&gt;- copy installation under win 7,&lt;/P&gt;&lt;P&gt;- install new P&amp;amp;E driver if needed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) if the above will not work the other solution will be the virtual PC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Fiona&lt;/P&gt;&lt;P&gt;Technical Information &amp;amp; Commercial Support&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Sep 2014 03:06:08 GMT</pubDate>
    <dc:creator>TICS_Fiona</dc:creator>
    <dc:date>2014-09-24T03:06:08Z</dc:date>
    <item>
      <title>Evaluation: CodeWarrior for MPC5xxv8.7 fails during installation, (windrvr6.inf file missing)</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Evaluation-CodeWarrior-for-MPC5xxv8-7-fails-during-installation/m-p/339083#M1393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When downloaded the Evaluation: CodeWarrior for MPC5xx v8.7 fails during installation, (windrvr6.inf file missing)&lt;/P&gt;&lt;P&gt;Tried the CW of MPC55xx evaluation - that installed fine.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(On windows 7 service pack1 32-bit system).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any chance to install that evaluation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Sep 2014 15:34:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Evaluation-CodeWarrior-for-MPC5xxv8-7-fails-during-installation/m-p/339083#M1393</guid>
      <dc:creator>ludekpokluda</dc:creator>
      <dc:date>2014-09-23T15:34:54Z</dc:date>
    </item>
    <item>
      <title>Re: Evaluation: CodeWarrior for MPC5xxv8.7 fails during installation, (windrvr6.inf file missing)</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Evaluation-CodeWarrior-for-MPC5xxv8-7-fails-during-installation/m-p/339084#M1394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately CodeWarrior for MPC5xx V8.7 is not working on Win 7. It is a 32-bit application. Please view the note on its webpage:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MPC5XX"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MPC5XX&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We recommend to use Windows 2000, Windows XP/Vista (32-bit).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are the official OS supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At this time there is no plan for a new version supporting Win 7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are two workarounds:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1)- install it on win XP,&lt;/P&gt;&lt;P&gt;- copy installation under win 7,&lt;/P&gt;&lt;P&gt;- install new P&amp;amp;E driver if needed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) if the above will not work the other solution will be the virtual PC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Fiona&lt;/P&gt;&lt;P&gt;Technical Information &amp;amp; Commercial Support&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Sep 2014 03:06:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Evaluation-CodeWarrior-for-MPC5xxv8-7-fails-during-installation/m-p/339084#M1394</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2014-09-24T03:06:08Z</dc:date>
    </item>
    <item>
      <title>Re: Evaluation: CodeWarrior for MPC5xxv8.7 fails during installation, (windrvr6.inf file missing)</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Evaluation-CodeWarrior-for-MPC5xxv8-7-fails-during-installation/m-p/339085#M1395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Fiona,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was aware of that note you are pointing, but there was written Win7 64bit - so I was thinking by mistake, that the Win7 32-bit will be ok.&lt;/P&gt;&lt;P&gt;The installation of virtual PC worked. I also tried to move that copy to Win7 and it seems working also.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 07:20:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Evaluation-CodeWarrior-for-MPC5xxv8-7-fails-during-installation/m-p/339085#M1395</guid>
      <dc:creator>ludekpokluda</dc:creator>
      <dc:date>2014-09-26T07:20:20Z</dc:date>
    </item>
  </channel>
</rss>