<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックIs there a way to import an ELF file into the cw 10 IDE to debug?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-there-a-way-to-import-an-ELF-file-into-the-cw-10-IDE-to-debug/m-p/334302#M1277</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I build my project using a 3rd party IDE but would like to debug my code.&amp;nbsp; Can I import or open an elf file within codewarrior to utilize the debugger?&amp;nbsp; Without creating a project.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Sep 2014 18:25:34 GMT</pubDate>
    <dc:creator>patrickfoley</dc:creator>
    <dc:date>2014-09-02T18:25:34Z</dc:date>
    <item>
      <title>Is there a way to import an ELF file into the cw 10 IDE to debug?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-there-a-way-to-import-an-ELF-file-into-the-cw-10-IDE-to-debug/m-p/334302#M1277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I build my project using a 3rd party IDE but would like to debug my code.&amp;nbsp; Can I import or open an elf file within codewarrior to utilize the debugger?&amp;nbsp; Without creating a project.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Sep 2014 18:25:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-there-a-way-to-import-an-ELF-file-into-the-cw-10-IDE-to-debug/m-p/334302#M1277</guid>
      <dc:creator>patrickfoley</dc:creator>
      <dc:date>2014-09-02T18:25:34Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a way to import an ELF file into the cw 10 IDE to debug?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-there-a-way-to-import-an-ELF-file-into-the-cw-10-IDE-to-debug/m-p/334303#M1278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What target are you using?&lt;/P&gt;&lt;P&gt;If you are using Power Architecture,You can use the Import a CodeWarrior Executable file wizard to debug an externally built executable file, this contains four tasks:&lt;/P&gt;&lt;P&gt;• Import an Executable File&lt;/P&gt;&lt;P&gt;• Edit the Launch Configuration&lt;/P&gt;&lt;P&gt;• Specify the Source Lookup Path&lt;/P&gt;&lt;P&gt;• Debug Executable File&lt;/P&gt;&lt;P&gt;See Section 5.17 Debugging Externally Built Executable Files in document Targeting_PA_Processors.pdf in CodeWarrior Help/PDF for details.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Sep 2014 01:29:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-there-a-way-to-import-an-ELF-file-into-the-cw-10-IDE-to-debug/m-p/334303#M1278</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2014-09-03T01:29:24Z</dc:date>
    </item>
  </channel>
</rss>