<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックGDI Protocol fatal error</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/GDI-Protocol-fatal-error/m-p/328450#M1130</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using a MC9S08QE32 processor along with CodeWarrior 10.6 and a P&amp;amp;E Multilink Universal for debugging.&amp;nbsp; I can download the program to the chip and run the program through the debugger, but after some time the program stops and I get a pop-up error: "GDI Protocol fatal error: The Debugger is not connected to the PE device" and then I can no longer reconnect to the device and I get the problem occurred pop up: "... Failed to resume target process."&amp;nbsp; I then have to restart Codewarrior (ending the DE process doesn't always do it) to be able to reconnect to the target board.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some things that I have tried that have not fixed the problem:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Upgraded Codewarrior to 10.6&lt;/LI&gt;&lt;LI&gt;Verified stable power supply to board&lt;/LI&gt;&lt;LI&gt;Used different boards (custom boards with same processor) and I still get the problem on all of the boards&lt;/LI&gt;&lt;LI&gt;Disabled COP Watchdog&lt;/LI&gt;&lt;/UL&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This problem makes debugging very difficult and any help or suggestions at all is greatly appreciated.&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and please let me know if more information is necessary to help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Oct 2014 21:23:14 GMT</pubDate>
    <dc:creator>jtask</dc:creator>
    <dc:date>2014-10-15T21:23:14Z</dc:date>
    <item>
      <title>GDI Protocol fatal error</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/GDI-Protocol-fatal-error/m-p/328450#M1130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using a MC9S08QE32 processor along with CodeWarrior 10.6 and a P&amp;amp;E Multilink Universal for debugging.&amp;nbsp; I can download the program to the chip and run the program through the debugger, but after some time the program stops and I get a pop-up error: "GDI Protocol fatal error: The Debugger is not connected to the PE device" and then I can no longer reconnect to the device and I get the problem occurred pop up: "... Failed to resume target process."&amp;nbsp; I then have to restart Codewarrior (ending the DE process doesn't always do it) to be able to reconnect to the target board.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some things that I have tried that have not fixed the problem:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Upgraded Codewarrior to 10.6&lt;/LI&gt;&lt;LI&gt;Verified stable power supply to board&lt;/LI&gt;&lt;LI&gt;Used different boards (custom boards with same processor) and I still get the problem on all of the boards&lt;/LI&gt;&lt;LI&gt;Disabled COP Watchdog&lt;/LI&gt;&lt;/UL&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This problem makes debugging very difficult and any help or suggestions at all is greatly appreciated.&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and please let me know if more information is necessary to help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Oct 2014 21:23:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/GDI-Protocol-fatal-error/m-p/328450#M1130</guid>
      <dc:creator>jtask</dc:creator>
      <dc:date>2014-10-15T21:23:14Z</dc:date>
    </item>
    <item>
      <title>Re: GDI Protocol fatal error</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/GDI-Protocol-fatal-error/m-p/328451#M1131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I had a problem a while back with overlapping memory (&lt;A href="http://mcuoneclipse.com/2012/03/30/problem-occurred-flash-programming-with-overlapping-memory/" title="http://mcuoneclipse.com/2012/03/30/problem-occurred-flash-programming-with-overlapping-memory/"&gt;Problem Occurred: Flash programming with overlapping memory&lt;/A&gt;), but this was somehow different as it failed while downloading?&lt;/P&gt;&lt;P&gt;The other tips I have:&lt;/P&gt;&lt;P&gt;- I had once a bad USB cable: replacing the cable solved the problem. I had problems as well with bad USB connectors (check the USB solder/connections on the Multilink).&lt;/P&gt;&lt;P&gt;- USB 3.0 port? I have seen a lot of problems with that. If you have USB 3.0, try a different (USB 2.0) port on your machine.&lt;/P&gt;&lt;P&gt;- Do you have a noisy environment? I had once a problem that a motor nearby was injecting noise into the debug cable: shortening the BDM cable and/or shielding it from the motor solved it.&lt;/P&gt;&lt;P&gt;- Then I had once a bad/flacky Multilink: using a different unit identified the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope that helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Oct 2014 06:11:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/GDI-Protocol-fatal-error/m-p/328451#M1131</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-10-16T06:11:52Z</dc:date>
    </item>
    <item>
      <title>Re: GDI Protocol fatal error</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/GDI-Protocol-fatal-error/m-p/328452#M1132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response and the time that you have put into your website.&amp;nbsp; I have spent a lot of time over the past few years on your website and it has helped me out on numerous occasions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This time I seemed to have fixed the problem by moving the workspace over to my local machine, instead of on the company's network.&amp;nbsp; Maybe the network was going in and out and I kept losing a connection?&amp;nbsp; Not sure entirely but it is working now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Oct 2014 17:55:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/GDI-Protocol-fatal-error/m-p/328452#M1132</guid>
      <dc:creator>jtask</dc:creator>
      <dc:date>2014-10-16T17:55:01Z</dc:date>
    </item>
    <item>
      <title>Re: GDI Protocol fatal error</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/GDI-Protocol-fatal-error/m-p/328453#M1133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James,&lt;/P&gt;&lt;P&gt;glad to hear that :-).&lt;/P&gt;&lt;P&gt;Interesting point about having the workspace on a network (drive?). That would explain it a lot, because Eclipse does a lot of writing/reading from the .metadata. So if there is enough latency on your network, it indeed could create such issues. I would never have thought about using a network drive for the workspace. It is ok to use it for the projects itself (although not ideal).&lt;/P&gt;&lt;P&gt;But good to know this, so I try to remember that case if someone else has the same problem. So many thanks for reporting back what was the (likely) cause and solution!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Oct 2014 18:19:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/GDI-Protocol-fatal-error/m-p/328453#M1133</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-10-16T18:19:21Z</dc:date>
    </item>
  </channel>
</rss>