<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックUSB Tap: How attach to a running target, halt it, then load ELF file.</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/USB-Tap-How-attach-to-a-running-target-halt-it-then-load-ELF/m-p/326132#M1092</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been looking through the codewarrior documentation, but have not been able to find the steps for doing the following:&lt;/P&gt;&lt;P&gt;1) Attach to a running target.&lt;/P&gt;&lt;P&gt;2) Halt the target&lt;/P&gt;&lt;P&gt;3) Load an ELF file&lt;/P&gt;&lt;P&gt;4) Issue "go" command to start the executable.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a special boot loaded on the target that sits in a while (1) loop after all initialization is complete (i.e. ram). I would like to perform the listed steps once boot has reached the loop. Maybe this is possible to do via the debugger command shell / command line? It would be nice to avoid the gui as much as possible.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Jul 2014 12:52:39 GMT</pubDate>
    <dc:creator>lfa100</dc:creator>
    <dc:date>2014-07-30T12:52:39Z</dc:date>
    <item>
      <title>USB Tap: How attach to a running target, halt it, then load ELF file.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/USB-Tap-How-attach-to-a-running-target-halt-it-then-load-ELF/m-p/326132#M1092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been looking through the codewarrior documentation, but have not been able to find the steps for doing the following:&lt;/P&gt;&lt;P&gt;1) Attach to a running target.&lt;/P&gt;&lt;P&gt;2) Halt the target&lt;/P&gt;&lt;P&gt;3) Load an ELF file&lt;/P&gt;&lt;P&gt;4) Issue "go" command to start the executable.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a special boot loaded on the target that sits in a while (1) loop after all initialization is complete (i.e. ram). I would like to perform the listed steps once boot has reached the loop. Maybe this is possible to do via the debugger command shell / command line? It would be nice to avoid the gui as much as possible.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jul 2014 12:52:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/USB-Tap-How-attach-to-a-running-target-halt-it-then-load-ELF/m-p/326132#M1092</guid>
      <dc:creator>lfa100</dc:creator>
      <dc:date>2014-07-30T12:52:39Z</dc:date>
    </item>
    <item>
      <title>Re: USB Tap: How attach to a running target, halt it, then load ELF file.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/USB-Tap-How-attach-to-a-running-target-halt-it-then-load-ELF/m-p/326133#M1093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think these could help:&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2012/10/10/attach-connect-download/" title="http://mcuoneclipse.com/2012/10/10/attach-connect-download/"&gt;http://mcuoneclipse.com/2012/10/10/attach-connect-download/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2012/12/08/adding-symbols-to-the-codewarrior-debugger/" title="http://mcuoneclipse.com/2012/12/08/adding-symbols-to-the-codewarrior-debugger/"&gt;http://mcuoneclipse.com/2012/12/08/adding-symbols-to-the-codewarrior-debugger/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2012/04/27/programming-part-of-flash/" title="http://mcuoneclipse.com/2012/04/27/programming-part-of-flash/"&gt;Programming part of flash | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jul 2014 13:16:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/USB-Tap-How-attach-to-a-running-target-halt-it-then-load-ELF/m-p/326133#M1093</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-07-30T13:16:43Z</dc:date>
    </item>
  </channel>
</rss>