<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CSM-56F801 in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CSM-56F801/m-p/135792#M870</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;The CSM-56F801 uses a serial interface, as you know. The debugger software, from what you've said, seems to be trying to connect to a parallel port. You need to check your debugger settings, especially the remote debugger settings. Check the end of this &lt;A href="http://forums.freescale.com/freescale/board/message?board.id=CWDSPCOMM&amp;amp;message.id=454&amp;amp;query.id=5366#M454" target="_blank"&gt;thread&lt;/A&gt; which describes the fix when the developer experienced similar problems, but with a DSP baord that used a USB interface. HTH.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Jun 2007 22:12:09 GMT</pubDate>
    <dc:creator>J2MEJediMaster</dc:creator>
    <dc:date>2007-06-05T22:12:09Z</dc:date>
    <item>
      <title>CSM-56F801</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CSM-56F801/m-p/135791#M869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello All&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I bought a CSM-56F801 to evaluate the 56F801 DSC and I cant&amp;nbsp;&amp;nbsp;have the debug comunicating to the target. Checked in 2 computers , changed cables, tryed all possible options,cutted the CT4 and CT5 according to the manual, aparently the&amp;nbsp; CCS Plugin try to connect using the parallel port&amp;nbsp; but with the kit comes a RS-232 Serial port DB9. I also noticed that there are several references in the flyers to an Evaluation board the has the parallel connector. So, I have no clue&amp;nbsp;what to do.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;1)What is the setting to establish connection to this Student board??? Where?&lt;/DIV&gt;&lt;DIV&gt;2)What are the limitations of the debug running on this target?&lt;/DIV&gt;&lt;DIV&gt;3)Did I do a mistake buying this board? What is the purpose for? Only for software simulation?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks!!!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jun 2007 07:58:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CSM-56F801/m-p/135791#M869</guid>
      <dc:creator>Vilbcam</dc:creator>
      <dc:date>2007-06-05T07:58:47Z</dc:date>
    </item>
    <item>
      <title>Re: CSM-56F801</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CSM-56F801/m-p/135792#M870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;The CSM-56F801 uses a serial interface, as you know. The debugger software, from what you've said, seems to be trying to connect to a parallel port. You need to check your debugger settings, especially the remote debugger settings. Check the end of this &lt;A href="http://forums.freescale.com/freescale/board/message?board.id=CWDSPCOMM&amp;amp;message.id=454&amp;amp;query.id=5366#M454" target="_blank"&gt;thread&lt;/A&gt; which describes the fix when the developer experienced similar problems, but with a DSP baord that used a USB interface. HTH.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jun 2007 22:12:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CSM-56F801/m-p/135792#M870</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2007-06-05T22:12:09Z</dc:date>
    </item>
    <item>
      <title>Re: CSM-56F801</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CSM-56F801/m-p/135793#M871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thanks for your time.&amp;nbsp; There is no option for using any serial target on the target&amp;nbsp; properties window, nothing other than USB ( not this case ) or simulator.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2007 13:10:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CSM-56F801/m-p/135793#M871</guid>
      <dc:creator>Vilbcam</dc:creator>
      <dc:date>2007-06-06T13:10:33Z</dc:date>
    </item>
    <item>
      <title>Re: CSM-56F801</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CSM-56F801/m-p/135794#M872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Ok, to confirm: if you check the remote connections panel (reached from edit | preferences &amp;gt; debugger &amp;gt; remote connections) what supported connections do you see? If there isn't a serial connection, you might need to install a driver. Did the board come with a CD that had software on it? If so, check to see if there's a serial driver on the disc that needs to be installed on your computer.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2007 21:58:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CSM-56F801/m-p/135794#M872</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2007-06-06T21:58:52Z</dc:date>
    </item>
    <item>
      <title>Re: CSM-56F801</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CSM-56F801/m-p/135795#M873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;No. There is none.&lt;/DIV&gt;&lt;DIV&gt;Thanks anyway, Im ordering a different kit with the parallel port conector.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2007 00:30:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CSM-56F801/m-p/135795#M873</guid>
      <dc:creator>Vilbcam</dc:creator>
      <dc:date>2007-06-07T00:30:37Z</dc:date>
    </item>
  </channel>
</rss>