<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FreeSacale CodeWarrior 10.6 compability with DSP56F807. in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FreeSacale-CodeWarrior-10-6-compability-with-DSP56F807/m-p/2050830#M7984</link>
    <description>&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;I have a Motorola board (DSP56F807EVMUM) with Motorola&amp;nbsp;DSP56F807.&lt;/P&gt;&lt;P&gt;I have also the Freescale CodeWarrior&amp;nbsp; 10.6 MC56Fxxxxxx processor family.&lt;/P&gt;&lt;P&gt;Which processor of MC56Fxxxxxx family is code compatible with DSP56F807?&lt;/P&gt;&lt;P&gt;Can I use this CodeWarrior with this board (Parallel Port interface)?&lt;/P&gt;&lt;P&gt;Also could you provide the latest CodeWarrior compatible with this board?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Luís Gonçalves.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 25 Feb 2025 12:34:33 GMT</pubDate>
    <dc:creator>luisgo007</dc:creator>
    <dc:date>2025-02-25T12:34:33Z</dc:date>
    <item>
      <title>FreeSacale CodeWarrior 10.6 compability with DSP56F807.</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FreeSacale-CodeWarrior-10-6-compability-with-DSP56F807/m-p/2050830#M7984</link>
      <description>&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;I have a Motorola board (DSP56F807EVMUM) with Motorola&amp;nbsp;DSP56F807.&lt;/P&gt;&lt;P&gt;I have also the Freescale CodeWarrior&amp;nbsp; 10.6 MC56Fxxxxxx processor family.&lt;/P&gt;&lt;P&gt;Which processor of MC56Fxxxxxx family is code compatible with DSP56F807?&lt;/P&gt;&lt;P&gt;Can I use this CodeWarrior with this board (Parallel Port interface)?&lt;/P&gt;&lt;P&gt;Also could you provide the latest CodeWarrior compatible with this board?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Luís Gonçalves.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Feb 2025 12:34:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FreeSacale-CodeWarrior-10-6-compability-with-DSP56F807/m-p/2050830#M7984</guid>
      <dc:creator>luisgo007</dc:creator>
      <dc:date>2025-02-25T12:34:33Z</dc:date>
    </item>
    <item>
      <title>Re: FreeSacale CodeWarrior 10.6 compability with DSP56F807.</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FreeSacale-CodeWarrior-10-6-compability-with-DSP56F807/m-p/2051283#M7985</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247311"&gt;@luisgo007&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;I checked&amp;nbsp;Release Notes&amp;nbsp;for CodeWarrior v10.6.&amp;nbsp;It only supports the DSP56800EX core which used in DSC56F8xxxx family. However, the DSP56F807 uses the DSP56800 core. Therefore, CodeWarrior v10.6 cannot be used on this board.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I recommend that you use CodeWarrior (Classic IDE) v8.3. Download page:&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/software/development-software/codewarrior-development-tools/codewarrior-legacy/codewarrior-development-studio-for-56800-e-digital-signal-controllers-classic-ide-v8-3:CW-56800E-DSC" target="_blank"&gt;CodeWarrior Development Tools for 56800/E DSC | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I'm quite sure that it can be used on the DSP56F807.&lt;/P&gt;
&lt;DIV id="tinyMceEditorCeleste_Liu_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;The CodeWarrior v8.3 was released a long time ago. It is more recommended to be used on Windows 7. If you want to use it on Windows 10/11, you can refer to the following link:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/CodeWarrior-Development-Tools/Windows-7-10-Using-USB-TAP-on-CodeWarrior-for-DSC/ta-p/1126441" target="_blank"&gt;Windows 7/10: Using USB TAP on CodeWarrior for DSC - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you.&amp;nbsp;If you have any further questions or need more information, please let me know.&lt;/P&gt;
&lt;P&gt;BRs,&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;BR /&gt;------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 26 Feb 2025 03:20:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FreeSacale-CodeWarrior-10-6-compability-with-DSP56F807/m-p/2051283#M7985</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2025-02-26T03:20:38Z</dc:date>
    </item>
  </channel>
</rss>