<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックIs the CodeWarrior USB Tap useful in a Linux environment?</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Is-the-CodeWarrior-USB-Tap-useful-in-a-Linux-environment/m-p/1362353#M7816</link>
    <description>&lt;P&gt;We have boards using the MPXS2010 PowerPC processor.&lt;BR /&gt;We have an environment where we develop code using GCC under Cygwin.&lt;BR /&gt;We are moving away from Cygwin to run a Linux virtual machine, with GCC running with 'wine'.&lt;/P&gt;&lt;P&gt;Next step is to have a native PowerPC compiler under Linux.&lt;/P&gt;&lt;P&gt;I understand that CodeWarrior does not allow compiling natively on Linux (wine is not an alternative)&lt;/P&gt;&lt;P&gt;I need to understand how I can debug the code.&lt;/P&gt;&lt;P&gt;We have a Trace-32 that is used to debug code, but we need an additional seat, and the Trace-32 is very expensive. I happen to have a "CodeWarrior USB TAP, rev F"&lt;/P&gt;&lt;P&gt;This is no longer sold.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;What is the latest version of CodeWarrior, where this is supported on Windows?&lt;/LI&gt;&lt;LI&gt;Can the "CodeWarrior USB TAP," be used by any other toolchain?&lt;/LI&gt;&lt;LI&gt;Can the "CodeWarrior TAP" (with Ethernet) which is still active be used by anything but CodeWarrior?&lt;/LI&gt;&lt;/UL&gt;</description>
    <pubDate>Wed, 27 Oct 2021 09:54:11 GMT</pubDate>
    <dc:creator>emagii</dc:creator>
    <dc:date>2021-10-27T09:54:11Z</dc:date>
    <item>
      <title>Is the CodeWarrior USB Tap useful in a Linux environment?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Is-the-CodeWarrior-USB-Tap-useful-in-a-Linux-environment/m-p/1362353#M7816</link>
      <description>&lt;P&gt;We have boards using the MPXS2010 PowerPC processor.&lt;BR /&gt;We have an environment where we develop code using GCC under Cygwin.&lt;BR /&gt;We are moving away from Cygwin to run a Linux virtual machine, with GCC running with 'wine'.&lt;/P&gt;&lt;P&gt;Next step is to have a native PowerPC compiler under Linux.&lt;/P&gt;&lt;P&gt;I understand that CodeWarrior does not allow compiling natively on Linux (wine is not an alternative)&lt;/P&gt;&lt;P&gt;I need to understand how I can debug the code.&lt;/P&gt;&lt;P&gt;We have a Trace-32 that is used to debug code, but we need an additional seat, and the Trace-32 is very expensive. I happen to have a "CodeWarrior USB TAP, rev F"&lt;/P&gt;&lt;P&gt;This is no longer sold.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;What is the latest version of CodeWarrior, where this is supported on Windows?&lt;/LI&gt;&lt;LI&gt;Can the "CodeWarrior USB TAP," be used by any other toolchain?&lt;/LI&gt;&lt;LI&gt;Can the "CodeWarrior TAP" (with Ethernet) which is still active be used by anything but CodeWarrior?&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Wed, 27 Oct 2021 09:54:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Is-the-CodeWarrior-USB-Tap-useful-in-a-Linux-environment/m-p/1362353#M7816</guid>
      <dc:creator>emagii</dc:creator>
      <dc:date>2021-10-27T09:54:11Z</dc:date>
    </item>
    <item>
      <title>Re: Is the CodeWarrior USB Tap useful in a Linux environment?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Is-the-CodeWarrior-USB-Tap-useful-in-a-Linux-environment/m-p/1363902#M7817</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I'm afraid that CodeWarrior (USB) TAP is not an option.&lt;/P&gt;
&lt;P&gt;MPXS2010 was an 'industrial' version of MPC5643L microcontroller and these devices are not supported by this tool. &lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 29 Oct 2021 11:55:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Is-the-CodeWarrior-USB-Tap-useful-in-a-Linux-environment/m-p/1363902#M7817</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-10-29T11:55:18Z</dc:date>
    </item>
    <item>
      <title>Re: Is the CodeWarrior USB Tap useful in a Linux environment?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Is-the-CodeWarrior-USB-Tap-useful-in-a-Linux-environment/m-p/1386252#M7829</link>
      <description>&lt;P&gt;It appears that is it supported in the CodeWarrior 11 running under Windows.&lt;/P&gt;</description>
      <pubDate>Tue, 14 Dec 2021 08:47:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Is-the-CodeWarrior-USB-Tap-useful-in-a-Linux-environment/m-p/1386252#M7829</guid>
      <dc:creator>emagii</dc:creator>
      <dc:date>2021-12-14T08:47:50Z</dc:date>
    </item>
  </channel>
</rss>