<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 Difference between Target Task and Run Configuration</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Difference-between-Target-Task-and-Run-Configuration/m-p/818120#M7542</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm running CodeWarrior 10.4 (Eclipse-based) and I have problems flashing a program to a board. Specifically, I can flash the program successfully if I select the project in the Code Warrior Projects view and use the Run As with the proper Run Configuration. That Run Configuration refers to a installation Task, say Install Program, to download the elf file generated in the compilation phase. If however, I select the Task Install Program directly in the Target Task window, with the same run configuration as above, and select&amp;nbsp; "Execute Task", the program is downloaded and installed but it doesn't start.&amp;nbsp; What is different?&amp;nbsp; I would expect that executing a Task with a given Run configuration would be equivalent as executing the Run Configuration with that task as the download step.&amp;nbsp; But it seems that it's not the case.&amp;nbsp; What is different and how do I use the Target Task to install and run the program?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;François&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Dec 2018 20:47:44 GMT</pubDate>
    <dc:creator>francoisbronsar</dc:creator>
    <dc:date>2018-12-19T20:47:44Z</dc:date>
    <item>
      <title>Difference between Target Task and Run Configuration</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Difference-between-Target-Task-and-Run-Configuration/m-p/818120#M7542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm running CodeWarrior 10.4 (Eclipse-based) and I have problems flashing a program to a board. Specifically, I can flash the program successfully if I select the project in the Code Warrior Projects view and use the Run As with the proper Run Configuration. That Run Configuration refers to a installation Task, say Install Program, to download the elf file generated in the compilation phase. If however, I select the Task Install Program directly in the Target Task window, with the same run configuration as above, and select&amp;nbsp; "Execute Task", the program is downloaded and installed but it doesn't start.&amp;nbsp; What is different?&amp;nbsp; I would expect that executing a Task with a given Run configuration would be equivalent as executing the Run Configuration with that task as the download step.&amp;nbsp; But it seems that it's not the case.&amp;nbsp; What is different and how do I use the Target Task to install and run the program?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;François&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Dec 2018 20:47:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Difference-between-Target-Task-and-Run-Configuration/m-p/818120#M7542</guid>
      <dc:creator>francoisbronsar</dc:creator>
      <dc:date>2018-12-19T20:47:44Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between Target Task and Run Configuration</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Difference-between-Target-Task-and-Run-Configuration/m-p/818121#M7543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Hello&amp;nbsp; François,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Could you please provide more information that I can reproduce your issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Which chip ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Please take screenshot about your steps&amp;nbsp; when using RUN of&amp;nbsp; Target Tasks :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/70536i18720B15DD76F739/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;For simple , please first use the simple demo , for example LED .&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;BR&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Dec 2018 07:45:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Difference-between-Target-Task-and-Run-Configuration/m-p/818121#M7543</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-12-21T07:45:09Z</dc:date>
    </item>
  </channel>
</rss>