<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックSDK101, pgs. 6-3 &amp; 6-17, Put data into PRAM, Why?</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/SDK101-pgs-6-3-6-17-Put-data-into-PRAM-Why/m-p/816466#M7535</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Page 6-3)&amp;nbsp;&amp;nbsp; 6.1.4 pramdata.h and pramdata.c&lt;BR /&gt;When writing an embedded application, it is sometimes useful to put some or all program variables into Program RAM instead of Data RAM. The pramdata.h and pramdata.c files isolate SDK data that is destined to be placed into Program RAM. See Section 6.3 for more information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Page 6-17)&amp;nbsp;&amp;nbsp;&amp;nbsp; 6.3.1.6 Linking: Initialized Data For Program RAM&lt;BR /&gt;Section 6.1.4 explains why data is placed into Program RAM. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Section 6.1.4 does NOT explain why data is placed into Program RAM. It only states that "sometimes it useful" with NO EXPLANATION at all. One of the big-boasts to the DSC parts is the Harvard Architecture and simultaneous access of instructions and data (some chips w\2 data busses). So, to suddenly say it is useful to put data in PRAM without any context is not helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why is it useful to put data into PRAM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Oct 2018 19:49:20 GMT</pubDate>
    <dc:creator>j___</dc:creator>
    <dc:date>2018-10-02T19:49:20Z</dc:date>
    <item>
      <title>SDK101, pgs. 6-3 &amp; 6-17, Put data into PRAM, Why?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/SDK101-pgs-6-3-6-17-Put-data-into-PRAM-Why/m-p/816466#M7535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Page 6-3)&amp;nbsp;&amp;nbsp; 6.1.4 pramdata.h and pramdata.c&lt;BR /&gt;When writing an embedded application, it is sometimes useful to put some or all program variables into Program RAM instead of Data RAM. The pramdata.h and pramdata.c files isolate SDK data that is destined to be placed into Program RAM. See Section 6.3 for more information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Page 6-17)&amp;nbsp;&amp;nbsp;&amp;nbsp; 6.3.1.6 Linking: Initialized Data For Program RAM&lt;BR /&gt;Section 6.1.4 explains why data is placed into Program RAM. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Section 6.1.4 does NOT explain why data is placed into Program RAM. It only states that "sometimes it useful" with NO EXPLANATION at all. One of the big-boasts to the DSC parts is the Harvard Architecture and simultaneous access of instructions and data (some chips w\2 data busses). So, to suddenly say it is useful to put data in PRAM without any context is not helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why is it useful to put data into PRAM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Oct 2018 19:49:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/SDK101-pgs-6-3-6-17-Put-data-into-PRAM-Why/m-p/816466#M7535</guid>
      <dc:creator>j___</dc:creator>
      <dc:date>2018-10-02T19:49:20Z</dc:date>
    </item>
    <item>
      <title>Re: SDK101, pgs. 6-3 &amp; 6-17, Put data into PRAM, Why?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/SDK101-pgs-6-3-6-17-Put-data-into-PRAM-Why/m-p/816467#M7536</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you tell us which MCU are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Oct 2018 02:14:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/SDK101-pgs-6-3-6-17-Put-data-into-PRAM-Why/m-p/816467#M7536</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2018-10-09T02:14:35Z</dc:date>
    </item>
    <item>
      <title>Re: SDK101, pgs. 6-3 &amp; 6-17, Put data into PRAM, Why?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/SDK101-pgs-6-3-6-17-Put-data-into-PRAM-Why/m-p/816468#M7537</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;I'm using the 56F807.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Oct 2018 13:43:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/SDK101-pgs-6-3-6-17-Put-data-into-PRAM-Why/m-p/816468#M7537</guid>
      <dc:creator>j___</dc:creator>
      <dc:date>2018-10-16T13:43:08Z</dc:date>
    </item>
  </channel>
</rss>