<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックProblem with CodeWarrior for Coldfire 6.4 and C++</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-CodeWarrior-for-Coldfire-6-4-and-C/m-p/756678#M7455</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an old project that uses CW for Coldfire 6.4 to build for the MCF5272. This has worked on XP for a while but i would like to move the development to the Windows 10 x64 platform. I ran into issues running the installation (driver would not install and updates could not be done through the utility) but I did manage eventually to get the app installed (without any updates). However, when i go to build my old project it appears that none of the selections from the preferences are being acknowledged. I get compile errors telling me that things like "bool" is not defined and "class" is not defined and the cplusplus pragmas are illegal even though I have selected "Force C++ Compilation" and "Enable bool support". Any idea what failed on the Win10 install that this would happen?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;DJ Sisolak&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Dec 2017 21:04:59 GMT</pubDate>
    <dc:creator>djsisolak</dc:creator>
    <dc:date>2017-12-01T21:04:59Z</dc:date>
    <item>
      <title>Problem with CodeWarrior for Coldfire 6.4 and C++</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-CodeWarrior-for-Coldfire-6-4-and-C/m-p/756678#M7455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an old project that uses CW for Coldfire 6.4 to build for the MCF5272. This has worked on XP for a while but i would like to move the development to the Windows 10 x64 platform. I ran into issues running the installation (driver would not install and updates could not be done through the utility) but I did manage eventually to get the app installed (without any updates). However, when i go to build my old project it appears that none of the selections from the preferences are being acknowledged. I get compile errors telling me that things like "bool" is not defined and "class" is not defined and the cplusplus pragmas are illegal even though I have selected "Force C++ Compilation" and "Enable bool support". Any idea what failed on the Win10 install that this would happen?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;DJ Sisolak&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Dec 2017 21:04:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-CodeWarrior-for-Coldfire-6-4-and-C/m-p/756678#M7455</guid>
      <dc:creator>djsisolak</dc:creator>
      <dc:date>2017-12-01T21:04:59Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with CodeWarrior for Coldfire 6.4 and C++</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-CodeWarrior-for-Coldfire-6-4-and-C/m-p/756679#M7456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi DJ Sisolak,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe that is happening because Win 10 is not an OS supported by CodeWarrior 6.4. If you want to move your project to Win 10 I would recommend you to use the newest CodeWarrior version:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-tools/codewarrior-legacy/codewarrior-development-studios/codewarrior-for-microcontrollers/codewarrior-for-mcus-eclipse-ide-coldfire-56800-e-dsc-kinetis-qorivva-56xx-rs08-s08-s12z-v11.0:CW-MCU10?&amp;amp;tid=vanCWMCU10" title="https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-tools/codewarrior-legacy/codewarrior-development-studios/codewarrior-for-microcontrollers/codewarrior-for-mcus-eclipse-ide-coldfire-56800-e-dsc-kinetis-qorivva-56xx-rs08-s08-s12z-v11.0:CW-MCU10?&amp;amp;tid=vanCWMCU10"&gt;CodeWarrior for Microcontrollers-Eclipse IDE|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will need to do some updates to your project while migrating to this new version of CodeWarrior, you can find detailed information on this thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/379597"&gt;https://community.nxp.com/thread/379597&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Dec 2017 15:15:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-CodeWarrior-for-Coldfire-6-4-and-C/m-p/756679#M7456</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2017-12-06T15:15:36Z</dc:date>
    </item>
  </channel>
</rss>