<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Ethernet not working in MQX2.5/RTSC2.97 when upgrading to CodeWarrior 7.1 from 6.3 in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Ethernet-not-working-in-MQX2-5-RTSC2-97-when-upgrading-to/m-p/660966#M7347</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am upgrading a project from CodeWarrior for ColdFire 6.3 to CodeWarrior for ColdFire 7.1.&amp;nbsp;&amp;nbsp; Current project uses MQX2.5, RTCS2.97.&amp;nbsp; However once I upgrade the project, ethernet doens't appear to work with the 7.1 runtime libraries.&amp;nbsp; If I point the libraries back to the 6.3 versions, it works.&amp;nbsp; Any idea what the issue might be?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Feb 2017 19:51:04 GMT</pubDate>
    <dc:creator>traceecraft</dc:creator>
    <dc:date>2017-02-22T19:51:04Z</dc:date>
    <item>
      <title>Ethernet not working in MQX2.5/RTSC2.97 when upgrading to CodeWarrior 7.1 from 6.3</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Ethernet-not-working-in-MQX2-5-RTSC2-97-when-upgrading-to/m-p/660966#M7347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am upgrading a project from CodeWarrior for ColdFire 6.3 to CodeWarrior for ColdFire 7.1.&amp;nbsp;&amp;nbsp; Current project uses MQX2.5, RTCS2.97.&amp;nbsp; However once I upgrade the project, ethernet doens't appear to work with the 7.1 runtime libraries.&amp;nbsp; If I point the libraries back to the 6.3 versions, it works.&amp;nbsp; Any idea what the issue might be?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 19:51:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Ethernet-not-working-in-MQX2-5-RTSC2-97-when-upgrading-to/m-p/660966#M7347</guid>
      <dc:creator>traceecraft</dc:creator>
      <dc:date>2017-02-22T19:51:04Z</dc:date>
    </item>
  </channel>
</rss>