<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 FXOS8700 BIT IO LIBRARY</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FXOS8700-BIT-IO-LIBRARY/m-p/561669#M7178</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an eeprom and a accelerometer, and it was conected to a I2C port. I have been using a kinetis MKV31F256VLH12 that works similar to the kf64 board, except the emmbeded components like the acelerometer.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If i use the PE componen for each individual &amp;nbsp;component, it's works ok , but if i use this components working together there is an error beacuse the single PE component use the same port of the other and make error between this both.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'll try to create a new library for each component , the eeprom works ok with the new library , but the accelerometer do not response to me . I think i don't make correctly this library.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To avoid the port pproblems i am using the BiT IO component for both (eeprom - &amp;nbsp;accelerometer ).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Somebody can helpme to do the right library for the accelerometer with the Bit IO method?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i am using the 24LC512 and the FXOS8700&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Aug 2016 19:31:26 GMT</pubDate>
    <dc:creator>marceladueñas</dc:creator>
    <dc:date>2016-08-25T19:31:26Z</dc:date>
    <item>
      <title>FXOS8700 BIT IO LIBRARY</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FXOS8700-BIT-IO-LIBRARY/m-p/561669#M7178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an eeprom and a accelerometer, and it was conected to a I2C port. I have been using a kinetis MKV31F256VLH12 that works similar to the kf64 board, except the emmbeded components like the acelerometer.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If i use the PE componen for each individual &amp;nbsp;component, it's works ok , but if i use this components working together there is an error beacuse the single PE component use the same port of the other and make error between this both.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'll try to create a new library for each component , the eeprom works ok with the new library , but the accelerometer do not response to me . I think i don't make correctly this library.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To avoid the port pproblems i am using the BiT IO component for both (eeprom - &amp;nbsp;accelerometer ).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Somebody can helpme to do the right library for the accelerometer with the Bit IO method?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i am using the 24LC512 and the FXOS8700&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Aug 2016 19:31:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FXOS8700-BIT-IO-LIBRARY/m-p/561669#M7178</guid>
      <dc:creator>marceladueñas</dc:creator>
      <dc:date>2016-08-25T19:31:26Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 BIT IO LIBRARY</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FXOS8700-BIT-IO-LIBRARY/m-p/561670#M7179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marcela&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Please manually enable the pin sharing in PE Component Inspector. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN style="font-size: 11.0pt;"&gt; The expert mode needs to be enabled - ensure that "Expert" button is selected in top of Component Inspector view&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL start="2"&gt;&lt;LI&gt;&lt;SPAN style="font-size: 11.0pt;"&gt; In the inspector of peripheral module (e.g Init_CAN, Init_UART…), click with the right mouse button on the pin and select the option "Pin sharing enabled", please see the attached screenshot. &lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Hope it helps! If not, please reply again, and attach your project&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2806i16B84CDE4C79BA9A/image-size/large?v=v2&amp;amp;px=999" title="pin share.png" alt="pin share.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Fiona Kuang&lt;BR /&gt;TIC - Technical Information Center&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Mark Correct button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2016 11:27:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FXOS8700-BIT-IO-LIBRARY/m-p/561670#M7179</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2016-08-29T11:27:00Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 BIT IO LIBRARY</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FXOS8700-BIT-IO-LIBRARY/m-p/561671#M7180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Your method could solve my life but i have some problem, you are using codewarrior 10.X i am using KDS and in this interface i can't find this option. I try for pins, components but i can't find share enable, in fact there are only two methods basic and advance but no expert. :/&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2016 14:37:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FXOS8700-BIT-IO-LIBRARY/m-p/561671#M7180</guid>
      <dc:creator>marceladueñas</dc:creator>
      <dc:date>2016-08-29T14:37:55Z</dc:date>
    </item>
  </channel>
</rss>