<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I'm trying to create a Processor Expert project for S12VR48 using a new install of CW v5.2 for HCS12. in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/I-m-trying-to-create-a-Processor-Expert-project-for-S12VR48/m-p/497522#M7063</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Pascal.&amp;nbsp; I hope we can get this fixed, as I am surprised the newer CodeWarrior software does not enable everything from the previous version.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Feb 2016 19:44:26 GMT</pubDate>
    <dc:creator>michaelgoudey</dc:creator>
    <dc:date>2016-02-09T19:44:26Z</dc:date>
    <item>
      <title>I'm trying to create a Processor Expert project for S12VR48 using a new install of CW v5.2 for HCS12.</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/I-m-trying-to-create-a-Processor-Expert-project-for-S12VR48/m-p/497520#M7061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This version of CodeWarrior includes Processor Expert v3.06 for HCS12(x).&amp;nbsp; First, I create a basic project and then try to open Processor Expert view.&amp;nbsp; There is a message stating selected CPU 'MC129S12VR48' is not supported by Processor Expert.&amp;nbsp; The dialog asks me if I want to select a different CPU.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I look under the installation directory &amp;lt;CWS12v5.2&amp;gt;/Processor Expert/CPUs.&amp;nbsp; Sure enough there is a directory there "MC9S12VR64_48".&amp;nbsp; However, the components library view only shows VR16 and VR32.&amp;nbsp; Can someone explain why VR48 and VR64 are not available?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks, Michael Goudey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Feb 2016 01:06:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/I-m-trying-to-create-a-Processor-Expert-project-for-S12VR48/m-p/497520#M7061</guid>
      <dc:creator>michaelgoudey</dc:creator>
      <dc:date>2016-02-09T01:06:32Z</dc:date>
    </item>
    <item>
      <title>Re: I'm trying to create a Processor Expert project for S12VR48 using a new install of CW v5.2 for HCS12.</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/I-m-trying-to-create-a-Processor-Expert-project-for-S12VR48/m-p/497521#M7062</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The VR48 is fully supported on HC12 v5.1.&lt;/P&gt;&lt;P&gt;Under V5.2, according to the release note, Processor Expert (PEx) should support the device too.&lt;/P&gt;&lt;P&gt;It's not the case.&lt;/P&gt;&lt;P&gt;VR48 and VR64 is not supported by PEx.&lt;/P&gt;&lt;P&gt;At this time I can not provide you workaround excepted recommend you to use V5.1 and not V5.2.&lt;/P&gt;&lt;P&gt;I will check with Product Manager.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Keep you informed.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;NXP Technical Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Feb 2016 09:21:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/I-m-trying-to-create-a-Processor-Expert-project-for-S12VR48/m-p/497521#M7062</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2016-02-09T09:21:02Z</dc:date>
    </item>
    <item>
      <title>Re: I'm trying to create a Processor Expert project for S12VR48 using a new install of CW v5.2 for HCS12.</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/I-m-trying-to-create-a-Processor-Expert-project-for-S12VR48/m-p/497522#M7063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Pascal.&amp;nbsp; I hope we can get this fixed, as I am surprised the newer CodeWarrior software does not enable everything from the previous version.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Feb 2016 19:44:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/I-m-trying-to-create-a-Processor-Expert-project-for-S12VR48/m-p/497522#M7063</guid>
      <dc:creator>michaelgoudey</dc:creator>
      <dc:date>2016-02-09T19:44:26Z</dc:date>
    </item>
    <item>
      <title>Re: I'm trying to create a Processor Expert project for S12VR48 using a new install of CW v5.2 for HCS12.</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/I-m-trying-to-create-a-Processor-Expert-project-for-S12VR48/m-p/497523#M7064</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just to inform you I've contacted Processor Expert team (PEx).&lt;/P&gt;&lt;P&gt;All VR devices should be supported through PEx in the V5.2.&lt;/P&gt;&lt;P&gt;The team logged it in the bug base and it should be fixed asap.&lt;/P&gt;&lt;P&gt;At this time I can not give you more information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding the devices supported on V5.2 vs V5.1.&lt;/P&gt;&lt;P&gt;The V5.2 is supporting the last devices only which are:&lt;/P&gt;&lt;P&gt;(2) This release includes support for the following derivatives: &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - MC9S12C128, MC9S12C32, MC9S12C64, MC9S12C96&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - MC9S12G128, MC9S12G96 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - MC9S12GC128, MC9S12GC16, MC9S12GC32, MC9S12GC64 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - MC9S12GN16, MC9S12GN32&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - MC9S12P32, MC9S12P64, MC9S12P96, MC9S12P128&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - MC9S12XEP100, MC9S12XEP768&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - MC9S12XEQ384, MC9S12XEQ512&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - MC9S12XET256&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - MC9S12XS128, MC9S12XS256, MC9S12XS64&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - MC9S12VR16, MC9S12VR32, MC9S12VR48, MC9S12VR64&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using another device you need to install and use the V5.1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Feb 2016 13:58:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/I-m-trying-to-create-a-Processor-Expert-project-for-S12VR48/m-p/497523#M7064</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2016-02-10T13:58:46Z</dc:date>
    </item>
  </channel>
</rss>