<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 Re: Help modify NCV7383 demo code?</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Help-modify-NCV7383-demo-code/m-p/463656#M6977</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bob,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You have opened discussion and question with the same content, so it would be good to talk about it at one place&lt;BR /&gt;&lt;A href="https://community.nxp.com/thread/391960"&gt;Flexray NCV7383 demo boards&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 May 2016 13:18:36 GMT</pubDate>
    <dc:creator>iggi</dc:creator>
    <dc:date>2016-05-12T13:18:36Z</dc:date>
    <item>
      <title>Help modify NCV7383 demo code?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Help-modify-NCV7383-demo-code/m-p/463655#M6976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings fellow CW5.1 users, HC12 c programmers, and Flexray experts to be. I have 2 of the Freescale NCV7383 demo boards. I can recompile the provided c source and burn it into the MC9S12XF512 and the 2 boards exchange pkts with frameID 1 and 2 and payload length of 6 words (12 bytes) as designed.This is a major milestone. Next step is to chg program to send a 32 byte payload with frameID like 0xAB rather than the slot address 1,2,3,4 selected by address switch. The Freescale dude that wrote most of it is Filip.Brtan and I bet he still works for NXP, and nothing would be better than a page or 2 memo of how to mod the demo to wake up and send ID 0x57 and a 16 byte payload just like my target system on the vehicle does. I have captured the frameIDs and payloads I need, and want to be able to send them every 100ms. I see there is one other guy like me in the NXP community trying to get familiar with the board and program. Maybe NXP can make a Flexray forum for us lone wolves to collaborate in? Flexray is going to get bigger here quick. NXP needs to support their new Freescale products. Thanks folks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 May 2016 15:13:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Help-modify-NCV7383-demo-code/m-p/463655#M6976</guid>
      <dc:creator>bobgardner</dc:creator>
      <dc:date>2016-05-11T15:13:14Z</dc:date>
    </item>
    <item>
      <title>Re: Help modify NCV7383 demo code?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Help-modify-NCV7383-demo-code/m-p/463656#M6977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bob,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You have opened discussion and question with the same content, so it would be good to talk about it at one place&lt;BR /&gt;&lt;A href="https://community.nxp.com/thread/391960"&gt;Flexray NCV7383 demo boards&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2016 13:18:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Help-modify-NCV7383-demo-code/m-p/463656#M6977</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2016-05-12T13:18:36Z</dc:date>
    </item>
  </channel>
</rss>