<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 Re: Problem debugging with P&amp;E Micro USB-ML-CFE cable</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-debugging-with-P-E-Micro-USB-ML-CFE-cable/m-p/411967#M6866</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Richard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CW for Coldfire V6.4 is an old version released in 2007.&lt;/P&gt;&lt;P&gt;This tool is using the USB-ML-CFE P&amp;amp;E interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; unfortunately I don't have this interface on my side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A good way to test it is to create an example via the project wizard File + New.&lt;/P&gt;&lt;P&gt;This example will include all configurations to use the P&amp;amp;E interface.&lt;/P&gt;&lt;P&gt;By this way you can check if there is a problem with your project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the example is not running, it could be:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - a driver problem,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - interface has been damaged.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To check these 2 options:&lt;/P&gt;&lt;P&gt;-&amp;gt; do you have another interfaces ?&lt;/P&gt;&lt;P&gt;-&amp;gt; can you check on another PC ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to P&amp;amp;E web sites the interface is not available anymore&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=163" title="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=163"&gt;P&amp;amp;E Microcomputer Systems - USB-ML-CFE (Discontinued) - USB BDM&amp;nbsp; Interface cable for the ColdFire V2/V3/V4&amp;nbsp; (Discontinue…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;For details please contact P&amp;amp;E directly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P&amp;amp;E recommend to switch on Multilink Universal or Universal FX interfaces.&lt;/P&gt;&lt;P&gt;These devices are not compatible with the CodeWarrior version used.&lt;/P&gt;&lt;P&gt;BUT P&amp;amp;E developed a solution for old development tool.&lt;/P&gt;&lt;P&gt;Please have a look to:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://www.pemicro.com/faqs/faq_view.cfm?id=211" title="http://www.pemicro.com/faqs/faq_view.cfm?id=211"&gt;P&amp;amp;E Microcomputer Systems&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will help you&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Aug 2015 15:23:46 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2015-08-12T15:23:46Z</dc:date>
    <item>
      <title>Problem debugging with P&amp;E Micro USB-ML-CFE cable</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-debugging-with-P-E-Micro-USB-ML-CFE-cable/m-p/411965#M6864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been using Codewarrior 6.4 (IDE version 5.7.0, build 2264) for over 5 years now with little problem for code development on a Coldfire ETX board.&amp;nbsp; This week it no longer will process breakpoints correctly.&amp;nbsp; It will stop execution at a breakpoint, but then when I try to single step execution the IDE displays low memory (address 00000000 with decoded assembler).&amp;nbsp; If I then try to resume nothing happens, and if I try to stop I get the message "PEMicroProtocolPlugin : Stop failed".&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So far I have swapped the coldfire CPU board, swapped the P&amp;amp;E USB-ML-CFE Rev D cable, attempted to reinstall all P&amp;amp;E Drivers, run the P&amp;amp;E driver test application (that passes OK) and finally I uninstalled CodeWarrior and the P&amp;amp;E drivers and reinstalled everything again.&amp;nbsp; I still can't debug.&amp;nbsp; I believe the licensing is OK because I can compile the largish C++ code without errors.&amp;nbsp; I reverted to an earlier project, in case something weird happened to the project, but it is behaving the same way.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems like this is a P&amp;amp;E problem.&amp;nbsp; I tried installing the latest driver (V11), but it failed to install on my Dell Precision M65 Windows XP Professional (service pack 3) notebook.&amp;nbsp; I have the V9 driver (the one I have been using for years now) installed.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone offer any idea what the problem is and how to fix it?&amp;nbsp; This is especially frustrating because two weeks ago it was all working just fine with all the same hardware and software!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Aug 2015 20:15:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-debugging-with-P-E-Micro-USB-ML-CFE-cable/m-p/411965#M6864</guid>
      <dc:creator>RichSMD</dc:creator>
      <dc:date>2015-08-04T20:15:36Z</dc:date>
    </item>
    <item>
      <title>Re: Problem debugging with P&amp;E Micro USB-ML-CFE cable</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-debugging-with-P-E-Micro-USB-ML-CFE-cable/m-p/411966#M6865</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Richard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please note that the CW version that you are using is really old and its been a while since Freescale does not support such old versions. However as you mentioned the problem seems to be on the debugger. You may contact P&amp;amp;E Micro at &lt;A href="https://community.nxp.com/www.pemicro.com/support" target="test_blank"&gt;www.pemicro.com/support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2015 00:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-debugging-with-P-E-Micro-USB-ML-CFE-cable/m-p/411966#M6865</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2015-08-12T00:22:35Z</dc:date>
    </item>
    <item>
      <title>Re: Problem debugging with P&amp;E Micro USB-ML-CFE cable</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-debugging-with-P-E-Micro-USB-ML-CFE-cable/m-p/411967#M6866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Richard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CW for Coldfire V6.4 is an old version released in 2007.&lt;/P&gt;&lt;P&gt;This tool is using the USB-ML-CFE P&amp;amp;E interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; unfortunately I don't have this interface on my side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A good way to test it is to create an example via the project wizard File + New.&lt;/P&gt;&lt;P&gt;This example will include all configurations to use the P&amp;amp;E interface.&lt;/P&gt;&lt;P&gt;By this way you can check if there is a problem with your project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the example is not running, it could be:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - a driver problem,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - interface has been damaged.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To check these 2 options:&lt;/P&gt;&lt;P&gt;-&amp;gt; do you have another interfaces ?&lt;/P&gt;&lt;P&gt;-&amp;gt; can you check on another PC ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to P&amp;amp;E web sites the interface is not available anymore&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=163" title="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=163"&gt;P&amp;amp;E Microcomputer Systems - USB-ML-CFE (Discontinued) - USB BDM&amp;nbsp; Interface cable for the ColdFire V2/V3/V4&amp;nbsp; (Discontinue…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;For details please contact P&amp;amp;E directly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P&amp;amp;E recommend to switch on Multilink Universal or Universal FX interfaces.&lt;/P&gt;&lt;P&gt;These devices are not compatible with the CodeWarrior version used.&lt;/P&gt;&lt;P&gt;BUT P&amp;amp;E developed a solution for old development tool.&lt;/P&gt;&lt;P&gt;Please have a look to:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://www.pemicro.com/faqs/faq_view.cfm?id=211" title="http://www.pemicro.com/faqs/faq_view.cfm?id=211"&gt;P&amp;amp;E Microcomputer Systems&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will help you&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2015 15:23:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-debugging-with-P-E-Micro-USB-ML-CFE-cable/m-p/411967#M6866</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-08-12T15:23:46Z</dc:date>
    </item>
  </channel>
</rss>