<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CW V6.3 on Windows 8 under VMware Player in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-V6-3-on-Windows-8-under-VMware-Player/m-p/261989#M6570</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was using Code Warrior 6.3 SE and PE USB Multilink Interface Rev.C in XP Pro guest of VMWare Workstation 12.5 and debugger being not detected. Then, I have tried all issues written in many blogs however could not solve the problem until I removed vmware package completely and install VMWare Workstation 14.3 pro. The problem has been solved easily without any driver installation or updating. The problem mostly occurred due to the USB arbitration services corruption. Then, I removed VMWare Workstation PRO because the licensing, installed VMWare Workstation Player which can be used free, and installed XP Pro too. Still debugger became active and visible, working without any problem. Do not try USB Multilink Interface 12 Rev.C in Windows 10, which is not compatible even if you install CW 6.3 regarding proposed procedures.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Sep 2018 11:23:34 GMT</pubDate>
    <dc:creator>resat</dc:creator>
    <dc:date>2018-09-12T11:23:34Z</dc:date>
    <item>
      <title>CW V6.3 on Windows 8 under VMware Player</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-V6-3-on-Windows-8-under-VMware-Player/m-p/261987#M6568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a Dell 64 bit laptop running Windows 8 Pro. This machine only has USB3 ports. I am running a VM using VMware Player. This has XP Pro installed as the guest OS. I have installed CW 6.3 but cannot get the USB Multilink to be recognised by the debugger. I have tried the included drivers and also the updated drivers from P&amp;amp;E with no success. Has anyone had this combination running? Or any suggestions as to where to turn to?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am also trying CW10.4 in Windows 8 but that is a steep learning curve.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jul 2013 10:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-V6-3-on-Windows-8-under-VMware-Player/m-p/261987#M6568</guid>
      <dc:creator>stevec</dc:creator>
      <dc:date>2013-07-09T10:24:53Z</dc:date>
    </item>
    <item>
      <title>Re: CW V6.3 on Windows 8 under VMware Player</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-V6-3-on-Windows-8-under-VMware-Player/m-p/261988#M6569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steve,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't have the Windows 8 but I think it should work as the Windows 7.&lt;/P&gt;&lt;P&gt;I've installed CW for MCU V6.3 on Virtual PC and plugged the Multilink interface.&lt;/P&gt;&lt;P&gt;To be recognized under virtual PC I need to link the interface to the Virtual PC else the interface is used by Win 7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I performed some tests on my side with a MCF5441x board and found an interresting behavior.&lt;/P&gt;&lt;P&gt;the customer used Windows 8 for a classic version too (CW for MCF V7.2) which was installed on Virtual PC.&lt;/P&gt;&lt;P&gt;the process solved the problem on customer side too (windows 8).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;+++++++++++++++++++++++++++++++&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;I'm back to my Win 7 32 bit OS with Virtual PC for Multilink Universal and TWR-MCF5441x board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;First I've created a project using CW for MCU V10.4 under Win 7.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;Refer to Multilink_win_7.jpg for Multilink driver.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;I launched debugger and got refer Eclipse_connection.jpg.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;The debugger is working fine via Multilink Universal Interface.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;Second, I've created a project for same hardware under CW for Coldfire V7.2.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;Build the project and launch the debugger I got an error (Multilink was not attached).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Refer to problem_1.jpg&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;Then I attached the Multilink - problem_2.jpg&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; In this case the Multilink led switch off and Multilink under Win 7 driver is not listed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; However the Virtual PC didn't recognized it at this time.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Now un-plug the Multilink and re-plug it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The Multilink will be listed under Virtual PC device - refer to problem_3.jpg&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Now you can launch the debugger.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;At this time the Multilink is attached to Virtual PC.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;It should work on Windows 8 too.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;The rule is to:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - attach Multilink,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - unplug and replug multilink.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;This will associated to multilink to Virtual PC.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;+++++++++++++++++++++++++++++++&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Hope this will help you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Pascal&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2013 15:10:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-V6-3-on-Windows-8-under-VMware-Player/m-p/261988#M6569</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2013-07-16T15:10:56Z</dc:date>
    </item>
    <item>
      <title>Re: CW V6.3 on Windows 8 under VMware Player</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-V6-3-on-Windows-8-under-VMware-Player/m-p/261989#M6570</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was using Code Warrior 6.3 SE and PE USB Multilink Interface Rev.C in XP Pro guest of VMWare Workstation 12.5 and debugger being not detected. Then, I have tried all issues written in many blogs however could not solve the problem until I removed vmware package completely and install VMWare Workstation 14.3 pro. The problem has been solved easily without any driver installation or updating. The problem mostly occurred due to the USB arbitration services corruption. Then, I removed VMWare Workstation PRO because the licensing, installed VMWare Workstation Player which can be used free, and installed XP Pro too. Still debugger became active and visible, working without any problem. Do not try USB Multilink Interface 12 Rev.C in Windows 10, which is not compatible even if you install CW 6.3 regarding proposed procedures.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Sep 2018 11:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-V6-3-on-Windows-8-under-VMware-Player/m-p/261989#M6570</guid>
      <dc:creator>resat</dc:creator>
      <dc:date>2018-09-12T11:23:34Z</dc:date>
    </item>
    <item>
      <title>Re: CW V6.3 on Windows 8 under VMware Player</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-V6-3-on-Windows-8-under-VMware-Player/m-p/261990#M6571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use a P&amp;amp;E&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;USB Multilink Interface 12 Rev. C under Windows 10 x64 on CW 6.3 everyday for programing a and development.&amp;nbsp;&lt;A href="https://community.nxp.com/thread/302974"&gt;How-to Directly Install CodeWarrior 6.3 Classic in Windows 7 and 10 x64 (Unofficial Method)&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Most people update the drivers but forget to follow&amp;nbsp;&lt;A class="" href="https://www.pemicro.com/faqs/faq_view.cfm?id=211" title="https://www.pemicro.com/faqs/faq_view.cfm?id=211"&gt;https://www.pemicro.com/faqs/faq_view.cfm?id=211&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One way to deal with USB3 issues is to use a USB2.0 hub.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another way is to use a USBDM instead of the P&amp;amp;E device (white box version on eBay).&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2018 13:35:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-V6-3-on-Windows-8-under-VMware-Player/m-p/261990#M6571</guid>
      <dc:creator>RodneyMcGee</dc:creator>
      <dc:date>2018-09-27T13:35:40Z</dc:date>
    </item>
  </channel>
</rss>